1 /* --COPYRIGHT--,ESD
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * --/COPYRIGHT--*/
13 /*
14 * ======== Thread.xdc ========
15 */
16
17 import xdc.runtime.Error;
18 import xdc.runtime.Assert;
19 import xdc.runtime.knl.IThreadSupport;
20
21 /*!
22 * ======== Thread ========
23 * Thread services. [EXPERIMENTAL]
24 *
25 * This module manages threads through a proxy which inherits from
26 * IThreadSupport interface. It has a module wide config parameter
27 * {@link #Proxy} which needs to be bound to an OS specific delegate before
28 * this module can be used.
29 *
30 * Here is an example showing how the proxy is bound to a BIOS 6.x specific
31 * delegate.
32 *
33 * var Thread = xdc.useModule('xdc.runtime.knl.Thread');
34 * Thread.Proxy = xdc.useModule('ti.sysbios.xdcruntime.ThreadSupport');
35 *
36 * Typically a package containing the delegates has a Settings module that
37 * will bind all {@link xdc.runtime.knl} proxies. The following
38 * example sets up all the xdc.runtime.knl proxies.
39 *
40 * xdc.useModule('ti.sysbios.xdcruntime.Settings');
41 *
42 */
43
44 @InstanceInitError /* because initialization can fail */
45 @InstanceFinalize /* have to Thread_Proxy_delete(sem) on delete */
46
47 module Thread
48 {
49 /*! Thread priorities which are mapped to OS specific value by Proxy */
50 enum Priority {
51 Priority_INVALID,
52 Priority_LOWEST,
53 Priority_BELOW_NORMAL,
54 Priority_NORMAL,
55 Priority_ABOVE_NORMAL,
56 Priority_HIGHEST
57 };
58
59 /*! Invalid OS priority value */
60 const Int INVALID_OS_PRIORITY = 0;
61
62 /*! Status returned by {@link #getPri} when an error occurs */
63 const Int GETPRI_FAILED = -2;
64
65 /*! Status returned by {@link #compareOsPriorities} when an error occurs */
66 enum CompStatus {
67 CompStatus_ERROR = -2,
68 CompStatus_LOWER = -1,
69 CompStatus_EQUAL = 0,
70 CompStatus_HIGHER = 1
71 };
72
73 /*! Proxy that needs to be bound to an OS specific delegate. */
74 proxy Proxy inherits IThreadSupport;
75
76 /*! Typedef for thread function */
77 typedef Void (*RunFxn)(IArg);
78
79 /*! Struct to hold thread statistics from {@link #stat} */
80 struct Stat {
81 SizeT stackSize;
82 SizeT stackUsed;
83 }
84
85 /*! Assert when timeout passed to {@link #sleep} is zero */
86 config Assert.Id A_zeroTimeout= {
87 msg: "A_zeroTimeout: Timeout value annot be zero"
88 };
89
90 /*! Default thread stack size. */
91 config SizeT defaultStackSize = 0;
92
93 /*!
94 * ======== self ========
95 * Return the currently executing thread's handle
96 *
97 * @param(eb) Pointer to Error.Block
98 * @a(returns) Returns a handle to the currently executing thread.
99 * If the current thread is the main thread, this function
100 * returns `NULL`. NULL is also returned in case of error.
101 */
102 Handle self(Error.Block *eb);
103
104 /*!
105 * ======== start ========
106 * Start threads running
107 *
108 * This function can be used to start all statically created threads,
109 * and all threads created dynamically before this function is called.
110 * Any thread created after this function is called, starts automatically.
111 * (i.e., there is no need to call Thread_start() more than once).
112 *
113 * @param(eb) Pointer to Error.Block
114 * @a(returns) true for success; false for error
115 */
116 Bool start(Error.Block *eb);
117
118 /*!
119 * ======== yield ========
120 * Yield the currently scheduled thread
121 *
122 * @param(eb) Pointer to Error.Block
123 * @a(returns) true for success; false for error
124 */
125 Bool yield(Error.Block *eb);
126
127 /*!
128 * ======== compareOsPriorities ========
129 * Compare two os specific priority values and find out which one
130 * represents a higher priority.
131 *
132 * @p(blist) 133 * -{@link #CompStatus_ERROR} if an error occured
134 * -{@link #CompStatus_LOWER} if p1 is lower than p2
135 * -{@link #CompStatus_EQUAL} if p1=p2
136 * -{@link #CompStatus_HIGHER} if p1 is higher than p2
137 * details.
138 * @p 139 *
140 * @param(p1) priority one
141 * @param(p2) priority two
142 * @param(eb) Pointer to Error.Block
143 * @a(returns) refer to description above
144 */
145 Int compareOsPriorities(Int p1, Int p2, Error.Block *eb);
146
147 /*!
148 * ======== sleep ========
149 * Sleep for given number of microseconds
150 *
151 * This function is gauranteed to sleep for at least as long as the
152 * timeout value but the actual sleep time may be longer. NOTE:
153 * The timeout value cannot be zero.
154 *
155 * @param(timeout) timeout in microseconds
156 * @param(eb) Pointer to Error.Block
157 * @a(returns) true for success; false for error
158 */
159 Bool sleep(UInt timeout, Error.Block *eb);
160
161 instance:
162
163 /*! Thread function argument. Default is 0. */
164 config IArg arg = 0;
165
166 /*!
167 * ======== priority ========
168 * Specify the new thread's priority
169 *
170 * Thread defines several constants which allows applications to select
171 * a priority in an OS independent way: Priority_LOWEST,
172 * Priority_BELOW_NORMAL, Priority_NORMAL, Priority_ABOVE_NORMAL and
173 * Priority_HIGHEST. These values get mapped to OS specific priorities
174 * by the OS specific delegate.
175 */
176 config Priority priority = Priority_NORMAL;
177
178 /*!
179 * ======== osPriority ========
180 * OS specific thread priority
181 *
182 * Used to specify an OS specific value for priority. If set this value
183 * takes precedence over {@link #priority}.
184 */
185 config Int osPriority = INVALID_OS_PRIORITY;
186
187 /*!
188 * ======== stackSize ========
189 * Thread stack size
190 *
191 * The default value of 0 means that `{@link #defaultStackSize}` is used.
192 */
193 config SizeT stackSize = 0;
194
195 /*!
196 * ======== tls ========
197 * Thread local storage.
198 *
199 * User data associated with a thread. Must persist for the life of
200 * the thread.
201 */
202 config Ptr tls = null;
203
204 /*!
205 * ======== create ========
206 * Create a Thread object
207 *
208 * This function spawns a new thread calling the function fxn.
209 *
210 * @param(fxn) function for new thread to begin execution
211 */
212 create(RunFxn fxn);
213
214 /*!
215 * ======== join ========
216 * Block calling thread until given thread terminates.
217 *
218 * Use this functions to ensure that a thread has terminated. It is OK to
219 * call this function on a thread that has already terminated.
220 *
221 * @param(eb) Pointer to Error.Block
222 * @a(returns) true for success; false for error
223 */
224 Bool join(Error.Block *eb);
225
226 /*!
227 * ======== getPriority ========
228 * Obtain a thread's priority.
229 *
230 * For OSes that support dynamic priority boosting, this function
231 * retrieves the base priority of the thread.
232 *
233 * @param(eb) Pointer to Error.Block
234 * @a(returns) thread priority in case of success; PRIORITY_INVALID in
235 * case of error;
236 */
237 Priority getPriority(Error.Block *eb);
238
239 /*!
240 * ======== setPriority ========
241 * Set a thread's priority.
242 *
243 * For OSes that support dynamic priority boosting, this function
244 * changes the base priority of the thread.
245 *
246 * @param(newPri) new thread priority
247 * @param(eb) Pointer to Error.Block
248 * @a(returns) true for success; false for error
249 */
250 Bool setPriority(Priority newPri, Error.Block *eb);
251
252 /*!
253 * ======== getOsPriority ========
254 * Obtain a thread's OS specific priority.
255 *
256 * For OSes that support dynamic priority boosting, the value returned
257 * is the base priority of the thread.
258 *
259 * @param(eb) Pointer to Error.Block
260 * @a(returns) thread priority in case of success; GETPRI_FAILED in
261 * case of error;
262 */
263 Int getOsPriority(Error.Block *eb);
264
265 /*!
266 * ======== setOsPriority ========
267 * Set a thread's priority.
268 *
269 * This API sets the base priority of the thread on OSes that
270 * support dynamic priority boosting
271 *
272 * @param(newPri) new thread priority
273 * @param(eb) Pointer to Error.Block
274 * @a(returns) true for success; false for error
275 */
276 Bool setOsPriority(Int newPri, Error.Block *eb);
277
278 /*!
279 * ======== getOsHandle ========
280 * Get the OS thread handle
281 *
282 * @a(returns) OS thread handle
283 */
284 Ptr getOsHandle();
285
286 /*!
287 * ======== getTls ========
288 * Obtain a thread's local storage.
289 *
290 * @a(returns) null when tls has not been set.
291 */
292 Ptr getTls();
293
294 /*!
295 * ======== setTls ========
296 * Change a thread's local storage.
297 *
298 * @param(tls) tls
299 */
300 Void setTls(Ptr tls);
301
302 /*!
303 * ======== stat ========
304 * Get thread statistics
305 *
306 * @param(buf) Pointer to Stat
307 * @param(eb) Pointer to Error.Block
308 * @a(returns) true for success; false for failure
309 */
310 Bool stat(Stat* buf, Error.Block *eb);
311
312 internal:
313
314 struct Instance_State {
315 Thread.Proxy.Handle proxyHandle; /*! handle for real implementation */
316 Ptr tls; /*! store tls parameter */
317 }
318 }
319
320 /*
321 *! Revision History
322 *! ================
323 *! 17-Apr-2009 nitya Review updates
324 */
325 /*
326 * @(#) xdc.runtime.knl; 1, 0, 0,24; 9-3-2009 11:42:01; /db/ztree/library/trees/xdc-t57x/src/packages/
327 */
328