1 /* --COPYRIGHT--,ESD
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * --/COPYRIGHT--*/
13 /*
14 * ======== Semaphore.xdc ========
15 */
16
17 import xdc.runtime.Assert;
18 import xdc.runtime.Error;
19 import xdc.runtime.knl.ISemaphore;
20
21 /*!
22 * ======== Semaphore ========
23 * Provides semaphore services when an ISemaphore.Handle is available.
24 * [EXPERIMENTAL]
25 *
26 * An application can isolate itself from ISemaphore implementations by using
27 * this module. The application must first obtain an ISemaphore.Handle.
28 * It make get such a handle by directly calling {@link SemThread#create} or
29 * {@link SemProcess#create}. Then the application can use the generic
30 * APIs provided by this module.
31 */
32
33 module Semaphore
34 {
35 /*!
36 * ======== PendStatus ========
37 * Error codes returned by Semaphore_pend
38 */
39 enum PendStatus {
40 PendStatus_ERROR = -1,
41 PendStatus_TIMEOUT = 0,
42 PendStatus_SUCCESS = 1
43 };
44
45 /*! Used as the timeout value to specify wait forever */
46 const UInt FOREVER = ISemaphore.FOREVER;
47
48 /*!
49 * Proxy used for optimization.
50 *
51 * If ALL ISemaphore.Handles were created using the same module
52 * (e.g SemProcess) then setting this Proxy to SemProcess and
53 * setting Semaphore.Proxy.abstractInstances$ = false,
54 * Semaphore APIs can have better performance.
55 */
56 proxy Proxy inherits ISemaphore;
57
58 /*!
59 * ======== pend ========
60 * Wait for the semaphore to have a nonzero count, then decrement it.
61 *
62 * @p(blist) 63 * -{@link #PendStatus_ERROR} if an error occured.
64 * -{@link #PendStatus_TIMEOUT} denotes timeout.
65 * -{@link #PendStatus_SUCCESS} semaphore was decremented.
66 * details.
67 * @p 68 *
69 * @param(sem) ISemaphore.Handle to be used
70 * @param(timeout) timeout in microseconds
71 * @param(eb) Pointer to Error.Block
72 * @a(returns) status returned. (refer to above description)
73 */
74 Int pend(ISemaphore.Handle sem, UInt timeout, Error.Block *eb);
75
76 /*!
77 * ======== post ========
78 * Increment the semaphore count.
79 *
80 * @param(sem) ISemaphore.Handle to be used
81 * @param(eb) Pointer to Error.Block
82 * @a(returns) true for success, false for error in Error block.
83 */
84 Bool post(ISemaphore.Handle sem, Error.Block *eb);
85 }
86
87 /*
88 *! Revision History
89 *! ================
90 *! 17-Apr-2009 nitya Review updates
91 */
92 /*
93 * @(#) xdc.runtime.knl; 1, 0, 0,24; 9-3-2009 11:42:01; /db/ztree/library/trees/xdc-t57x/src/packages/
94 */
95