1 /* --COPYRIGHT--,ESD
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * --/COPYRIGHT--*/
13 /*
14 * ======== LoggerBuf.xdc ========
15 *
16 *! Revision History
17 *! ================
18 *! 13-Jun-2007 nitya Fixed SDSCM00020303, SDSCM00020305, SDSCM00020304
19 *! 13-Jun-2007 nitya flushAllInternal cannot be in internal section
20 *! 22-Mar-2007 rt Updated with concepts from avala-e02's LoggerBufAtomic
21 */
22
23 /*!
24 * ======== LoggerBuf ========
25 * A logger which stores `Log` events in a buffer.
26 *
27 * This module provides a logger which captures `{@link Log}` events to a
28 * buffer in realtime. The `Log` events stored in the buffer are
29 * unformatted; `Log` event formatting is deferred until some client reads
30 * the raw event data from the buffer. You can use
31 * `{@link #flush LoggerBuf_flush()}` to process the `Log` events stored
32 * in the buffer and stream the formatted output to stdout
33 * (via `{@link System#printf}`). Alternatively, you can read a raw event
34 * (via `{@link #getNextEntry}`) and send it to another client that
35 * has the resources to format the event for display.
36 *
37 * The implementation of this logger is fast with minimal stack usage
38 * making it appropriate for a realtime application.
39 * This logger writes all `Log` events to a circular buffer. As a
40 * result, the execution time of all `Log` methods bound to this type
41 * of logger are deterministic (and quite short) because there are no
42 * additional memory allocation calls after the circular buffer was
43 * allocated.
44 *
45 * If this logger is used in a preemptive environment, then an appropriate
46 * gate must be assigned to the module. For example, if events are generated
47 * from an interrupt context, then a gate that disables interrupts
48 * must be used.
49 *
50 * @p(code) 51 * var LoggerBuf = xdc.useModule('xdc.runtime.LoggerBuf');
52 * LoggerBuf.common$.gate = ...some gate instance...
53 * @p 54 *
55 * If the buffer type is circular, the log buffer of size
56 * `{@link #numEntries}` contains the last `numEntries` of `Log` events. If
57 * the buffer type is fixed, the log buffer contains the first
58 * `numEntries` events.
59 *
60 * @a(Examples) 61 * Configuration example: The following XDC configuration statements
62 * create a logger instance, assign it as the default logger for all
63 * modules, and enable `USER1` logging in all modules of the package
64 * `my.pkg`. See the `{@link Diags#setMaskMeta Diags.setMaskMeta()}` function
65 * for details on specifying the module names.
66 *
67 * @p(code) 68 * var Defaults = xdc.useModule('xdc.runtime.Defaults');
69 * var Diags = xdc.useModule('xdc.runtime.Diags');
70 * var LoggerBuf = xdc.useModule('xdc.runtime.LoggerBuf');
71 *
72 * LoggerBuf.enableFlush = true;
73 * var LoggerBufParams = new LoggerBuf.Params();
74 * LoggerBufParams.exitFlush = true;
75 * Defaults.common$.logger = LoggerBuf.create(LoggerBufParams);
76 * Diags.setMaskMeta("my.pkg.%", Diags.USER1, Diags.RUNTIME_ON);
77 * @p 78 */
79
80 @ModuleStartup /* Initialize static instances */
81 @InstanceFinalize /* this mod has cleanup fxn when instances are deleted */
82 @InstanceInitError /* instance create can fail */
83 @Gated
84
85 module LoggerBuf inherits ILogger {
86
87 /*!
88 * ======== BufType ========
89 * Type of log buffer
90 */
91 enum BufType {
92 BufType_CIRCULAR, /*! The log buffer wraps, overwriting old entries */
93 BufType_FIXED /*! The log buffer halts collection when full */
94 };
95
96 metaonlystruct BasicView {
97 String label;
98 Int lastSerial;
99 Bool enabledFlag;
100 };
101
102 metaonlystruct RecordView {
103 Int serial;
104 Int timestamp;
105 String modName;
106 String text;
107 Int eventId;
108 String eventName;
109 IArg arg0;
110 IArg arg1;
111 IArg arg2;
112 IArg arg3;
113 }
114
115 /*!
116 * ======== rovViewInfo ========
117 * @_nodoc 118 */
119 @Facet
120 metaonlyconfig xdc.rov.ViewInfo.Instance rovViewInfo =
121 xdc.rov.ViewInfo.create({
122 viewMap: [
123 ['Basic',
124 {
125 type: xdc.rov.ViewInfo.INSTANCE,
126 viewInitFxn: 'viewInitBasic',
127 structName: 'BasicView'
128 }
129 ],
130 ['Records',
131 {
132 type: xdc.rov.ViewInfo.INSTANCE_DATA,
133 viewInitFxn: 'viewInitRecords',
134 structName: 'RecordView'
135 }
136 ]
137 ]
138 });
139
140 /*!
141 * ======== TimestampProxy ========
142 * User supplied time-stamp proxy
143 *
144 * This proxy allows `LoggerBuf` to use a timestamp server different
145 * from the server used by `{@link xdc.runtime.Timestamp}`. However, if
146 * not supplied by a user, this proxy defaults to whichever timestamp
147 * server is used by `Timestamp`.
148 */
149 proxy TimestampProxy inherits ITimestampClient;
150
151 /*!
152 * ======== enableFlush ========
153 * Flush all logs at system exit
154 */
155 config Bool enableFlush = false;
156
157 /*!
158 * ======== flushAll ========
159 * Flush logs of all instances of `LoggerBuf`
160 *
161 * The user is responsible for making sure that no `LoggerBuf` instances
162 * are created or deleted while in this API, by using an appropriate gate.
163 */
164 Void flushAll();
165
166 /*!
167 * ======== flushAllInternal ========
168 * @_nodoc 169 */
170 Void flushAllInternal(Int stat);
171
172 instance:
173 /*!
174 * ======== create ========
175 * Create a `LoggerBuf` logger
176 *
177 * @see LoggerBuf#Params
178 */
179 create();
180
181 /*!
182 * ======== numEntries ========
183 * Number of entries in buffer
184 *
185 * Each entry is large enough to store one `Log` event containing up to
186 * 4 optional arguments. Events containing more than 4 arguments (such
187 * as those from `{@link Log#write5}`) use 2 entries.
188 *
189 * `numEntries` must be a power of 2.
190 */
191 config Int numEntries = 64;
192
193 /*!
194 * ======== bufType ========
195 * Log buffer type
196 */
197 config BufType bufType = BufType_CIRCULAR;
198
199 /*!
200 * ======== exitFlush ========
201 * Flush log at system exit
202 *
203 * Only used when module parameter `{@link #enableFlush}` is `true`.
204 */
205 config Bool exitFlush = false;
206
207 /*!
208 * ======== bufSection ========
209 * Section name for the buffer managed by the static instance.
210 *
211 * The default section is the 'dataSection' in the platform.
212 */
213 metaonlyconfig String bufSection = null;
214
215 /*!
216 * ======== bufHeap ========
217 * The heap that contains the `Log` buffer for dynamic instances.
218 *
219 * The default value `null` means the buffer will be allocated from
220 * the `{@link Memory#defaultHeapInstance}` heap.
221 */
222 config IHeap.Handle bufHeap = null;
223
224 /*!
225 * ======== enable ========
226 * Enable a log
227 *
228 * @a(returns) 229 * The function returns the state of the log (`TRUE` if enabled,
230 * `FALSE` if disabled) before the call. That allow clients to restore
231 * the previous state.
232 */
233 Bool enable();
234
235 /*!
236 * ======== disable ========
237 * Disable a log
238 *
239 * Events written to a disabled log are silently discarded.
240 *
241 * @a(returns) 242 * The function returns the state of the log (`TRUE` if enabled,
243 * `FALSE` if disabled) before the call. That allow clients to restore
244 * the previous state.
245 */
246 Bool disable();
247
248 /*!
249 * ======== reset ========
250 * Reset a log to empty state and enable it
251 *
252 * @a(WARNING) This method is not synchronized with other instance
253 * methods and, as a result, it must never be called when there is a
254 * chance that another instance method is currently in operation or
255 * when another method on this instance may preempt this call.
256 */
257 Void reset();
258
259 /*!
260 * ======== flush ========
261 * Read, clear, and output the contents of the log
262 *
263 * This method reads, clears, and "prints" each `Log` event (via
264 * `{@link System#printf}`) in the log.
265 */
266 Void flush();
267
268 /*!
269 * ======== getNextEntry ========
270 * Fills the passed `{@link Log#EventRec}` with the next entry in the log.
271 *
272 * This function is used to read and clear `Log` events from the
273 * buffer maintained by the `LoggerBuf` instance. The `Log` event can
274 * then be transmitted and displayed on a host.
275 *
276 * A read pointer is maintained in the `LoggerBuf` instance and
277 * points to the next record to read. Entries are not necessarily
278 * returned in chronological order, since buffers of type
279 * `{@link #BufType_CIRCULAR}` can wrap.
280 *
281 * @param(evtRec) pointer to a supplied `EventRec` object where the next
282 * entry in the log is copied to
283 *
284 * @a(returns) 285 * This function reports the number of entries actually read. The only
286 * values that can be returned are:
287 * @p(blist) 288 * - 0 no more entries to read
289 * - 1 or 2 read a complete entry written by `write4` or `write8`
290 * - -1 cleared an incomplete/overwritten entry, more entries to read
291 */
292 Int getNextEntry(Log.EventRec *evtRec);
293
294 internal:
295
296 const Int8 FULL = -1;
297 const Int8 WRAP = 0;
298
299 const Int8 NEXT = 1;
300
301 struct Entry {
302 Types.Timestamp64 tstamp;
303 Bits32 serial;
304 Types.Event evt;
305 IArg arg1;
306 IArg arg2;
307 IArg arg3;
308 IArg arg4;
309 };
310
311 struct Instance_State {
312 IHeap.Handle bufHeap;
313 Entry entryArr[];
314 Entry *curEntry;
315 Entry *endEntry;
316 Entry *readEntry;
317 Bits32 serial;
318 Int16 numEntries;
319 Int8 advance;
320 Bool enabled;
321 Bool flush;
322 };
323
324 }
325 /*
326 * @(#) xdc.runtime; 2, 0, 0, 0,215; 9-3-2009 11:42:00; /db/ztree/library/trees/xdc-t57x/src/packages/
327 */
328