From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() ![]() |
Demo of Target Configuration Creation in CCSv4
Using CCStudio v4 to create a target configuration for debugging
This Flash demo shows how to create a "target configuration" in CCSv4. Such target configurations are used by CCSv4 when debugging a project.
When the demo pauses, click "Next" to continue. A table of contents at the end lets you review specific actions.
If you don't see the demo, you can download the Flash player, or save the demo to disk.
See also
RTSC+CCStudio v4 QuickStart | Using CCStudio v4 to create, build, and debug RTSC projects |
Runtime Object Viewer | Using ROV for Eclipse-Based Debugging |
Real-Time Analysis Tools | Using RTA Tools in CCSv4 |
![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved