From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC |
Config Model FAQs
General questions about the XDCtools configuration model
FAQ-080923-1 | How do I set a function configuration parameter |
FAQ-081229-1 | How can I insert my own C code into the configuration generated .c file |
FAQ-081229-2 | How do I define C language global variables within a configuration script |
[printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved