From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
C - Object count
Get the number of statically created instances
Contents |
Synopsis
| #include <«pkg»/«Mod».h> Int «Mod»_Object_count(void); |
Description
This function is automatically defined for all target modules, where «Mod» is the name of some module, and returns the number of instance objects created during configuration. This function is typically used in conjunction with «Mod»_Object_get to perform some operation at runtime on all instances created during configuration; e.g., initialization of these instances within a module's runtime startup function.
See also
C - Object_get | Get the instance handle of a statically created instance |
C - Object_first | Get the handle of the first dynamically created instance |
C - Object_next | Get the handle of the next dynamically created instance |
![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved