From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
C - Module startupDone
Query if a module's startup is complete
Contents |
Synopsis
| #include <«pkg»/«Mod».h> Bool «Mod»_Module_startupDone(void); |
Description
This function is automatically defined for all target modules and proxies, where «Mod» is the name of some module or proxy. This function is typically used in situations where the startup of one module depends upon another having completed its startup processing.
See also
xdc.runtime.Startup | Client documentation for xdc.runtime.Startup |
![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved