From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
C - Handle name
Get an instance's name
Contents |
Synopsis
| #include <«pkg»/«Mod».h> String «Mod»_Handle_name(«Mod»_Handle handle); |
Description
This function is automatically defined for all target modules that support instances, where «Mod» is the name of some module. This function returns the name of the instance object identified by handle.
See also
xdc.runtime.Types.Common$ | Client documentation for xdc.runtime.Types.Common$ |
C - create | Allocate and initialize a new instance object and return its handle |
![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved