1 /* --COPYRIGHT--,ESD
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * --/COPYRIGHT--*/
13 /*
14 * ======== ITimestampClient.xdc ========
15 *
16 *! Revision History
17 *! ================
18 *! 11-Mar-2008 agd xdc runtime review changes
19 *! 14-Dec-2007 sasa Documented parameters and retrun values
20 */
21 package xdc.runtime;
22
23 /*!
24 * ======== ITimestampClient ========
25 * Timestamp Client Interface
26 *
27 * This interface defines the methods used by client applications to
28 * get timestamp values. It is implemented by the
29 * `{@link xdc.runtime.Timestamp Timestamp}` module.
30 */
31 interface ITimestampClient {
32
33 /*!
34 * ======== get32 ========
35 * Return a 32-bit timestamp
36 *
37 * @a(returns) 38 * Returns a 32-bit timestamp value.
39 * Use `{@link #getFreq}` to convert this value into units of real time.
40 *
41 * @see #get64
42 */
43 Bits32 get32();
44
45 /*!
46 * ======== get64 ========
47 * Return a 64-bit timestamp
48 *
49 * @param(result) pointer to 64-bit result
50 *
51 * This parameter is a pointer to a structure representing a 64-bit
52 * wide timestamp value where the current timestamp is written.
53 *
54 * If the underlying hardware does not support 64-bit resolution, the
55 * `hi` field of `result` is always set to 0; see
56 * `{@link xdc.runtime.Types#Timestamp64}`. So, it is possible for
57 * the `lo` field to wrap around without any change to the `hi` field.
58 * Use `{@link #getFreq}` to convert this value into units of real
59 * time.
60 *
61 * @see #get32
62 */
63 Void get64(Types.Timestamp64 *result);
64
65 /*!
66 * ======== getFreq ========
67 * Get the timestamp timer's frequency (in Hz)
68 *
69 * @param(freq) pointer to a 64-bit result
70 *
71 * This parameter is a pointer to a structure representing a 64-bit
72 * wide frequency value where the timer's frequency (in Hz)
73 * is written; see `{@link xdc.runtime.Types#FreqHz}`.
74 * This function provides a way of converting timestamp
75 * values into units of real time.
76 *
77 * @see #get32
78 * @see #get64
79 */
80 Void getFreq(Types.FreqHz *freq);
81 }
82 /*
83 * @(#) xdc.runtime; 2, 0, 0, 0,214; 7-29-2009 14:53:44; /db/ztree/library/trees/xdc-t56x/src/packages/
84 */
85