From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
XDCscript - xdc.om.$homepkg
A model-specific home package
Synopsis
| var pkg = xdc.om.$homepkg; |
Description
Unless undefined, xdc.useModule() resolves unqualified module names within this package. The configuration model defines $homepkg as the package containing the configuration script unless explicitly overridden by a build script setting of an executable's cfgHome attribute. If the configuration script is not in any package, the $homepkg is the package containing the generated configuration files for the executable.
![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved