From RTSC-Pedia

Jump to: navigation, search
revision tip
—— LANDSCAPE orientation
[printable version]  [offline version]offline version generated on 11-Jun-2009 18:06 UTC

XDCscript - Template-Object.genStream

Generate textual output stream from a template

Contents

Synopsis

 
 
var tplt = xdc.loadTemplate(templateFile);
tplt.genStream(outStream, thisObj, args);

Parameters

outStream 
a java.io.PrintStream where all output is written and referenced within the template via $out
thisObj 
object that is referenced within the template via this
args 
array of arguments referenced within the template via $args

Description

Generates output to outStream, an instance of class java.io.PrintStream. All three parameters are passed to the underlying template generation function. This method can be recursively invoked from within a template.

See also

XDCscript - Template-Body Contents of the template file
XDCscript - Template-Object.genFile Generate textual output file from a template

[printable version]  [offline version]offline version generated on 11-Jun-2009 18:06 UTC
Copyright © 2008 The Eclipse Foundation. All Rights Reserved


Views
Personal tools
package reference