From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
XDCscript - Struct-Object.$sizeof
The target size of a structure
Contents |
Synopsis
| «tobj».$sizeof() |
Description
Returns the target size of the structure «tobj» in target chars. In other words, this function returns the same value that the target compiler would provide when applying the C sizeof() operator on the structure. Note this may be different from the number of 8-bit bytes in the structure; some target architectures have a 16-bit char.
See also
XDCscript - Typed-Object | Objects specified by the RTSC Interface Definition Language |
![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved