From RTSC-Pedia

Jump to: navigation, search
revision tip
—— LANDSCAPE orientation
[printable version]  [offline version]offline version generated on 11-Jun-2009 18:06 UTC

XDCscript - Instance-Body.instance$meta$init

Initialize a meta-only module's instance

Contents

Synopsis

 
function instance$meta$init([r1, ...])

Parameters

r1, ... 
the arguments declared in the module's create method.

Description

This function is invoked whenever a meta-only module's instance create() is called. Configuration model data can be changed as a function of the arguments passed to create().

In instance$meta$init, this is a reference to a structure containing instance configuration parameters.

For information about the order in which module and instance functions are invoked, see Creating Configurable Content.

See also

XDCscript - Instance-Body.instance$static$init Initialize a target module's instance object
Creating Configurable Content How to leverage the configuration process

[printable version]  [offline version]offline version generated on 11-Jun-2009 18:06 UTC
Copyright © 2008 The Eclipse Foundation. All Rights Reserved


Views
Personal tools
package reference