From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
ROV Module Writers Guide/Conventions and Keywords
Discussion of conventions for naming views, functions, etc.
Conventions and Keywords
There are no reserved words in ROV.
- The tabs may have any name.
- The view structures may have any name.
- The view functions may have any name.
- The module Facet configuration parameter may have any name.
The following are some recommended conventions, though.
Tab Names
- Use 'Basic' for a view of the module's instances which returns quickly
- Use 'Detailed' for a view of the module's instances which requires more time to process. Detailed views should generally include all of the fields from the 'Basic' view.
- Use 'Module' for a view of the of the module's state.
- Name data views based on what they contain, for example 'Records' or 'Buffers'.
- Display instance tabs first, followed by module tabs, and finally data tabs. For example, 'Basic', 'Detailed', 'Module', 'Records'.
View Structures
- Name the view structures after the tab names. For example, 'BasicView', 'DetailedView', 'ModuleView', 'RecordsView'
View Functions
- Give the view functions the name viewInit<tab name>. For example, 'viewInitBasic', 'viewInitDetailed', etc.
Module Facet
- Name the module facet configuration parameter 'rovViewInfo'.