TI-RTOS Drivers  tidrivers_cc13xx_cc26xx_2_16_01_13
UDMACC26XX.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
111 #ifndef ti_drivers_UDMACC26XX__include
112 #define ti_drivers_UDMACC26XX__include
113 
114 #ifdef __cplusplus
115 extern "C" {
116 #endif
117 
118 #include <stdint.h>
119 #include <stdbool.h>
120 #include "driverlib/udma.h"
121 #include "inc/hw_types.h"
122 
123 #include <ti/drivers/Power.h>
125 
136 /* Add DMACC26XX_STATUS_* macros here */
137 
150 /* Add DMACC26XX_CMD_* macros here */
151 
155 #ifndef UDMACC26XX_CONFIG_BASE
156  #define UDMACC26XX_CONFIG_BASE 0x20000400
157 #endif
158 
160 #if(UDMACC26XX_CONFIG_BASE & 0x3FF)
161  #error "Base address for DMA control table 'UDMACC26XX_CONFIG_BASE' must be 1024 bytes aligned."
162 #endif
163 
165 #if defined(__IAR_SYSTEMS_ICC__)
166 #define ALLOCATE_CONTROL_TABLE_ENTRY(ENTRY_NAME, CHANNEL_INDEX) \
167 __no_init static volatile tDMAControlTable ENTRY_NAME @ UDMACC26XX_CONFIG_BASE + CHANNEL_INDEX * sizeof(tDMAControlTable)
168 #elif defined(__TI_COMPILER_VERSION__)
169 #define ALLOCATE_CONTROL_TABLE_ENTRY(ENTRY_NAME, CHANNEL_INDEX) \
170 PRAGMA(LOCATION( ENTRY_NAME , UDMACC26XX_CONFIG_BASE + CHANNEL_INDEX * sizeof(tDMAControlTable) );)\
171 static volatile tDMAControlTable ENTRY_NAME
172 #define PRAGMA(x) _Pragma(#x)
173 #elif defined(__GNUC__)
174 #define ALLOCATE_CONTROL_TABLE_ENTRY(ENTRY_NAME, CHANNEL_INDEX) \
175  extern int UDMACC26XX_ ## ENTRY_NAME ## _is_placed; __attribute__ ((section("."#ENTRY_NAME))) static volatile tDMAControlTable ENTRY_NAME = {&UDMACC26XX_ ## ENTRY_NAME ## _is_placed}
176 #else
177 #error "don't know how to define ALLOCATE_CONTROL_TABLE_ENTRY for this toolchain"
178 #endif
179 
181 #define UDMACC26XX_SET_TRANSFER_SIZE(SIZE) (((SIZE - 1) << UDMA_XFER_SIZE_S) & UDMA_XFER_SIZE_M)
182 
183 #define UDMACC26XX_GET_TRANSFER_SIZE(CONTROL) (((CONTROL & UDMA_XFER_SIZE_M) >> UDMA_XFER_SIZE_S) + 1)
184 
188 typedef struct UDMACC26XX_Object {
189  bool isOpen;
190  ti_sysbios_family_arm_m3_Hwi_Struct hwi;
192 
196 typedef struct UDMACC26XX_HWAttrs {
197  uint32_t baseAddr;
199  uint8_t intNum;
223  uint8_t intPriority;
225 
229 typedef struct UDMACC26XX_Config {
230  void *object;
231  void const *hwAttrs;
233 
238 
239 /* Extern'd hwiIntFxn */
240 extern void UDMACC26XX_hwiIntFxn(UArg callbacks);
241 
254 __STATIC_INLINE void UDMACC26XX_init(UDMACC26XX_Handle handle)
255 {
257 
258  /* Get the pointer to the object */
259  object = handle->object;
260 
261  /* mark the module as available */
262  object->isOpen = FALSE;
263 }
264 
280 extern UDMACC26XX_Handle UDMACC26XX_open();
281 
295 __STATIC_INLINE void UDMACC26XX_channelEnable(UDMACC26XX_Handle handle, uint32_t channelBitMask)
296 {
298 
299  /* Get the pointer to the hwAttrs */
300  hwAttrs = handle->hwAttrs;
301 
302  /* Enable DMA channel */
303  HWREG(hwAttrs->baseAddr + UDMA_O_SETCHANNELEN) = channelBitMask;
304 }
305 
324 __STATIC_INLINE bool UDMACC26XX_channelDone(UDMACC26XX_Handle handle, uint32_t channelBitMask)
325 {
327 
328  /* Get the pointer to the hwAttrs */
329  hwAttrs = handle->hwAttrs;
330 
331  /* Check if REQDONE is set for a specific channel */
332  return (uDMAIntStatus(hwAttrs->baseAddr) & channelBitMask) ? true : false;
333 }
334 
352 __STATIC_INLINE void UDMACC26XX_clearInterrupt(UDMACC26XX_Handle handle, uint32_t channelBitMask)
353 {
355 
356  /* Get the pointer to the hwAttrs and object */
357  hwAttrs = handle->hwAttrs;
358 
359  /* Clear UDMA done interrupt */
360  uDMAIntClear(hwAttrs->baseAddr, channelBitMask);
361 }
362 
380 __STATIC_INLINE void UDMACC26XX_channelDisable(UDMACC26XX_Handle handle, uint32_t channelBitMask)
381 {
383 
384  /* Get the pointer to the hwAttrs and object */
385  hwAttrs = handle->hwAttrs;
386 
387  /* disable DMA channel */
388  uDMAChannelDisable(hwAttrs->baseAddr, channelBitMask);
389 }
390 
406 extern void UDMACC26XX_close(UDMACC26XX_Handle handle);
407 
408 #ifdef __cplusplus
409 }
410 #endif
411 
412 #endif /* ti_drivers_UDMACC26XX__include */
bool isOpen
Definition: UDMACC26XX.h:189
PowerCC26XX_Resource powerMngrId
Definition: UDMACC26XX.h:198
void UDMACC26XX_close(UDMACC26XX_Handle handle)
Function to close the DMA driver.
__STATIC_INLINE void UDMACC26XX_clearInterrupt(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:352
Power manager interface.
__STATIC_INLINE void UDMACC26XX_channelEnable(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:295
uint8_t intNum
Definition: UDMACC26XX.h:199
__STATIC_INLINE void UDMACC26XX_init(UDMACC26XX_Handle handle)
Function to initialize the CC26XX DMA driver.
Definition: UDMACC26XX.h:254
UDMACC26XX Global configuration.
Definition: UDMACC26XX.h:229
Power manager interface for CC26XX.
ti_sysbios_family_arm_m3_Hwi_Struct hwi
Definition: UDMACC26XX.h:190
struct UDMACC26XX_Object UDMACC26XX_Object
UDMACC26XX object.
uint8_t PowerCC26XX_Resource
Definition: PowerCC26XX.h:66
UDMACC26XX_Handle UDMACC26XX_open()
Function to initialize the CC26XX DMA peripheral.
struct UDMACC26XX_Config UDMACC26XX_Config
UDMACC26XX Global configuration.
UDMACC26XX hardware attributes.
Definition: UDMACC26XX.h:196
void * object
Definition: UDMACC26XX.h:230
uint8_t intPriority
UDMACC26XX error interrupt priority. intPriority is the DMA peripheral's interrupt priority...
Definition: UDMACC26XX.h:223
__STATIC_INLINE void UDMACC26XX_channelDisable(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:380
__STATIC_INLINE bool UDMACC26XX_channelDone(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:324
uint32_t baseAddr
Definition: UDMACC26XX.h:197
void UDMACC26XX_hwiIntFxn(UArg callbacks)
UDMACC26XX object.
Definition: UDMACC26XX.h:188
struct UDMACC26XX_Config * UDMACC26XX_Handle
A handle that is returned from a UDMACC26XX_open() call.
Definition: UDMACC26XX.h:237
void const * hwAttrs
Definition: UDMACC26XX.h:231
struct UDMACC26XX_HWAttrs UDMACC26XX_HWAttrs
UDMACC26XX hardware attributes.
Copyright 2016, Texas Instruments Incorporated