IPC API  3.40.01.08
Mx.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2012-2015, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
42 #ifndef Mx__include
43 #define Mx__include
44 
45 #include <stddef.h>
46 #include <stdint.h>
47 
48 #if defined(__cplusplus)
49 extern "C" {
50 #endif
51 
55 #define Mx_S_SUCCESS (0)
56 
60 #define Mx_E_FAIL (-1)
61 
65 typedef struct {
66  uint32_t coef;
67  int key;
68  int size;
69  uint32_t * inBuf;
70  uint32_t * outBuf;
71 } Mx_Compute;
72 
76 int Mx_initialize(UInt16 procId);
77 
81 void Mx_finalize(void);
82 
86 int32_t Mx_triple(uint32_t a);
87 
91 int32_t Mx_add(int32_t a, int32_t b);
92 
93 #if defined(IPC_BUILDOS_QNX)
94 
99 int32_t Mx_compute_QnX(Mx_Compute *compute);
100 
101 #else /* Linux */
102 
108 int32_t Mx_compute_Linux(Mx_Compute *compute, int fd, int fdIn, int fdOut);
109 
110 #endif
111 
112 #if defined(__cplusplus)
113 }
114 #endif
115 #endif /* Mx__include */
uint32_t coef
Definition: Mx.h:66
uint32_t * outBuf
Definition: Mx.h:70
Compute structure.
Definition: Mx.h:65
int32_t Mx_compute_Linux(Mx_Compute *compute, int fd, int fdIn, int fdOut)
Sample function which has pointer parameter (DMA_BUF) to a structure with two embedded pointers...
void Mx_finalize(void)
Finalize the module, must be called last.
int key
Definition: Mx.h:67
int Mx_initialize(UInt16 procId)
Initialize the module, must be called first.
int32_t Mx_triple(uint32_t a)
Sample function which multiplies argument by three.
int32_t Mx_add(int32_t a, int32_t b)
Sample function which addes two arguments.
uint32_t * inBuf
Definition: Mx.h:69
int size
Definition: Mx.h:68
Copyright 2015, Texas Instruments Incorporated