IPC API  3.40.01.08
MmServiceMgr.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2013-2014, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
43 #ifndef ti_ipc_mm_MmServiceMgr__include
44 #define ti_ipc_mm_MmServiceMgr__include
45 
46 #include <ti/grcm/RcmServer.h>
47 #include <ti/ipc/mm/MmType.h>
48 #include <ti/srvmgr/omaprpc/OmapRpc.h>
49 
50 #if defined (__cplusplus)
51 extern "C" {
52 #endif
53 
57 #define MmServiceMgr_S_SUCCESS (0)
58 
62 #define MmServiceMgr_E_FAIL (-1)
63 
64 typedef Void (*MmServiceMgr_DelFxn)(Void);
65 
70 Int MmServiceMgr_init(Void);
71 
76 Void MmServiceMgr_exit(Void);
77 
82 Int MmServiceMgr_register(const String name, RcmServer_Params *params,
83  MmType_FxnSigTab *fxnSigTab, MmServiceMgr_DelFxn delFxn);
84 
90 Int MmServiceMgr_start(const String name, Int aryLen,
91  OmapRpc_FuncSignature *sigAry);
101 UInt32 MmServiceMgr_getId();
102 
103 #if defined (__cplusplus)
104 }
105 #endif
106 #endif /* ti_ipc_mm_MmServiceMgr__include */
Int MmServiceMgr_register(const String name, RcmServer_Params *params, MmType_FxnSigTab *fxnSigTab, MmServiceMgr_DelFxn delFxn)
Register a new service.
Void MmServiceMgr_exit(Void)
Finalize the MmServiceMgr module.
Remote Command Message Server Module. An RcmServer processes inbound messages received from an RcmCli...
UInt32 MmServiceMgr_getId()
Get the ID of the current service instance This function can only be called in the context of skeleto...
Void(* MmServiceMgr_DelFxn)(Void)
Definition: MmServiceMgr.h:64
Function Signature Table.
Definition: MmType.h:126
Int MmServiceMgr_init(Void)
Initialize the MmServiceMgr module.
Specific types to support the MmRpc and MmServiceMgr modules.
RcmServer Instance create parameters.
Definition: RcmServer.h:281
Copyright 2015, Texas Instruments Incorporated