43 #ifndef MxServer__include
44 #define MxServer__include
49 #if defined(__cplusplus)
56 #define MxServer_S_SUCCESS (0)
61 #define MxServer_E_FAIL (-1)
91 #if defined(__cplusplus)
uint32_t * outBuf
Definition: MxServer.h:71
int size
Definition: MxServer.h:69
int32_t MxServer_add(int32_t a, int32_t b)
Sample function which addes two arguments.
uint32_t * inBuf
Definition: MxServer.h:70
int key
Definition: MxServer.h:68
int32_t MxServer_triple(uint32_t a)
Sample function which multiplies argument by three.
Compute structure.
Definition: MxServer.h:66
uint32_t coef
Definition: MxServer.h:67
int32_t MxServer_compute(MxServer_Compute *compute)
Sample function which has pointer parameter to a structure with two embedded pointers.