![]() |
![]() |
IPC 1.25.01.09 is an GA release of IPC
Interprocess communication mechanisms including message passing, streams, and linked lists, which work transparently in both uniprocessor and muiltiprocessor configurations.
The IPC product is comprised of the following main packages
The following documentation is available:
User Install Guide | |
User Guide (SPRUGO6E) | |
Doxygen API guide | Documents runtime-APIs, type definitions, error codes and constants |
Cdoc API guide | Documents config-time (RTSC) APIs, Asserts and Errors; Indexed and searchable within CCS/Eclipse |
Static Analysis Reports |
Manifest and License:
IPC Software Manifest and License
Release notes from previous releases are also available in the relnotes_archive directory.
Changes since IPC 1.25.00:
SDOCM00078115 | Ipc_readConfig does not free shared memory for the entry after returning it to the user |
SDOCM00078946 | write test cases to look for IPC memory leaks |
SDOCM00085207 | Ipc_stop not supported on all-bios system |
SDOCM00095908 | IPC does not allow single core Stellaris parts to be specified |
SDOCM00095961 | IPC: pre-built instrumented and nonInstrumented library build flows have a flaw in their makefile dependencies |
SDOCM00096267 | Memory leak in Ipc_attach() and Ipc_detach() loop |
SDOCM00096667 | Bug in GateHWSem_getReservedMask() |
SDOCM00096671 | Look at removing restriction of limiting cache invalidates to one core at a time |
SDOCM00097085 | Source files *.c and *.cfg missing from ti/sdo/ipc/examples/multicore |
For information on enhancements and defect fixes in earlier releases, please refer to the release notes from previous releases that are available in the relnotes_archive directory.
Interface/API changes:
No APIs or shared memory interfaces were changed in this release. However, this release requires new SYS/BIOS, XDC, and CCS components as described in the dependency section below.
This release supports the following operating systems:
This release requires the following other software components and tools versions to successfully function:
No known issues
All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 1.21.00.01_eng).
This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. ipc_1_21_00_01.
Subsequent releases of patch upgrades will be identified by the patch number, ex. IPC 1.21.00.01 with directory ipc_1_21_00_01. Typically, these patches only include critical bug fixes.
Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.
For technical support, use the community forum TI E2E Community, or email softwaresupport@ti.com.
Last updated: November 07, 2012