![]() |
![]() |
IPC 1.24.03.32 is an GA release of IPC
Interprocess communication mechanisms including message passing, streams, and linked lists, which work transparently in both uniprocessor and muiltiprocessor configurations.
The IPC product is comprised of the following main packages
The following documentation is available:
User Install Guide | |
User Guide (SPRUGO6D) | |
Doxygen API guide | Documents runtime-APIs, type definitions, error codes and constants |
Cdoc API guide | Documents config-time (RTSC) APIs, Asserts and Errors; Indexed and searchable within CCS/Eclipse |
Static Analysis Reports |
Manifest and License:
IPC Software Manifest and License
Release notes from previous releases are also available in the relnotes_archive directory.
Changes since IPC 1.24.02:
SDOCM00089985 | Run Coverity static code analysis tool and save report to the project page to archive the results |
SDOCM00089989 | add examples for CentEVE -- need examples for all cores including the new ARP32 |
SDOCM00090001 | move arp32 libraries into the c6000 product/install .zip file like BIOS (currently in base.zip) |
SDOCM00090050 | add support for Keystone2 devices (see similar bug filed against BIOS) |
SDOCM00090448 | add API.html (match name from SYS/BIOS) to help users find API documentation (see latest SYS/BIOS) |
SDOCM00090450 | update IPC's cdoc to have better page title (instead of RTSC Package Documenation) (see latest SYS/BIOS) |
SDOCM00090802 | update IPC/C6x code to fix a few Coverity findings |
SDOCM00091799 | Incorrect documentation for List_dequeue |
SDOCM00092486 | Cache invalidate bug in HeapMemMP_free(). |
For information on enhancements and defect fixes in earlier releases, please refer to the release notes from previous releases that are available in the relnotes_archive directory.
Interface/API changes:
SharedRegion_DEFAULTOWNERID has been removed from the SharedRegon common header file, ti/ipc/SharedRegion.h (SDOCM00083271). Applications referencing this value should use MultiProc_INVALIDID instead (defined in ti/ipc/MultiProc.h).
Most of the APIs in IPC 1.24 are compatible with IPC 1.22/1.23. However, code using IPC 1.22/1.23 will have to be recompiled for use with IPC 1.24.00. You must recompile -- relink will not work.
ti.sdo.ipc.* and ti.sdo.utils.* APIs in the IPC 1.2X.XX.XX releases are not compatible with those in the IPC 1.00.0X.XX (GA) release. These APIs have been updated to be consistent with the Linux APIs to share common header files in ti/ipc/. However, APIs in the ti.sdo.io package have not changed since the 1.00 GA release.
OMAP3530 Mailbox assignments swapped
In previous IPC releases, Mailbox 0 was used for DSP-to-ARM notifications and 1 was used for ARM-to-DSP communication. This has been swapped as of IPC 1.22.02. In order for ARM-DSP notifications to work, both the ARM and the DSP must use the same mailbox assignments.
DM8168 MultiProc name changesThis release supports the following operating systems:
This release requires the following other software components and tools versions to successfully function:
No known issues
All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 1.21.00.01_eng).
This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. ipc_1_21_00_01.
Subsequent releases of patch upgrades will be identified by the patch number, ex. IPC 1.21.00.01 with directory ipc_1_21_00_01. Typically, these patches only include critical bug fixes.
Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.
For technical support, use the community forum TI E2E Community, or email softwaresupport@ti.com.
Last updated: May 22, 2012