This is a engineering release of IPC 1.20
Interprocess communication mechanisms including message passing, streams, and linked lists, which work transparently in both uniprocessor and muiltiprocessor configurations.
The IPC product is comprised of three main packages
The following documentation is available:
User Install Guide | |
User Guide (SPRUGO6A) | |
Doxygen API guide | Documents runtime-APIs, type definitions, error codes and constants |
Cdoc API guide | Documents config-time (RTSC) APIs, Asserts and Errors |
Release notes from previous releases are also available in the relnotes_archive directory.
1.20.00.21 Engineering Release (this release)
This is an Early Adopter Release of IPC 1.20. This release should be used for evaluation and early development only. It will not be supported once the official IPC 1.20 GA release is available (April timeframe). Only minor, if any, API changes will occur between this release and the GA release.
The IPC User's Guide examples and code samples are slightly out of synch with the APIs in this version of the software. The documentation available via the 'cdoc' documentation and CCSv4 Help are accurate and should be used as reference. User code should use the APIs defined by the headers in /docs/doxygen/html/index.html
For information on enhancements and defect fixes in earlier releases, please refer to the release notes from previous releases that are available in the relnotes_archive directory.
Interface/API changes: This release is not compatible with IPC 1.00.0X.XX (GA) release. The APIs have been updated to be consistent with the Linux APIs to share common header files in ti/ipc/. Source files that use IPC 1.00 will have to be reviewed and updated.
This release supports the following hosts:
Windows XP SP2/SP3
Windows Vista
Linux (Redhat 4 and 5)
This release requires the following other software components and tools versions to successfully function:
ID | Headline |
All releaseshave 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 1.20.00.01_eng).
This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. ipc_1_20_00_01.
Subsequent releases of patch upgrades will be identified by the patch number, ex. IPC 1.20.00.01 with directoryipc_1_20_00_01. Typically, these patches only include critical bug fixes.
Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.
For technical support, contact softwaresupport@ti.com
Last updated: April 01, 2010