config TransportNullSetup_priority // module-wide |
|
priority of the transport
extern const UInt TransportNullSetup_priority;
TransportNullSetup_attach() // module-wide |
|
Function that will be called in MessageQ_attach
Int TransportNullSetup_attach(UInt16 remoteProcId, Ptr sharedAddr);
TransportNullSetup_detach() // module-wide |
|
Function that will be called in MessageQ_detach
Int TransportNullSetup_detach(UInt16 remoteProcId);
TransportNullSetup_isRegistered() // module-wide |
|
Determines if a transport has been registered to a remote processor
Bool TransportNullSetup_isRegistered(UInt16 remoteProcId);
TransportNullSetup_sharedMemReq() // module-wide |
|
Shared memory required
SizeT TransportNullSetup_sharedMemReq(Ptr sharedAddr);
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool TransportNullSetup_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool TransportNullSetup_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 TransportNullSetup_Module_getMask();
// Returns the diagnostics mask for this module
Void TransportNullSetup_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module