struct InterruptHost_IntInfo |
|
typedef struct InterruptHost_IntInfo {
UInt localIntId;
UInt remoteIntId;
UInt intVectorId;
} InterruptHost_IntInfo;
InterruptHost_intClear() // module-wide |
|
Clear interrupt
ARGUMENTS
remoteProcId
Remote MultiProc Id
intInfo
Information needed to configure interrupt line
RETURNS
Value (if any) of the interrupt before
it was cleared
InterruptHost_intDisable() // module-wide |
|
Disables the interrupt corresponding to intId
ARGUMENTS
remoteProcId
Remote MultiProc Id
intInfo
Information needed to configure interrupt line
InterruptHost_intEnable() // module-wide |
|
Enables the interrupt corresponding to intId
ARGUMENTS
remoteProcId
Remote MultiProc Id
intInfo
Information needed to configure interrupt line
InterruptHost_intRegister() // module-wide |
|
Register an interrupt line to a remote processor
Void InterruptHost_intRegister(
UInt16 remoteProcId,
IInterrupt_IntInfo *
intInfo,
Fxn func,
UArg arg);
ARGUMENTS
remoteProcId
Remote MultiProc Id
intInfo
Information needed to configure interrupt line
func
Function to register.
arg
Argument that will be passed to func
InterruptHost_intSend() // module-wide |
|
Send interrupt to the remote processor
ARGUMENTS
remoteProcId
Remote MultiProc Id
intInfo
Information needed to configure interrupt line
arg
Argument for sending interrupt.
InterruptHost_intUnregister() // module-wide |
|
Unregister an interrupt line to a remote processor
ARGUMENTS
remoteProcId
Remote MultiProc Id
intInfo
Information needed to configure interrupt line
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool InterruptHost_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool InterruptHost_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 InterruptHost_Module_getMask();
// Returns the diagnostics mask for this module
Void InterruptHost_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module