metaonly module ti.sdo.io.driverTemplate.Main |
 |
Generate driver starter files
This command line tool helps driver writers by generating starter
files. The driver writer can then fill in driver specific code
and rebuild.
[
more ... ]
var Main = xdc.useModule('ti.sdo.io.driverTemplate.Main');
module-wide config parameters
'-m modName -o outputDir',
'[--help]'
];
module-wide functions
per-instance config parameters
DETAILS
This command line tool helps driver writers by generating starter
files. The driver writer can then fill in driver specific code
and rebuild.
required arguments are the output directory name "-o" and the module
name "-m".
The name of the module and the package name is derived from the module
name. For e.g for -m drivers.io.Uart the module name is Uart and the
package name is drivers.dma.
The "-o" option must inlcude package path. For the example above
-o "C:\Product\drivers\dma.
config Main.usage // module-wide |
 |
XDCscript usage |
meta-domain |
Main.usage = String[] [
'-m modName -o outputDir',
'[--help]'
];
Main.main() // module-wide |
 |
main() function, invoked from the command line
XDCscript usage |
meta-domain |
Main.main(String[] arguments) returns Int
DETAILS
Parses command line arguments then calls
mkpkg().
Instance Config Parameters |
 |
XDCscript usage |
meta-domain |
var params = new Main.Params;
// Instance config-params object
params.arguments = Any[] undefined;
// Positional parameters
params.input = String undefined;
//
params.inputPath = String undefined;
//
params.modName = String undefined;
// Name of the generated module. You need to specify package name within
the modName
params.output = String undefined;
// Output file or directory
params.preserveModTime = Bool false;
// Only modify the timestamps of output files whose contents changed
config Main.arguments // instance |
 |
Positional parameters
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.arguments = Any[] undefined;
config Main.input // instance |
 |
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
const params.input = String computed value;
config Main.inputPath // instance |
 |
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
const params.inputPath = String computed value;
config Main.modName // instance |
 |
Name of the generated module. You need to specify package name within
the modName
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.modName = String undefined;
config Main.output // instance |
 |
Output file or directory
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.output = String undefined;
config Main.preserveModTime // instance |
 |
Only modify the timestamps of output files whose contents changed
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.preserveModTime = Bool false;
DETAILS
This flag changes the behavior of mkpkg in the case when some
of the output files already exists, in particular from a previous
invocation of mkpkg. If true, any output file that already
exists will only be touched if its contents must change.
If the new content is identical, then the timestamp on the
file remains unmodified.
This is an optimization that can improve the behavior of
mkpkg when used with programs like "make" that are sensitive
to file timestamps.
generated on Sat, 11 Feb 2012 00:37:42 GMT