1    /* --COPYRIGHT--,BSD
     2     * Copyright (c) $(CPYYEAR), Texas Instruments Incorporated
     3     * All rights reserved.
     4     *
     5     * Redistribution and use in source and binary forms, with or without
     6     * modification, are permitted provided that the following conditions
     7     * are met:
     8     *
     9     * *  Redistributions of source code must retain the above copyright
    10     *    notice, this list of conditions and the following disclaimer.
    11     *
    12     * *  Redistributions in binary form must reproduce the above copyright
    13     *    notice, this list of conditions and the following disclaimer in the
    14     *    documentation and/or other materials provided with the distribution.
    15     *
    16     * *  Neither the name of Texas Instruments Incorporated nor the names of
    17     *    its contributors may be used to endorse or promote products derived
    18     *    from this software without specific prior written permission.
    19     *
    20     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
    21     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
    22     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
    23     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
    24     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
    25     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
    26     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
    27     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
    28     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
    29     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
    30     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    31     * --/COPYRIGHT--*/
    32    /*
    33     *  ======== SharedRegion.xdc ========
    34     *
    35     *! Revision History
    36     *! ================
    37     *! 23-Mar-2010 skp     cdoc updates
    38     *! 02-Oct-2009 jv      Added cacheEnable, cacheAlign flags, rename
    39     *!                     Info to TableEntry, add support for single image.
    40     *! 05-Jun-2009 jv      Implement code review comments
    41     *! 20-Mar-2009 jv      change the types for meta function so they work.
    42     *! 05-Feb-2009 jv      Applied code review comments.
    43     *! 29-Nov-2009 jv      Copy from interface to here. Add Info functions.
    44     *! 20-Nov-2008 jv      Created from design review.
    45     */
    46    
    47    package ti.sdo.ipc;
    48    
    49    import xdc.runtime.Error;
    50    import xdc.runtime.IHeap;
    51    import xdc.rov.ViewInfo;
    52    
    53    /*!
    54     *  ======== SharedRegion ========
    55     *  Shared memory manager and address translator.
    56     *
    57     *  @p(html)
    58     *  This module has a common header that can be found in the {@link ti.ipc}
    59     *  package.  Application code should include the common header file (not the
    60     *  RTSC-generated one):
    61     *
    62     *  <PRE>#include &lt;ti/ipc/SharedRegion.h></PRE>
    63     *
    64     *  The RTSC module must be used in the application's RTSC configuration file
    65     *  (.cfg) if runtime APIs will be used in the application:
    66     *
    67     *  <PRE>SharedRegion = xdc.useModule('ti.sdo.ipc.SharedRegion');</PRE>
    68     *
    69     *  Documentation for all runtime APIs, instance configuration parameters,
    70     *  error codes macros and type definitions available to the application
    71     *  integrator can be found in the
    72     *  <A HREF="../../../../doxygen/html/files.html">Doxygen documenation</A>
    73     *  for the IPC product.  However, the documentation presented on this page
    74     *  should be referred to for information specific to the RTSC module, such as
    75     *  module configuration, Errors, and Asserts.
    76     *  @p
    77     *
    78     *  The SharedRegion module is designed to be used in a multi-processor
    79     *  environment in which memory regions are shared and accessed
    80     *  across different processors. The module itself does not use any shared
    81     *  memory, because all module state is stored locally.  SharedRegion
    82     *  APIs use the system gate for thread protection.
    83     *
    84     *  This module creates and stores a local shared memory region table.  The
    85     *  table contains the processor's view for every shared region in the system.
    86     *  The table must not contain any overlapping regions.  Each processor's
    87     *  view of a particular shared memory region is determined by the region id.
    88     *  In cases where a processor cannot access a certain shared memory region,
    89     *  that shared memory region should be left invalid for that processor.
    90     *  Note:  The {@link #numEntries} must be the same on all processors.
    91     *
    92     *  Each shared region contains the following:
    93     *  @p(blist)
    94     *  -base:          The base address
    95     *  -len:           The length
    96     *  -name:          The name of the region
    97     *  -isValid:       Whether the region is valid
    98     *  -ownerProcId:   The id of the processor which owns the region
    99     *  -cacheEnable:   Whether the region is cacheable
   100     *  -cacheLineSize: The cache line size
   101     *  -createHeap:    Whether a heap is created for the region.
   102     *  @p
   103     *
   104     *  A region is added statically using the {@link #setEntryMeta} API.
   105     *  The length of a region must be the same across all processors.
   106     *  The owner of the region can be specified.  If specified, the owner
   107     *  manages the shared region.  It creates a HeapMemMP instance which spans
   108     *  the full size of the region.  The other processors open the same HeapMemMP
   109     *  instance.
   110     *
   111     *  An example of a SharedRegion configuration is as follows:
   112     *
   113     *  @p(code)
   114     *
   115     * var SharedRegion = xdc.useModule('ti.sdo.ipc.SharedRegion');
   116     * SharedRegion.setEntryMeta(0,
   117     *     { base: 0x80000000,
   118     *       len: 0x20000,
   119     *       ownerProcId: 0,
   120     *       isValid: true,
   121     *       cacheLineSize: 64,
   122     *       name: "DDR2",
   123     *     });
   124     *
   125     *  @p
   126     *
   127     *  The shared region table along with a shared region pointer (SRPtr)
   128     *  is used to do address translation at runtime. The shared region
   129     *  pointer is a 32-bit portable pointer composed of an id and offset.
   130     *  The most significant bits of a SRPtr are used for the id.
   131     *  The id corresponds to the index of the entry in the table.
   132     *  The offset is the offset from the base of the shared memory region.
   133     *  The number of entries in the table determines the number of bits to
   134     *  use for the id.  Increasing the number of entries increases the
   135     *  range of ids but decreases the range of the offset.
   136     *
   137     *  Note:  Region 0 must be visible by all processors.  Region 0 is used for
   138     *         synchonizing the processors, creating the default GateMP, and
   139     *         creating Notify and MessageQ transport instances.  The HeapMemMP
   140     *         created in Region 0 is the length of the region minus memory
   141     *         reserved for creating these internal instances.
   142     *
   143     *  Refer to the doxygen documentation for run-time API documenation.
   144     *
   145     */
   146    
   147    module SharedRegion
   148    {
   149        /*!
   150         *  ======== RegionView ========
   151         *  @_nodoc
   152         */
   153        metaonly struct RegionView {
   154            String       base;
   155            String       end;
   156            String       len;
   157            UInt16       ownerProcId;
   158            Bool         cacheEnable;
   159            Bool         isValid;
   160            UInt16       cacheLineSize;
   161            SizeT        reservedSize;
   162            Ptr          heap;
   163            String       name;
   164        };
   165    
   166        /*!
   167         *  ======== rovViewInfo ========
   168         *  @_nodoc
   169         */
   170        @Facet
   171        metaonly config xdc.rov.ViewInfo.Instance rovViewInfo =
   172            xdc.rov.ViewInfo.create({
   173                viewMap: [
   174                    ['Regions',
   175                        {
   176                            type: xdc.rov.ViewInfo.MODULE_DATA,
   177                            viewInitFxn: 'viewInitRegions',
   178                            structName: 'RegionView'
   179                        }
   180                    ]
   181                ]
   182            });
   183    
   184        /*!
   185         *  Definition of shared region pointer type
   186         */
   187        typedef Bits32 SRPtr;
   188    
   189        /*!
   190         *  Assert raised when the id is larger than numEntries.
   191         */
   192        config xdc.runtime.Assert.Id A_idTooLarge =
   193            {msg: "A_idTooLarge: id cannot be larger than numEntries"};
   194    
   195        /*!
   196         *  Assert raised when an address is out of the range of the region id.
   197         */
   198        config xdc.runtime.Assert.Id A_addrOutOfRange =
   199            {msg: "A_addrOutOfRange: Address is out of region id's range"};
   200    
   201        /*!
   202         *  Assert raised when attempting to clear region 0
   203         */
   204        config xdc.runtime.Assert.Id A_region0Clear =
   205            {msg: "A_region0Clear: Region 0 cannot be cleared"};
   206    
   207        /*!
   208         *  Assert raised when region zero is invalid
   209         */
   210        config xdc.runtime.Assert.Id A_region0Invalid =
   211            {msg: "A_region0Invalid: Region zero is invalid"};
   212    
   213        /*!
   214         *  Assert raised when region is invalid
   215         */
   216        config xdc.runtime.Assert.Id A_regionInvalid =
   217            {msg: "A_regionInvalid: Region is invalid"};
   218    
   219        /*!
   220         *  Assert raised when the trying to reserve too much memory.
   221         */
   222        config xdc.runtime.Assert.Id A_reserveTooMuch =
   223            {msg: "A_reserveTooMuch: Trying to reserve too much memory"};
   224    
   225        /*!
   226         *  Assert raised when cache enabled but cache line size = 0.
   227         */
   228        config xdc.runtime.Assert.Id A_cacheLineSizeIsZero =
   229            {msg: "A_cacheLineSizeIsZero: cache line size cannot be zero"};
   230    
   231        /*!
   232         *  Assert raised when a new entry overlaps an existing one.
   233         */
   234        config xdc.runtime.Assert.Id A_overlap  =
   235            {msg: "A_overlap: Shared region overlaps"};
   236    
   237        /*!
   238         *  Assert raised when a valid table entry already exists.
   239         */
   240        config xdc.runtime.Assert.Id A_alreadyExists =
   241            {msg: "A_alreadyExists: Trying to overwrite an existing valid entry"};
   242    
   243        /*!
   244         *  Assert raised when trying to use a heap for a region that has no heap
   245         */
   246        config xdc.runtime.Assert.Id A_noHeap =
   247            {msg: "A_noHeap: Region has no heap"};
   248    
   249        /*!
   250         *  ======== Entry ========
   251         *  Structure for specifying a region.
   252         *
   253         *  Each region entry should not overlap with any other entry.  The
   254         *  length of a region should be the same across all processors.
   255         *
   256         *  During static configuration, the 'isValid' field can be set to 'false'
   257         *  to signify a partially completed entry.  This should only be done
   258         *  if the base address of the entry is not known during static
   259         *  configuration.  The entry can be completed and the
   260         *  'isValid' field can be set to true at runtime.
   261         *
   262         *  @field(base)          The base address.
   263         *  @field(len)           The length.
   264         *  @field(ownerProcId)   MultiProc id of processor that manages region.
   265         *  @field(isValid)       Whether the region is valid or not.
   266         *  @field(cacheEnable)   Whether the region is cacheable.
   267         *  @field(cacheLineSize) The cache line size for the region.
   268         *  @field(createHeap)    Whether a heap is created for the region.
   269         *  @field(name)          The name associated with the region.
   270         */
   271        struct Entry {
   272            Ptr    base;
   273            SizeT  len;
   274            UInt16 ownerProcId;
   275            Bool   isValid;
   276            Bool   cacheEnable;
   277            SizeT  cacheLineSize;
   278            Bool   createHeap;
   279            String name;
   280        };
   281    
   282        /*! Specifies the invalid id */
   283        const UInt16 INVALIDREGIONID = 0xFFFF;
   284    
   285        /*! Specifies the default owner proc id */
   286        const UInt16 DEFAULTOWNERID = ~0;
   287    
   288        /*!
   289         *  Worst-case cache line size
   290         *
   291         *  This is the default system cache line size for all modules.
   292         *  When a module puts structures in shared memory, this value is
   293         *  used to make sure items are aligned on a cache line boundary.
   294         *  If no cacheLineSize is specified for a region, it will use this
   295         *  value.
   296         */
   297        config SizeT cacheLineSize = 128;
   298    
   299        /*!
   300         *  The number of shared region table entries.
   301         *
   302         *  This value is used for calculating the number of bits for the offset.
   303         *  Note: This value must be the same across all processors in the system.
   304         *        Increasing this parameter will increase the footprint and
   305         *        the time for translating a pointer to a SRPtr.
   306         */
   307        config UInt16 numEntries = 4;
   308    
   309        /*!
   310         *  Determines whether address translation is required.
   311         *
   312         *  This configuration parameter should be set to 'false' if and only if all
   313         *  shared memory regions have the same base address for all processors.
   314         *  If 'false', it results in a fast {@link #getPtr} and {@link #getSRPtr},
   315         *  because a SRPtr is equivalent to a Ptr and no translation is done.
   316         */
   317        config Bool translate = true;
   318    
   319        /*! @_nodoc
   320         *  Value that corresponds to NULL in SRPtr address space.
   321         */
   322        config SRPtr INVALIDSRPTR = 0xFFFFFFFF;
   323    
   324        /*! @_nodoc
   325         *  ======== attach ========
   326         *  Opens a heap, for non-owner processors, for each SharedRegion.
   327         *
   328         *  Function is called in Ipc_attach().
   329         */
   330        Int attach(UInt16 remoteProcId);
   331    
   332        /*! @_nodoc
   333         *  ======== clearReservedMemory ========
   334         *  Clears the reserve memory for each region in the table.
   335         */
   336        Void clearReservedMemory();
   337    
   338        /*!
   339         *  ======== getCacheLineSizeMeta ========
   340         *  Meta version of Ipc_getCacheLineSize
   341         */
   342        metaonly SizeT getCacheLineSizeMeta(UInt16 id);
   343    
   344        /*! @_nodoc
   345         *  ======== getIdMeta ========
   346         *  Returns the region id for a given local address
   347         *
   348         *  @param(addr)    Address to retrieve the shared region pointer.
   349         *
   350         *  @b(returns)     region id
   351         */
   352        metaonly UInt16 getIdMeta(Ptr addr);
   353    
   354        /*! @_nodoc
   355         *  ======== getPtrMeta ========
   356         *  Meta version of {@link #getPtr}
   357         */
   358        metaonly Ptr getPtrMeta(SRPtr srptr);
   359    
   360        /*! @_nodoc
   361         *  ======== getPtrMeta$view ========
   362         *  ROV-time version of getPtrMeta
   363         *
   364         *  @param(srptr)   Shared region pointer.
   365         *
   366         *  @b(returns)     Pointer associated with shared region pointer.
   367         */
   368        metaonly Ptr getPtrMeta$view(SRPtr srptr);
   369    
   370        /*! @_nodoc
   371         *  ======== getSRPtrMeta ========
   372         *  Meta version of {@link #getSRPtr}
   373         */
   374        metaonly SRPtr getSRPtrMeta(Ptr addr);
   375    
   376        /*! @_nodoc
   377         *  ======== getSRPtrMeta$view ========
   378         *  ROV-time version of getSRPtrMeta
   379         *
   380         *  @param(addr)    Address to retrieve the shared region pointer.
   381         *
   382         *  @b(returns)     Shared region pointer.
   383         */
   384        metaonly SRPtr getSRPtrMeta$view(Ptr addr);
   385    
   386        /*! @_nodoc
   387         *  ======== isCacheEnabledMeta ========
   388         *  Meta version of {@link #isCacheEnabled}
   389         */
   390        metaonly Bool isCacheEnabledMeta(UInt16 id);
   391    
   392        /*! @_nodoc
   393         *  ======== reserveMemory ========
   394         *  Reserves the specified amount of memory from the specified region id.
   395         *
   396         *  Must be called before Ipc_start().  The amount of memory reserved
   397         *  must be the same on all cores.
   398         *  The return pointer is the starting address that was reserved.
   399         *
   400         *  @param(id)      Region id.
   401         *  @param(size)    Amount of memory to reserve.
   402         *
   403         *  @b(returns)     Starting address of memory reserved.
   404         */
   405        Ptr reserveMemory(UInt16 id, SizeT size);
   406    
   407        /*!
   408         *  ======== setEntryMeta ========
   409         *  Sets the entry at the specified region id in the shared region table.
   410         *
   411         *  The required parameters are base and len. All the other fields will
   412         *  get their default if not specified.
   413         *
   414         *  @param(id)          Region id.
   415         *  @param(entry)       Entry fields about the region.
   416         */
   417        metaonly Void setEntryMeta(UInt16 id, Entry entry);
   418    
   419        /*! @_nodoc
   420         *  ======== start ========
   421         *  Creates a heap by owner of region for each SharedRegion.
   422         *
   423         *  Function is called by Ipc_start().  Requires that SharedRegion 0
   424         *  be valid before calling start().
   425         */
   426        Int start();
   427    
   428    
   429    internal:
   430    
   431        const UInt32 CREATED = 0x08111963;
   432    
   433        /* Information stored on a per region basis */
   434        struct Region {
   435            Entry        entry;
   436            SizeT        reservedSize;
   437            IHeap.Handle heap;
   438        };
   439    
   440        /* Temporary storage of shared regions */
   441        metaonly config Entry entry[];
   442    
   443        /* internal to keep track of the number of entries added */
   444        metaonly config UInt entryCount;
   445    
   446        /* number of bits for the offset for a SRPtr. This value is calculated */
   447        config UInt32 numOffsetBits;
   448    
   449        /* offset bitmask using for generating a SRPtr */
   450        config UInt32 offsetMask;
   451    
   452        /*
   453         *  ======== checkOverlap ========
   454         *  Determines if there is an overlap with an existing entry
   455         *
   456         *  @param(base)    Base address of the region
   457         *  @param(len)     Size of the region
   458         *
   459         *  @b(returns)     Status if successful or not.
   460         */
   461        Int checkOverlap(Ptr base, SizeT len);
   462    
   463        /*
   464         *  ======== Module State structure ========
   465         *  The regions array contains information for each shared region entry.
   466         *  The size of the table will be determined by the number of entries.
   467         */
   468        struct Module_State {
   469            Region      regions[];
   470        };
   471    }
   472