package ti.ipc    

Inter processor communication common headers

This is a package that serves as a container for common header files for various IPC modules supplied with the IPC product. [ more ... ]
XDCspec declarations sourced in ti/ipc/package.xdc
package ti.ipc [1, 0, 0, 0] {
 
}
DETAILS
This is a package that serves as a container for common header files for various IPC modules supplied with the IPC product.
Documentation for all runtime APIs, instance configuration parameters, error codes macros and type definitions available to the application integrator can be found in the Doxygen documenation for the IPC product. However, the documentation presented in RTSC cdoc should be referred to for information specific to the RTSC module, such as module configuration, Errors, and Asserts.
The following table shows a list of all IPC modules that have common header files. Follow the corresponding links for doxygen or cdoc documentation for each of the modules.
GateMP Multiple processor gate that provides local and remote context protection Doxygen cdoc
HeapBufMP Multi-processor fixed-size buffer heap Doxygen cdoc
HeapMemMP Multi-processor variable size buffer heap Doxygen cdoc
HeapMultiBufMP Multiple fixed size buffer heap Doxygen cdoc
HeapQueueMgr Multi-processor fixed-size buffer heap using hardware queues Doxygen cdoc
Ipc Ipc Manager Doxygen cdoc
ListMP Multiple processor shared memory list Doxygen cdoc
MessageQ Message-passing with queuing Doxygen cdoc
MultiProc Processor id manager Doxygen cdoc
NameServer Name manager Doxygen cdoc
Notify Notification manager for IPC Doxygen cdoc
SharedRegion Shared memory manager and address translator Doxygen cdoc
generated on Tue, 10 Aug 2010 00:54:49 GMT