![]() |
![]() |
|
Framework Components Application Programming Interface (API)
fc-v04
|
ECPY Definitions - High performance functional library for use with the EDMA3 DMA peripheral. Provides a comprehensive list of DMA operations an algorithm can perform on logical DMA channels it acquires through the IRES_EDMA3CHAN protocol.
The non-direct APIs are slightly easier to use and maintain state and persistence of 1st transfer's settings across transfers.
It is important to not mix and match direct and non-direct functions for any given channel, as this may result in unexpected behavior.
#include <ti/sdo/fc/ires/edma3chan/ires_edma3Chan.h>

Go to the source code of this file.
Functions | |
| Void | ECPY_configure (ECPY_Handle handle, ECPY_Params *restrict params, short transferNo) |
| Configures the DMA transfer settings for the transfer=transferNo of the logical channel. Except for transferNo==1, the physical EDMA3 PaRAM associated with the transfer is modified. For transferNo==1 a "shadow" of the PaRAM registers gets configured, so that the configuration of 1st transfer remains persistent following ECPY_startEdma() calls. More... | |
| Void | ECPY_directConfigure (ECPY_Handle handle, ECPY_Params *restrict params, short transferNo) |
| Configure the DMA transfer settings of handle's 'transferNo' transfer. This function always directly configures the physical EDMA3 PaRAM associated with the transfer. Since no shadow is used for the 1st transfer, the configuration settings of the 1st transfer gets lost following linked transfers or when the 1st transfer is a 3D transfer (numFrames > 1). More... | |
| Void | ECPY_configure16 (ECPY_Handle handle, ECPY_ParamField16b fieldId, unsigned short value, short transferNo) |
| Modify the 16-bit DMA transfer parameter, indicated by the parameter field id, fieldId, of the current channel settings. More... | |
| Void | ECPY_directConfigure16 (ECPY_Handle handle, ECPY_ParamField16b fieldId, unsigned short value, short transferNo) |
| Modify the 16-bit DMA transfer parameter, indicated by the parameter field id, fieldId, of the current channel settings. This function always directly configures the physical EDMA3 PaRAM's 16-bit half of the 32-bit registered associated with the transfer & field . No shadow is used. More... | |
| Void | ECPY_configure32 (ECPY_Handle handle, ECPY_ParamField32b fieldId, unsigned int value, short transferNo) |
| Modify the 32-bit DMA transfer parameter, indicated by the parameter field id, fieldId, of the current channel settings. More... | |
| Void | ECPY_directConfigure32 (ECPY_Handle handle, ECPY_ParamField32b fieldId, unsigned int value, short transferNo) |
| Modify the 32-bit DMA transfer parameter, indicated by the parameter field id, fieldId, of the current channel settings. More... | |
| Void | ECPY_setFinal (ECPY_Handle handle, short transferNo) |
| Indicate that a given transfer will be the last in a sequence of linked transfers. More... | |
| Void | ECPY_directSetFinal (ECPY_Handle handle, short transferNo) |
| Indicate that a given transfer will be the last in a sequence of linked transfers. More... | |
| Void | ECPY_setDestinationMemoryMode (ECPY_Handle handle, short mode) |
| Indicate the memory space that DMA transfers submitted to the channel associated with the handle will modify. This information can be used for channel to TC Queue mapping for avoiding known Silicon GEM lockup issues or for performance improvements. More... | |
| Void | ECPY_start (ECPY_Handle handle) |
| Submit a single or linked transfer using the most recently configured transfer parameter settings. More... | |
| Void | ECPY_directStartEdma (ECPY_Handle handle) |
| Submit a single or linked transfer using the most recently 'direct' configured transfer parameter settings. More... | |
| Void | ECPY_directStartQdma (ECPY_Handle handle) |
| ECPY_directStartQdma has not been implemented. More... | |
| Void | ECPY_wait (ECPY_Handle handle) |
| Wait for all data transfers on a logical channel to complete. More... | |
| Void | ECPY_directWait (ECPY_Handle handle) |
| Wait for all EDMA data transfers submitted to the logical channel via ECPY_directStartEdma to complete. More... | |
| Void | ECPY_activate (ECPY_Handle handle) |
| Activate the given channel. More... | |
| ECPY_Handle | ECPY_createHandle (IRES_EDMA3CHAN2_Handle handle, IALG_Handle alg) |
| Create an ECPY Handle using the supplied IRES_EDMA3CHAN handle. More... | |
| Void | ECPY_deleteHandle (ECPY_Handle handle) |
| Delete ECPY_Handle. More... | |
| Void | ECPY_deactivate (ECPY_Handle handle) |
| Deactivates the given channel. More... | |
| Void | ECPY_setEarlyCompletionMode (ECPY_Handle handle, short enabled) |
| Setting the TCCMODE (Early or Normal) affects only the 'intermediate transfers' of the linked transfers submitted using this channel. All subsequent direct and non-direct ECPY_configure* calls using this ecpyHandle will program the OPT's TCCMODE to select Early or Normal completion mode based on the 'enabled' argument. More... | |
| Void | ECPY_init (Void) |
| Initialize the ECPY module. Called by framework. More... | |
| Void | ECPY_exit (Void) |
| Finalization of the ECPY module. More... | |
Macros | |
| #define | ti_sdo_fc_ires_NOPROTOCOLREV |
| #define | ECPY_GTNAME "ti.sdo.fc.ecpy" |
| #define | ECPY_MODNAME "ti.sdo.fc.ecpy" |
| Name to pass to Diags_setMask() to enable logging for ECPY functions. For example, Diags_setMask(ECPY_MODNAME"+EX1234567"); turns on all Log statements in this module. Diags_setMask() must be called after initialization to take effect. More... | |
Data Structures | |
| struct | ECPY_Params |
| DMA transfer specific parameters. Defines the configuration of a logical channel. More... | |
| struct | ECPY_CfgParams |
| The module configuration structure for ECPY. It is set at design time by the system integrator to register customize memory allocation/free implementations. More... | |
Typedefs | |
| typedef enum ECPY_ParamField16b | ECPY_ParamField16b |
| ECPY 16-bit param field structure. These values are passed to ECPY_configure16() to indicate the field of the ECPY_Params structure to be changed. More... | |
| typedef enum ECPY_ParamField32b | ECPY_ParamField32b |
| ECPY 32-bit param field structure. These values are passed to ECPY_configure32() to indicate the field of the ECPY_Params structure to be changed. More... | |
| typedef enum ECPY_TransferType | ECPY_TransferType |
| ECPY DMA Transfer Types: More... | |
| typedef struct ECPY_Obj * | ECPY_Handle |
| Handle to "logical" ECPY Channel. More... | |
| typedef struct ECPY_Params | ECPY_Params |
| DMA transfer specific parameters. Defines the configuration of a logical channel. More... | |
| typedef Bool( | ECPY_PersistentAllocFxn) (IALG_MemRec *memTab, Int numRecs) |
| Memory allocation function signature for module configuration. More... | |
| typedef Void( | ECPY_PersistentFreeFxn) (IALG_MemRec *memTab, Int numRecs) |
| Memory deallocation function signature for module configuration. More... | |
| typedef Bool( | ECPY_ScratchAllocFxn) (IALG_Handle alg, Int scratchId, IALG_MemRec *memTab, Int numRecs) |
| Scratch Memory allocation function for all shared scratch ECPY handle state. More... | |
| typedef Void( | ECPY_ScratchFreeFxn) (Int mutexId, Void *addr, UInt size) |
| Scratch Memory free function for all scratch allocated memory in ECPY Handle. More... | |
| typedef Int( | ECPY_getScratchIdFxn) (IALG_Handle alg) |
| Function, when supplied, returns the scratchId associated with the algorithm instance whose handle is passed. More... | |
| typedef struct ECPY_CfgParams | ECPY_CfgParams |
| The module configuration structure for ECPY. It is set at design time by the system integrator to register customize memory allocation/free implementations. More... | |
Enumerations | |
| enum | ECPY_ParamField16b { ECPY_PARAMFIELD_ELEMENTSIZE = 8, ECPY_PARAMFIELD_NUMELEMENTS = 10, ECPY_PARAMFIELD_ELEMENTINDEX_SRC = 16, ECPY_PARAMFIELD_ELEMENTINDEX_DST = 18, ECPY_PARAMFIELD_FRAMEINDEX_SRC = 24, ECPY_PARAMFIELD_FRAMEINDEX_DST = 26, ECPY_PARAMFIELD_NUMFRAMES = 28 } |
| ECPY 16-bit param field structure. These values are passed to ECPY_configure16() to indicate the field of the ECPY_Params structure to be changed. More... | |
| enum | ECPY_ParamField32b { ECPY_PARAMFIELD_SRCADDR = 4, ECPY_PARAMFIELD_DSTADDR = 12, ECPY_PARAMFIELD_ELEMENTINDEXES = 16, ECPY_PARAMFIELD_FRAMEINDEXES = 24 } |
| ECPY 32-bit param field structure. These values are passed to ECPY_configure32() to indicate the field of the ECPY_Params structure to be changed. More... | |
| enum | ECPY_TransferType { ECPY_1D1D, ECPY_1D2D, ECPY_2D1D, ECPY_2D2D } |
| ECPY DMA Transfer Types: More... | |
Variables | |
| __FAR__ ECPY_CfgParams | ECPY_CFG_PARAMS |
| Initialization parameters for the ECPY module. More... | |