1    /* 
     2     * Copyright (c) 2012, Texas Instruments Incorporated
     3     * All rights reserved.
     4     *
     5     * Redistribution and use in source and binary forms, with or without
     6     * modification, are permitted provided that the following conditions
     7     * are met:
     8     *
     9     * *  Redistributions of source code must retain the above copyright
    10     *    notice, this list of conditions and the following disclaimer.
    11     *
    12     * *  Redistributions in binary form must reproduce the above copyright
    13     *    notice, this list of conditions and the following disclaimer in the
    14     *    documentation and/or other materials provided with the distribution.
    15     *
    16     * *  Neither the name of Texas Instruments Incorporated nor the names of
    17     *    its contributors may be used to endorse or promote products derived
    18     *    from this software without specific prior written permission.
    19     *
    20     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
    21     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
    22     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
    23     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
    24     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
    25     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
    26     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
    27     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
    28     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
    29     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
    30     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    31     * 
    32     */
    33    
    34    /*
    35     *  ======== package.xdc ========
    36     *
    37     */
    38    
    39    /*!
    40     *  ======== ti.sdo.opencl ========
    41     *  OpenCL API Implementation
    42     *
    43     *  OpenCL is a programming framework for heterogeneous compute resources
    44     *  developed by the Khronos group. It allows a host processor to execute
    45     *  code on multiple device processors.
    46     *
    47     *  This implementation of the OpenCL specification supports only the
    48     *  task-parallel model. Please note, this implementation is still under
    49     *  development.
    50     *
    51     *  The following diagram illustrates an OpenCL application architecture.
    52     *
    53     *  @p(html)
    54     *  <br>
    55     *  <img src="./doc-files/AppArch.png" />
    56     *  <br>
    57     *  @p
    58     *
    59     *  The application, running on the host processor, makes OpenCL API
    60     *  calls to execute kernel functions on the device processor. In this
    61     *  example, the application is running on the C674x processor and the
    62     *  kernel functions are executed on the ARP32 processor. The application
    63     *  provides the thread (red circle) which calls the OpenCL APIs. The
    64     *  OpenCL Runtime provides the thread on the device processor which is
    65     *  used to execute the kernel functions. There may be multiple device
    66     *  processors in a system but only one host processor.
    67     *
    68     *  The application and the kernel functions have access to the framework
    69     *  components. For example, they can make calls into the XDC and SYS/BIOS
    70     *  components. The kernel functions also have access to the ECPY component.
    71     *
    72     *  @a(OpenCL Programming Model)
    73     *  The application must create the following objects to setup an OpenCL
    74     *  execution environment: a context object, a command queue, and a program
    75     *  object. This is done with the following functions.
    76     *
    77     *  @p(blist)
    78     *  - clGetPlatformIDs
    79     *  - clGetDeviceIDs
    80     *  - clCreateContext
    81     *  - clCreateCommandQueue
    82     *  - clCreateProgramWithBinary
    83     *  @p
    84     *  Once these objects have been created, the application creates a kernel
    85     *  object for each kernel function it wants to execute on the compute
    86     *  device. The kernel object is used to set the function argument values.
    87     *  The command queue is used to schedule a kernel function for execution.
    88     *
    89     *  @p(blist)
    90     *  - clCreateKernel
    91     *  - clSetKernelArg
    92     *  - clEnqueueTask
    93     *  @p
    94     *  After a kernel function has been scheduled with a call to clEnqueueTask,
    95     *  the kernel object can be reused with new argument values to schedule
    96     *  the kernel function again.
    97     *  @p
    98     *  To release the resources used by OpenCL, the application must call the
    99     *  following functions before terminating.
   100     *
   101     *  @p(blist)
   102     *  - clReleaseKernel
   103     *  - clReleaseProgram
   104     *  - clReleaseCommandQueue
   105     *  - clReleaseContext
   106     *  @p
   107     *
   108     *  @a(OpenCL API Example Code)
   109     *  The following psudeo code gives an example of what an OpenCL program
   110     *  would look like. See the
   111     *  {@link ti.sdo.opencl.examples.hello Hello Example} for a working program.
   112     *
   113     *  @p(code)
   114     *  #include <CL/opencl.h>
   115     *
   116     *  cl_context          context;
   117     *  cl_command_queue    cmdQue;
   118     *  cl_program          program;
   119     *  cl_kernel           helloKnl;
   120     *  Ptr                 bufBase;
   121     *
   122     *
   123     *  //  -------- OpenCL Initialization --------
   124     *
   125     *  // get the default platform
   126     *  clGetPlatformIDs(.., platformAry, ..);
   127     *
   128     *  // get an accelerator device
   129     *  clGetDeviceIDs(platformAry, .., deviceAry, ..);
   130     *
   131     *  // create a context for the accelerator device
   132     *  context = clCreateContext(.., deviceAry, ..);
   133     *
   134     *  // create a command-queue for the accelerator device
   135     *  cmdQue = clCreateCommandQueue(context, deviceAry, ..);
   136     *
   137     *  // create program object
   138     *  program = clCreateProgramWithBinary(context, .., deviceAry, ..);
   139     *
   140     *
   141     *  //  -------- Application Execute Phase --------
   142     *
   143     *  // create a handle to the OpenCL kernel (function)
   144     *  helloKnl = clCreateKernel(program, "HelloKnl", ..);
   145     *
   146     *  // allocate buffer using host allocated memory
   147     *  bufBase = Memory_alloc(heap, 64, ..);
   148     *
   149     *  // assign the kernel arguments
   150     *  clSetKernelArg(helloKnl, 0, sizeof(Ptr), &bufBase);
   151     *
   152     *  // invoke the hello world kernel
   153     *  clEnqueueTask(cmdQue, helloKnl, ..);
   154     *
   155     *  // read the buffer contents
   156     *  System_printf("%s\n", (Char *)bufBase);
   157     *  Memory_free(heap, bufBase, bufSize);
   158     *
   159     *
   160     *  //  -------- OpenCL Finalization --------
   161     *
   162     *  clReleaseKernel(helloKnl);
   163     *  clReleaseProgram(program);
   164     *  clReleaseCommandQueue(cmdQue);
   165     *  clReleaseContext(context);
   166     *
   167     *  @a(OpenCL Kernel Example Code)
   168     *  The following psudeo code gives an example of what an OpenCL kernel
   169     *  function looks like. For the most part, it looks just like an ordinary
   170     *  function. However, a kernel function must have a return type of void,
   171     *  cannot use recursion, and does not support pointers to functions.
   172     *  Additional restrictions are specified in the OpenCL Spec in Section 6.8.
   173     *
   174     *  @p(code)
   175     *  #include <string.h>
   176     *
   177     *  void HelloKnl(char *buffer)
   178     *  {
   179     *      strncpy(buffer, "Hello World");
   180     *  }
   181     *
   182     *  @a(OpenCL Runtime Registration)
   183     *  All kernel functions must be registered with the OpenCL Runtime. This
   184     *  is done using static initialization. The OpenCL Runtime references the
   185     *  following two symbols.
   186     *  @p(code)
   187     *  Int                 ti_sdo_opencl_ComputeDevices_numUnits
   188     *  ComputeDevice_Unit  ti_sdo_opencl_ComputeDevices_units[]
   189     *  @p
   190     *  When building an executable, you must provide a source file which declares
   191     *  and statically initializes these two symbols. The following figure
   192     *  gives an example.
   193     *  @p(html)
   194     *  <img src="./doc-files/KernelTable.png" />
   195     *  @p
   196     *  In the figure above, there are two units, ModA.c and ModB.c. The ModA
   197     *  unit defines one kernel function. The second unit, ModB, defines an
   198     *  init and exit function and two kernel functions. In the file KernelTable.c,
   199     *  an array of units is declared and initialized with the contents of
   200     *  ModA and ModB.
   201     *
   202     *  Here is the source code of KernelTable.c
   203     *  @p(code)
   204     *  #include <xdc/std.h>
   205     *  #include <ti/sdo/opencl/ComputeDevice.h>
   206     *
   207     *  UInt ModA_func1_args[] = {
   208     *      ti_cl_arg_type_GlobalPtr,
   209     *      ti_cl_arg_type_Int,
   210     *      ti_cl_arg_type_Int
   211     *  };
   212     *
   213     *  ComputeDevice_FxnDesc ModA_fxnTab[] = {
   214     *      {
   215     *          "ModA_func1",     // fxn name
   216     *          (Fxn)ModA_func1,  // fxn address
   217     *          3,                // num args
   218     *          ModA_func1_args   // arg types
   219     *      }
   220     *  };
   221     *
   222     *  UInt ModB_func1_args[] = {
   223     *      ti_cl_arg_type_Int,
   224     *      ti_cl_arg_type_Int
   225     *  };
   226     *
   227     *  UInt ModB_func2_args[] = {
   228     *      ti_cl_arg_type_Int,
   229     *      ti_cl_arg_type_Int,
   230     *      ti_cl_arg_type_Int,
   231     *      ti_cl_arg_type_Int
   232     *  };
   233     *
   234     *  ComputeDevice_FxnDesc ModB_fxnTab[] = {
   235     *      {
   236     *          "ModB_func1",     // fxn name
   237     *          (Fxn)ModB_func1,  // fxn address
   238     *          2,                // num args
   239     *          ModB_func1_args   // arg types
   240     *      },
   241     *      {
   242     *          "ModB_func2",     // fxn name
   243     *          (Fxn)ModB_func2,  // fxn address
   244     *          4,                // num args
   245     *          ModB_func2_args   // arg types
   246     *      }
   247     *  };
   248     *
   249     *  Int ti_sdo_opencl_ComputeDevice_numUnits = 2;
   250     *  ComputeDevice_Unit ti_sdo_opencl_ComputeDevice_units[] = {
   251     *      {   // ModA
   252     *          NULL,
   253     *          NULL,
   254     *          1,
   255     *          ModA_fxnTab
   256     *      },
   257     *      {   // ModB
   258     *          ModB_initFxn,
   259     *          ModB_exitFxn,
   260     *          2,
   261     *          ModB_fxnTab
   262     *      }
   263     *  };
   264     *
   265     *  @a(Available Functions)
   266     *  The following list of OpenCL APIs are functional in this port. Please
   267     *  note, this is work in progress and not all features may be currently
   268     *  implemented.
   269     *  
   270     *  OpenCL Platform Layer
   271     *  @p(blist)
   272     *  - clGetPlatformIDs
   273     *  - clGetPlatformInfo
   274     *  - clGetDeviceIDs
   275     *  - clGetDeviceInfo
   276     *  - clCreateContext
   277     *  - clCreateContextFromType
   278     *  - clRetainContext
   279     *  - clReleaseContext
   280     *  - clGetContextInfo
   281     *  @p
   282     *
   283     *  OpenCL Execution Layer
   284     *  @p(blist)
   285     *  - clCreateCommandQueue
   286     *  - clRetainCommandQueue
   287     *  - clReleaseCommandQueue
   288     *  - clGetCommandQueueInfo
   289     *  - clSetCommandQueueProperty
   290     *  - clCreateProgramWithBinary
   291     *  - clRetainProgram
   292     *  - clReleaseProgram
   293     *  - clGetProgramInfo
   294     *  - clCreateKernel
   295     *  - clSetKernelArg
   296     *  - clRetainKernel
   297     *  - clReleaseKernel
   298     *  @p
   299     *
   300     *  @a(Legend)
   301     *  This legend applies to all figures.
   302     *  @p(html)
   303     *  <img src="./doc-files/Legend.png" />
   304     *  @p
   305     *
   306     *  @a(See Also)
   307     *  @p(dlist)
   308     *  - {@link http://www.khronos.org/registry/cl/ Khronos OpenCL Web Site}
   309     *  - {@link ti.sdo.opencl.examples Suite of OpenCL examples for TI devices}
   310     *  - {@link ti.sdo.opencl.examples.hello Hellow World example}
   311     *  @p
   312     */
   313    package ti.sdo.opencl [1,0,0] {
   314        module OpenCL;
   315        module ComputeDevice;
   316    }
   317    /*
   318     *  @(#) ti.sdo.opencl; 1, 0, 0,3; 4-16-2012 00:03:02; /db/atree/library/trees/fc/fc-q08/src/ xlibrary
   319    
   320     */
   321