Modules
Remote Command Message - message based remote function execution
The Remote Command Message (RCM) package provides a client/server implementation for executing functions on a remote processor. The package contains the following modules.
This package provides modules for a client/server based implementation for executing functions on a remote processor. The IPC layer is based on messages. The application uses the RcmClient module to allocate a message, specify the remote function and its arguments, and then send the message to the server for execution. When the message returns, it contains the remote function's return values. The server is typically on a remote processor, but local server instances (on the same processor as the client) are also supported.
The following image provides an overview of a typical use case. An application running on the local cpu creates an RcmClient instance. Using the RcmClient instance handle, the application has access to all the necessary operations for executing a message on the remote server. The application must fill in the message with the remote function index, as supplied by the server, and the context needed by the remote function to execute. For higher level operations such as RPC, see the link ti.sdo.rpc.gen
package which provides support for generating the stub and skeleton functions.
Diagram 1: RCM Overview
The RcmClient module is used to create instance objects. Each instance can send messages only to the server specified at create time. You create an instance for each server you want to send messages to. At create time the heap must be specified. The heap is used by the instance for allocating messages.
There are four types of execute commands:
- synchronous blocking
- synchronous non-blocking
- synchronous deferred
- asynchronous non-blocking
Here is an overview of the exec commands. See the RcmClient module for more details on each function.
- RcmClient_exec() - synchronous blocking This function sends a message to the server and waits for the server to execute the message and to send the return message back to the client.
- RcmClient_execNoWait() - synchronous non-blocking This function sends a message to the server but does not wait for the return message. Control returns to the caller as soon as the message has been delivered to the underlying transport. The server will execute the message and send the return message back to the client where it is placed in a mailbox. The client collects the return message with a call to RcmClient_waitUntilDone() which is a blocking call. This is useful when the client has more work to do while the remote function is executing. It is also efficient because it does not require a local callback thread.
- RcmClient_execDpc() - synchronous deferred This function sends a message to the server and waits for the return message. When the server receives the message, it does not immediately execute it. Instead, it copies the message context into a local buffer and sends the message back to the client. Only after the message has been sent to the client, does the server execute the function. This is useful for server shutdown. This allows the client to regain ownership of the message and to return it to the heap and allows the server to shutdown without owning any resources allocated by the client.
- RcmClient_execAsync() - asynchronous non-blocking This function sends a message to the server but does not wait for the return message. Control returns to the caller as in the synchronous non-blocking case above. The server will execute the message and send the return message back to the client for delivery to a callback thread. When the return message arrives, the callback thread will invoke an application callback to notify the application that the return message has arrived. This is the only asynchronous part of the sequence as the application will be preempted by the callback thread. It is the application's responsibility to periodically monitor a flag (set by the callback) to complete the message delivery.
RTSC Configuration
When using XDCtools to build your executable, use the following module to define the build time configuration options.
RCM Settings Module