![]() |
![]() |
IRES PROTOCOL TILEDMEMORY Interface Definitions (Beta) - Allows algorithms to request and receive handles representing the TILEDMEMORY resource.
#include <ti/xdais/xdas.h>
#include <ti/xdais/ires_common.h>
#include <ti/xdais/ires.h>
Go to the source code of this file.
Defines | |
#define | IRES_TILEDMEMORY_PROTOCOLNAME "ti.sdo.fc.ires.tiledmemory" |
Name used to describe this protocol. | |
#define | TILEDMEMORY_MODNAME "ti.sdo.fc.ires.tiledmemory" |
Name to pass to Diags_setMask() to enable logging for TILEDMEMORY functions. For example, Diags_setMask(TILEDMEMORY_MODNAME"+EX1234567"); turns on all Log statements in this module. Diags_setMask() must be called after initialization to take effect. | |
Data Structures | |
struct | IRES_TILEDMEMORY_ProtocolArgs |
TILEDMEMORY Protocol Arguments definition. More... | |
struct | IRES_TILEDMEMORY_Obj |
IRES_TILEDMEMORY_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource. More... | |
struct | IRES_TILEDMEMORY_RegisterLayer |
TILEDMEMORY Register Layout. More... | |
struct | IRES_TILEDMEMORY_Properties |
Static Resource Properties. More... | |
Typedefs | |
typedef struct IRES_TILEDMEMORY_Obj * | IRES_TILEDMEMORY_Handle |
Handle to "logical" resource. | |
typedef enum IRES_TILEDMEMORY_AccessDimension | IRES_TILEDMEMORY_AccessDimension |
Indicates whether requested/granted memory is of type 1D or 2D. | |
typedef enum IRES_TILEDMEMORY_AccessUnit | IRES_TILEDMEMORY_AccessUnit |
Indicates the size of the Tiler elements requested by the codec. | |
typedef struct IRES_TILEDMEMORY_ProtocolArgs | IRES_TILEDMEMORY_ProtocolArgs |
TILEDMEMORY Protocol Arguments definition. | |
typedef struct IRES_TILEDMEMORY_Obj | IRES_TILEDMEMORY_Obj |
IRES_TILEDMEMORY_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource. | |
typedef struct IRES_TILEDMEMORY_RegisterLayer | IRES_TILEDMEMORY_RegisterLayer |
TILEDMEMORY Register Layout. | |
typedef struct IRES_TILEDMEMORY_Properties | IRES_TILEDMEMORY_Properties |
Static Resource Properties. | |
Enumerations | |
enum | IRES_TILEDMEMORY_AccessDimension { IRES_TILEDMEMORY_1D = 0, IRES_TILEDMEMORY_2D = 1 } |
Indicates whether requested/granted memory is of type 1D or 2D. More... | |
enum | IRES_TILEDMEMORY_AccessUnit { IRES_TILEDMEMORY_RAW = 0, IRES_TILEDMEMORY_PAGE = 1, IRES_TILEDMEMORY_8BIT = 2, IRES_TILEDMEMORY_16BIT = 3, IRES_TILEDMEMORY_32BIT = 4 } |
Indicates the size of the Tiler elements requested by the codec. More... |