![]() |
![]() |
ACPY3 Definitions (C64P) - 3rd Generation ACPY. Provides a comprehensive list of DMA operations an algorithm can perform on logical DMA channels it acquires through the IDMA3 protocol.
#include <ti/xdais/idma3.h>
Go to the source code of this file.
Functions | |
Void | ACPY3_configure (IDMA3_Handle handle, ACPY3_Params *params, short transferNo) |
Functions called by the framework for allocating and initializing the channel state. | |
Void | ACPY3_fastConfigure16b (IDMA3_Handle handle, ACPY3_ParamField16b fieldId, unsigned short value, short transferNo) |
Modify the 16-bit DMA transfer parameter, indicated by the parameter field id, fieldId, of the current channel settings. | |
Void | ACPY3_fastConfigure32b (IDMA3_Handle handle, ACPY3_ParamField32b fieldId, Uns value, short transferNo) |
Modify the 32-bit DMA transfer parameter, indicated by the parameter field id, fieldId, of the current channel settings. | |
Void | ACPY3_setFinal (IDMA3_Handle handle, short transferNo) |
Indicate that a given transfer will be the last in a sequence of linked transfers. | |
Void | ACPY3_fastSetFinal (IDMA3_Handle handle, short transferNo) |
Indicate that a given transfer will be the last in a sequence of linked transfers. | |
Void | ACPY3_start (IDMA3_Handle handle) |
Submit a single or linked transfer using the most recently configured transfer parameter settings. | |
Void | ACPY3_wait (IDMA3_Handle handle) |
Wait for all data transfers on a logical channel to complete. | |
Void | ACPY3_waitLinked (IDMA3_Handle handle, unsigned short waitId) |
Wait for an individual transfer in a Linked transfer to finish. | |
Bool | ACPY3_complete (IDMA3_Handle handle) |
Check to see if all dma transfers on logical channel are finished. | |
Bool | ACPY3_completeLinked (IDMA3_Handle handle, unsigned short waitId) |
Non-blocking query to check completion of an individual transfer in a Linked transfer. | |
Void | ACPY3_activate (IDMA3_Handle handle) |
Activate the given channel. | |
Void | ACPY3_deactivate (IDMA3_Handle handle) |
Deactivates the given channel. | |
Void | ACPY3_init (Void) |
Initialize the ACPY3 module. Called by framework. | |
Void | ACPY3_exit (Void) |
Finalization of the ACPY3 module. | |
Defines | |
#define | ACPY3_GTNAME "ti.sdo.fc.acpy3" |
#define | ACPY3_MODNAME "ti.sdo.fc.acpy3" |
Name to pass to Diags_setMask() to enable logging for ACPY3 functions. For example, Diags_setMask(ACPY3_MODNAME"+EX1234567"); turns on all Log statements in this module. Diags_setMask() must be called after initialization to take effect. | |
Data Structures | |
struct | ACPY3_Params |
DMA transfer specific parameters. Defines the configuration of a logical channel. More... | |
Typedefs | |
typedef enum ACPY3_ParamField16b | ACPY3_ParamField16b |
ACPY3 16-bit param field structure. These values are passed to ACPY3_fastConfigure16b() to indicate the field of the ACPY3_Params structure to be changed. | |
typedef enum ACPY3_ParamField32b | ACPY3_ParamField32b |
ACPY3 32-bit param field structure. These values are passed to ACPY3_fastConfigure32b() to indicate the field of the ACPY3_Params structure to be changed. | |
typedef enum ACPY3_TransferType | ACPY3_TransferType |
ACPY3 DMA Transfer Types: | |
typedef struct ACPY3_Params | ACPY3_Params |
DMA transfer specific parameters. Defines the configuration of a logical channel. | |
Enumerations | |
enum | ACPY3_ParamField16b { ACPY3_PARAMFIELD_ELEMENTSIZE = 8, ACPY3_PARAMFIELD_NUMELEMENTS = 10, ACPY3_PARAMFIELD_ELEMENTINDEX_SRC = 16, ACPY3_PARAMFIELD_ELEMENTINDEX_DST = 18, ACPY3_PARAMFIELD_FRAMEINDEX_SRC = 24, ACPY3_PARAMFIELD_FRAMEINDEX_DST = 26, ACPY3_PARAMFIELD_NUMFRAMES = 28 } |
ACPY3 16-bit param field structure. These values are passed to ACPY3_fastConfigure16b() to indicate the field of the ACPY3_Params structure to be changed. More... | |
enum | ACPY3_ParamField32b { ACPY3_PARAMFIELD_SRCADDR = 4, ACPY3_PARAMFIELD_DSTADDR = 12, ACPY3_PARAMFIELD_ELEMENTINDEXES = 16, ACPY3_PARAMFIELD_FRAMEINDEXES = 24 } |
ACPY3 32-bit param field structure. These values are passed to ACPY3_fastConfigure32b() to indicate the field of the ACPY3_Params structure to be changed. More... | |
enum | ACPY3_TransferType { ACPY3_1D1D, ACPY3_1D2D, ACPY3_2D1D, ACPY3_2D2D } |
ACPY3 DMA Transfer Types: More... | |
Variables | |
IDMA3_ProtocolObj | ACPY3_PROTOCOL |