![]() |
![]() |
Remote Command Message Server Module. An RcmServer processes inbound messages received from an RcmClient.
The RcmServer processes inbound messages received from an RcmClient. After processing a message, the server will return the message to the client.
#include <xdc/runtime/knl/GateThread.h>
#include <xdc/runtime/knl/Thread.h>
Go to the source code of this file.
Functions | |
Int | RcmServer_addSymbol (RcmServer_Handle handle, String name, RcmServer_MsgFxn addr, UInt32 *index) |
Add a symbol to the server's function table. | |
Int | RcmServer_construct (RcmServer_Struct *structPtr, String name, const RcmServer_Params *params) |
Initialize a new instance object inside the provided structure. | |
Int | RcmServer_create (String name, RcmServer_Params *params, RcmServer_Handle *handle) |
Create an RcmServer instance. | |
Int | RcmServer_delete (RcmServer_Handle *handlePtr) |
Delete an RcmServer instance. | |
Int | RcmServer_destruct (RcmServer_Struct *structPtr) |
Finalize the instance object inside the provided structure. | |
Void | RcmServer_exit (Void) |
Finalize the RcmServer module. | |
Void | RcmServer_init (Void) |
Initialize the RcmServer module. | |
Void | RcmServer_Params_init (RcmServer_Params *params) |
Initialize the instance create params structure. | |
Int | RcmServer_removeSymbol (RcmServer_Handle handle, String name) |
Remove a symbol and from the server's function table. | |
Int | RcmServer_start (RcmServer_Handle handle) |
Start the server. | |
Defines | |
#define | RcmServer_S_SUCCESS (0) |
Success return code. | |
#define | RcmServer_E_FAIL (-1) |
General failure return code. | |
#define | RcmServer_E_NOMEMORY (-2) |
The was insufficient memory left on the heap. | |
#define | RcmServer_E_SYMBOLNOTFOUND (-3) |
The given symbol was not found in the server's symbol table. | |
#define | RcmServer_E_SYMBOLSTATIC (-4) |
The given symbols is in the static table, it cannot be removed. | |
#define | RcmServer_E_SYMBOLTABLEFULL (-5) |
The server's symbol table is full. | |
Data Structures | |
struct | RcmServer_FxnDesc |
Function descriptor. More... | |
struct | RcmServer_FxnDescAry |
Function descriptor array. More... | |
struct | RcmServer_ThreadPoolDesc |
Worker pool descriptor. More... | |
struct | RcmServer_ThreadPoolDescAry |
Worker pool descriptor array. More... | |
struct | RcmServer_Params |
RcmServer Instance create parameters. More... | |
struct | RcmServer_Struct |
Opaque client structure large enough to hold an instance object. More... | |
Typedefs | |
typedef Int32(* | RcmServer_MsgFxn )(UInt32, UInt32 *) |
Remote function type. | |
typedef struct RcmServer_Object_tag * | RcmServer_Handle |
RcmServer instance object handle. |