VICPSYNC Interface Definitions - Framework support package for synchronization between codec and VICP usage. This package allows algorithms to wait on interrupt completion of individual functional units of the VICP * coprocessor.
#include <ti/xdais/ialg.h>
#include <ti/sdo/fc/ires/vicp/ires_vicp2.h>
Go to the source code of this file.
Data Structures | |
struct | VICPSYNC_Params |
The module configuration structure for VICPSYNC implementation. More... | |
Defines | |
#define | VICPSYNC_GTNAME "ti.sdo.fc.vicpsync" |
Enumerations | |
enum | VICPSYNC_ResourceType { VICPSYNC_IMX0, VICPSYNC_IMX1, VICPSYNC_MJCP, VICPSYNC_NSF } |
Resource types for which the API can be called. More... | |
enum | VICPSYNC_InterruptLine { VICPSYNC_FIXED, VICPSYNC_FLEXIBLE } |
Interrupt line that can be specified for each Resource type. More... | |
enum | VICPSYNC_InterruptType { VICPSYNC_IRQ, VICPSYNC_FIQ } |
Interrupt type that can be specified for each Resource type. More... | |
enum | VICPSYNC_Status { VICPSYNC_OK, VICPSYNC_EFAIL, VICPSYNC_ENORESOURCE } |
Functions | |
VICPSYNC_Status | VICPSYNC_start (IALG_Handle handle, VICPSYNC_ResourceType res, VICPSYNC_InterruptType intType, VICPSYNC_InterruptLine intLine, IRES_VICP2_Handle vicpHandle) |
This is the top level function that allows ARM-side algorithms to mark beginning of the usage of individual functional units of VICP. | |
VICPSYNC_Status | VICPSYNC_wait (IRES_VICP2_Handle vicpHandle, VICPSYNC_ResourceType res) |
This is the top level function that allows the ARM-side algorithms to wait for interrupt corresponding to the functional unit of the VICP to fire. | |
Bool | VICPSYNC_done (IRES_VICP2_Handle vicpHandle, VICPSYNC_ResourceType res) |
This is the top level function that allows the ARM-side algorithms to query the status of the interrupt corresponding to the functional unit that was configured using VICPSYNC_start call. | |
VICPSYNC_Status | VICPSYNC_unregister (IRES_VICP2_Handle vicpHandle, VICPSYNC_ResourceType res) |
This is the top level function that allows the ARM-side algorithms to unregister the ISR associated with the VICP resource that may have been previously registered via a call to VICPSYNC_start. | |
Variables | |
VICPSYNC_Params | VICPSYNC_PARAMS |
Default module configuration structure (defined in vicpsync.c). |