Welcome!

DaVinci Technology from TI makes the next generation of digital video and audio end-equipment applications possible. Learn more at The DaVinci Effect website.

This web page is being served from an HTTP server running on the ARM926 processor of the DaVinci SoC on the DaVinci DVEVM board. For the latest news and software updates on the DVEVM, see the DVEVM website.

Control the A/V Demo

The DVEVM comes with a demo application that shows the power of the DaVinci hardware and software that can be used to build incredible digital video and audio products. You can start the demo and query the state of the system by using the links below (which invoke simple CGI scripts on the DVEVM web server). Note that if the demo is already running, you will have to exit the demo using the IR remote before it can be (re)started using the web interface.

This is the same demo application that is automatically started whenever you turn on the EVM board.