![]() |
![]() |
|
Codec Engine Application Programming Interface (API)
ce-w08
|
The VIDANALYTICS video analytics interface. Provides the user an interface to create and interact with XDAIS algorithms that are compliant with the XDM-defined IVIDANALYTICS video analytics interface.
#include <ti/xdais/dm/xdm.h>#include <ti/xdais/dm/ividanalytics.h>#include <ti/sdo/ce/Engine.h>#include <ti/sdo/ce/visa.h>#include <ti/sdo/ce/skel.h>
Go to the source code of this file.
Macros | |
| #define | VIDANALYTICS_EOK IVIDANALYTICS_EOK |
| | |
| #define | VIDANALYTICS_EFAIL IVIDANALYTICS_EFAIL |
| | |
| #define | VIDANALYTICS_EUNSUPPORTED IVIDANALYTICS_EUNSUPPORTED |
| | |
| #define | VIDANALYTICS_ETIMEOUT VISA_ETIMEOUT |
| Timeout occurred. | |
| #define | VIDANALYTICS_FOREVER VISA_FOREVER |
| Special value for timeout parameter indicating never timeout. | |
| #define | VIDANALYTICS_STUBSNAME "VIDANYLITIC_STUBS" |
| Name of stub functions. Use this name when registering the VIDANALYTICS_STUBS functions with Engine_addStubFxns. | |
| #define | VIDANALYTICS_VISATYPE "ti.sdo.ce.vidanalytics.IVIDANALYTICS" |
| The VISA type. | |
Typedefs | |
| typedef VISA_Handle | VIDANALYTICS_Handle |
| Opaque handle to a VIDANALYTICS codec. | |
| typedef IVIDANALYTICS_Params | VIDANALYTICS_Params |
| Defines the creation time parameters for all IVIDANALYTICS instance objects. | |
| typedef IVIDANALYTICS_InArgs | VIDANALYTICS_InArgs |
| Defines the input arguments for all IVIDANALYTICS instance process function. | |
| typedef IVIDANALYTICS_OutArgs | VIDANALYTICS_OutArgs |
| Defines the run time output arguments for all IVIDANALYTICS instance objects. | |
| typedef IVIDANALYTICS_Cmd | VIDANALYTICS_Cmd |
| Defines the control commands for the IVIDANALYTICS module. | |
| typedef IVIDANALYTICS_DynamicParams | VIDANALYTICS_DynamicParams |
| This structure defines the algorithm parameters that can be modified after creation via control() calls. | |
| typedef IVIDANALYTICS_Status | VIDANALYTICS_Status |
| Defines instance status parameters. | |
Functions | |
| Int32 | VIDANALYTICS_control (VIDANALYTICS_Handle handle, VIDANALYTICS_Cmd id, VIDANALYTICS_DynamicParams *params, VIDANALYTICS_Status *status) |
| Execute the control() method in this instance of a video analytics algorithm. | |
| VIDANALYTICS_Handle | VIDANALYTICS_create (Engine_Handle e, String name, VIDANALYTICS_Params *params) |
| Create an instance of a video analytics algorithm. | |
| Void | VIDANALYTICS_delete (VIDANALYTICS_Handle handle) |
| Delete the instance of a video analytics algorithm. | |
| Int32 | VIDANALYTICS_process (VIDANALYTICS_Handle handle, XDM1_BufDesc *inBufs, XDM1_BufDesc *outBufs, VIDANALYTICS_InArgs *inArgs, VIDANALYTICS_OutArgs *outArgs) |
| Execute the process() method in this instance of a video analytics algorithm. | |
| XDAS_Int32 | VIDANALYTICS_processAsync (VIDANALYTICS_Handle handle, XDM1_BufDesc *inBufs, XDM1_BufDesc *outBufs, IVIDANALYTICS_InArgs *inArgs, IVIDANALYTICS_OutArgs *outArgs) |
| Perform asynchronous submission to this instance of a video analytics algorithm. | |
| XDAS_Int32 | VIDANALYTICS_processWait (VIDANALYTICS_Handle handle, XDM1_BufDesc *inBufs, XDM1_BufDesc *outBufs, IVIDANALYTICS_InArgs *inArgs, IVIDANALYTICS_OutArgs *outArgs, UInt timeout) |
| Wait for a return message from a previous invocation of VIDANALYTICS_processAsync() in this instance of an video analytics algorithm. | |