The Codec Engine is a software platform for algorithm execution that
satisfies the following, high-level goals:
Robust - drives pre-integrated components with fully
characterized performance.
Easy to use - app developers specify what needs to
be run, but not how or where.
Extensible and Configurable - new algorithms can be added
by anyone, using standard tools and techniques.
Portable - API's are target, platform, and in many cases
even codec independant.
Primary packages in this Codec Engine release are briefly described here.
(There are others, see the Configuration Reference
Guide documentation for a complete package list.)
ti.sdo.ce - The Codec Engine runtime.
ti.sdo.ce.video3 - The Codec Engine video component
(supporting the XDM IVIDDEC3 interface). An example is also
provided.
ti.sdo.ce.video2 - The Codec Engine video component
(supporting the XDM IVIDDEC2 and IVIDENC2 interfaces). An example is also
provided.
ti.sdo.ce.video1 - The Codec Engine video component
(supporting the XDM IVIDDEC1 and IVIDENC1 interfaces). An example is also
provided.
ti.sdo.ce.image1 - The Codec Engine image component
(supporting the XDM IIMGDEC1 and IIMGENC1 interfaces). An example is also
provided.
ti.sdo.ce.speech1 - The Codec Engine speech component
(supporting the XDM ISPHDEC1 and ISPHENC1 interfaces). An example is also
provided.
ti.sdo.ce.audio1 - The Codec Engine audio component
(supporting the XDM IAUDDEC1 and IAUDENC1 interfaces). An example is also
provided.
ti.sdo.ce.osal - The Codec Engine OS Abstraction
Layer. This package insulates CE from the OS it's running on, and
provides a few Modules for customers to use (e.g. Memory).
Some distributions of this product include a "cetools" directory
containing some dependent products for convenience. Products included in this release are:
Enable Codec Engine product build without IPC dependency
3.23.00.07
New features
Introduced support for TI813X and TI811X
Removed features
Android support has been removed.
uClibc support has been removed.
Updated Dependencies
OSAL 1.23.00.04
Framework Components 3.23.00.13
DSP/BIOS 6.33.06.50
IPC 1.24.03.32
XDC 3.23.03.53
SysLink 2.20.00.14
The following defects were resolved:
ID
Headline
SDOCM00089271
Remove unsupported TraceUtils library
The following enhancements were resolved:
ID
Headline
SDOCM00046517
Examples should be self contained with all needed files
SDOCM00088611
Add TI813X support
SDOCM00090123
Add support for C6A8149
3.22.00.03
New features
Introduced Android support for TI814X
Updated Dependencies
XDAIS 7.22
OSAL 1.22
Framework Components 3.22
DSP/BIOS 6.33
IPC 1.23
XDC 3.23
Linux Utils 3.22
SysLink 2.10
The following defects were resolved:
ID
Headline
SDOCM00087470
rtcfg makefile needs to use updated XDC-generated preConfig_p* filename
SDOCM00084199
GenCodecPkg fails to load some .genalg files created with earlier versions of XDAIS genalg wizard
SDOCM00086605
Seg fault if user provides invalid procId to Engine_open()
The following enhancements were resolved:
ID
Headline
SDOCM00087472
Add makefile to build Linux ARM libraries without XDC tools
SDOCM00080349
Provide a source only release in addition to existing 'full' and 'lite' releases
SDOCM00085241
Enable 3Ps (e.g. SDKs) to clean/rebuild/redistribute a subset of the CE libraries
3.21.00.19
New features
Introduced support for TI814X and TI816X devices
Restored support for OMAP3 using SysLink and BIOS 6
Updated Dependencies
XDAIS 7.21
OSAL 1.21
Framework Components 3.21
EDMA3 LLD 2.11
DSP/BIOS 6.32
IPC 1.23
XDC 3.22
Linux Utils 3.21
SysLink 2.00
The following defects were resolved:
ID
Headline
SDOCM00081569
GenCodecPkg Wizard Cannot Add Repositories to the XDC Path When Running In Code Composer Studio
SDOCM00047849
DMAN3 and ACPY3 shouldn't be required if not used
SDOCM00077132
GenCodecPkg should detect (and reject) module, vendor, and package names with spaces
SDOCM00080458
Engine_close() should ensure slave side calls Ipc_detach() to detach from HOST
SDOCM00066693
If user fails to assign any value to DEVICES in xdcpaths.mak, a build script crashes - should provide a better error
SDOCM00077205
Server.priority only supports assignment to Server.MINPRI
SDOCM00076030
VIDANALYTICS_control() and process() can crash if zero buffers are provided in/out data arrays
SDOCM00076616
ELF support in the "I have an existing XDAIS library file" option in GenCodecPkg Wizard is broken
SDOCM00080557
GenCodecPkg validation of GenAlg version fails inside of CCS
The following enhancements were resolved:
ID
Headline
SDOCM00081138
Better error msg (during config) when codec producer forgets to override ialgFxns
SDOCM00079905
Codec Engine IUniversal should allow for non-invalidation of select buffers before process()
SDOCM00082848
Provide makefiles to rebuild Linux-side libraries without XDC dependency
SDOCM00047438
Deliver a trace-free version for memory-constrained systems
SDOCM00078117
Remove date/time stamp from ce.lib
SDOCM00078779
Server_getCpuLoad() support for SYS/BIOS
SDOCM00076800
Add support for "-1" (i.e. none) scratch id
SDOCM00075378
Need a configuration parameter to disable run-time config of remote apps
3.20.00.16
New features
Introduced remote algorithm support on homogenous BIOS 6-based
devices
Updated Dependencies
C6x toolchain 7.0.0 (for COFF)
C6x toolchain 7.0.2 (for ELF)
XDAIS 7.20
OSAL 1.20
Framework Components 3.20
EDMA3 LLD 2.10
SYS/BIOS 6.30
IPC 1.21
XDC 3.20
The following defects were resolved:
ID
Headline
SDOCM00066628
CE releases that contain cetools should report that as a repository in the eclipse product plugin
SDOCM00071307
Server isn't sanity checking C674 scratch array sizes during config
The following enhancements were resolved:
ID
Headline
3.00.00.31
New features
Added support for ARM M3 and 64T devices
Added support for SYS/BIOS 6
Removed features
Removed support for multicore devices
Removed support for DSP/BIOS 5
Removed support for WinCE
Updated Dependencies
XDAIS 7.00
OSAL 1.00
Framework Components 3.00
BIOS 6.21
The following defects were resolved:
ID
Headline
The following enhancements were resolved:
ID
Headline
2.26.00.08
The following defects were resolved:
ID
Headline
SDOCM00072472
DSP can hang if it runs out of MSGQs
SDOCM00072473
xdcpaths.mak doesn't add BIOS to the XDCPATH when building with PROGRAMS including APP_LOCAL and not DSP_SERVER
SDOCM00073919
Memory_contigFree() half-succeeds with wrong 'size', leading to bad translation cache entry
SDOCM00073258
CERuntime_init() should call Global_init() before calling Global_getenv()
SDOCM00073918
Close XML file when saving in GenCodecPkg and Genserver wizards
SDOCM00071306
Server isn't sanity checking C674 scratch array sizes during config
SDOCM00072476
Codec Engine "speech" example does not initialize SPHENC1_InArgs encInArgs.data.buf to NULL
SDOCM00072478
Off-chip memory in Genserver Memory Config pane for OMAPL13[78] should be SDRAM
SDOCM00071559
CERuntime_init()/CERuntime_exit()/CERuntime_init()/VISA call from same process will cause seg fault in Linux
SDOCM00073237
IVAMMU section support in Genserver
SDOCM00073941
CE releases that contain cetools should report that as a repository in the eclipse product plugin
SDOCM00072398
CE Codec Class stubs built for debug will segfault in processWait() function if VISA_wait() fails by timing out
SDOCM00071542
Genserver Wizard is settiing the default memory segment to SDRAM for OMAPL138 when it should be DDR2
SDOCM00072388
BIOSUTILS_INSTALL_DIR in xdcpaths.mak should list correct version
SDOCM00072750
Codec Engine doesn't have loadmodules.sh, etc. for DM365
SDOCM00073927
Replace deprecated Memory_contigAlloc() calls in examples with supported Memory_alloc() calls
SDOCM00073930
Genserver Wizard may generate duplicate config params and incorrect config param assignments
SDOCM00072386
OMAPL138 folder missing from examples/apps/system_files
The following enhancements were resolved:
ID
Headline
SDOCM00072384
Add com.ti.dvt.tools.menu addition to codec engine eclipse plugin
SDOCM00072399
Need option to use Cache_wbInvAll() in codec engine skeletons
SDOCM00072401
Provide better tracing when BIOS memory runs out during remote thread creation
SDOCM00073914
Add 'producerId' to all packages, ensuring the marketing version follows the pre-built packages
SDOCM00073916
Integrate GenServer and GenCodecPkg feedback
SDOCM00072470
GenCodecPkg Wizard Enhancements
SDOCM00073924
Provide IALG-requested cached memory on a per-alg basis
SDOCM00073014
Add multiple target support to GenCodecPkg
SDOCM00073015
Codec Engine should support runtime configuration of engine alg tables
2.25.00.05
New features
Added support for DM6467T and OMAP-L138 devices.
Updated Dependencies
XDAIS 6.25
Framework Components 2.25
Linux Utils 2.25.01
DSP Link 1.64
DSP/BIOS 5.41
XDCtools 3.16
The following defects were resolved:
ID
Headline
SDOCM00061210
xdcpaths.mak doesn't add LPM_INSTALL_DIR and EDMA3_LLD_INSTALL_DIR to XDCPATH
SDOCM00062770
UNIVERSAL_process() fails to pass outBufs to remote algs if inBufs is NULL
SDOCM00061557
Queue_get and Queue_put should be atomic
SDOCM00062280
ti.sdo.ce.alg's package.xs always plugs in Sem_* functions for RMAN, MP use-cases would need SemMP_* functions.
The following enhancements were resolved:
ID
Headline
SDOCM00062281
CE needs to plug in implementations for "acquire/releaseLock" functions for the ti.sdo.fc.ires.grouputils.GROUPTUILS module
SDOCM00062629
ICodec.serverFxns and .stubFxns shouldn't be 'readonly' so app and server cfg scripts can assign them
SDOCM00062826
OMAPL138 Support in Genserver
SDOCM00063583
Enable error logging when CE_CHECK is set
SDOCM00060523
Add memory map config to genserver wizard
2.24
New features
WinCE support added for OMAP3 and DM644x
Updated Dependencies
XDCtools 3.10.05
XDAIS 6.24
Framework Components 2.24
Linux Utils 2.24.01 (Linux only)
DSP Link 1.61.03 (Linux) and DSP Link 1.61.04 (WinCE)
LPM 1.24
DSP/BIOS 5.33.05
New Dependencies
WinCE Utils 1.00 (WinCE only)
The following defects were resolved:
ID
Headline
SDOCM00046289
Missing Directories in Codec Engine build_instructions.html file
SDOCM00056026
Lad daemon renders the dsp inoperable on evmDM6446
SDOCM00056164
Power enabled server missing on evmDM6446
SDOCM00056166
Power enabled image1 copy example missing on evmDM6446
SDOCM00057124
genserver wizard generates wrong groupId values
SDOCM00057323
Power management is broken on omap2530
SDOCM00057417
Need instructions on how to rebuild DSPLINK for CE
SDOCM00058045
IUNIVERSAL DSP-side skeleton can cause memory access violations when codec doesn't write to outbuf with CPU
The following enhancements were resolved:
ID
Headline
SDOCM00046186
Need a better solution for setting LONGNAME
SDOCM00054323
Need a better way to build codec engine examples
2.23
Updated Dependencies
Framework Components 2.23
Linux Utils 2.23
DSP Link 1.61.01
LPM 1.23
The following defects were resolved:
ID
Headline
SDOCM00053545
Need to add/set EDMA3_LLD_INSTALL_DIR and LPM_INSTALL_DIR in xdcpaths.mak
SDOCM00053715
LPM drivers missing in loadmodules script on evmDM6446
SDOCM00054193
CE Comm_delete for DSPLink needs to validate/trace return value from MSGQ_close.
2.22
New features
Added support for DM365 and OMAP-L137 devices
Added hibernate/resume power management for OMAP3 devices (built on
the LPM - Local Power Manager - product)
Initial, experimental release of
ti.sdo.ce.wizards.genserver - a graphical
wizard for generating Codec Servers (supports multiple codecs).
Updated Dependencies
Framework Components 2.22
Linux Utils 2.22
DSP/BIOS 5.33.03
DSP Link 1.61
LPM 1.22
EDMA3 LLD 1.06.00.01
The following enhancements were resolved:
ID
Headline
SDOCM00050926
Support and document mechanisms for linking debug libs into end executables
SDOCM00050926
Update to latest LPM release with hibernate/resume omap3 support
2.21
New features
Added support for DM357 devices
Non-rebuildable source code is provided for reference
All content is BSD licensed
Restored support for DaVinci devices (DM644x, DM6467, and DM355) -
this was temporarily removed in CE 2.20
Updated Dependencies
Framework Components 2.21
Linux Utils 2.21
DSP/BIOS 5.33.02
DSP Link 1.60
LPM 1.21
The following defects were resolved:
ID
Headline
SDOCM00046065
Engine_open() needs to create message queues with names that are unique accross processes
SDOCM00046126
Memory_getBuffer*Address() APIs should 'fail better' if size of the buffer provided is zero
SDOCM00046128
Custom BIOS mem segments can be handled incorrectly, leading to createFromServer() errors
SDOCM00046138
Each AUDENC_process() call for a remote codec invokes the codec's IAUDENC_Fxns->process() call twice
SDOCM00049745
CreateFromServer no longer automatically map internal memory segments
The following enhancements were resolved:
ID
Headline
SDOCM00050295
Change Licensing to BSD
SDOCM00050211
Synchronous APIs should support a configurable timeout value
2.20
New features
Added support for OMAP3530 and OMA2530
Source code is provided for reference
New default external memory map used by Codec Engine. See
ti/sdo/ce/ipc/dsplink/DspLinkCfg.xdc for details.
New support for DSP/BIOS Link porting integration. See
ti/sdo/ce/ipc/dsplink/README.txt for details.
Removed features
Removed support for DaVinci ARM-based devices (DM644x, DM355
and DM6467). This is a temporary hiccup in the CE roadmap, but
was done to more quickly support OMAP customers. DaVinci device
support will be restored in a release later this year.
Updated Dependencies
XDAIS 6.20
Framework Components 2.20
Linux Utils 2.20 (Note, the CMEM product has grown in scope, and was
renamed "Linux Utils")
DSP/BIOS 5.32.04
DSP Link 1.51
LPM 1.20
XDCtools 3.10
The following defects were resolved:
ID
Headline
SDSCM00025838
Engine.createFromServer() fails if DSP addr 0x8ad00000 is found
The following enhancements were resolved:
ID
Headline
SDSCM00025012
Codec Engine should automatically configure RMAN's SEM functions correctly
SDSCM00025417
Add CE_CHECK env var to to modify checked flag without a rebuild
SDSCM00026142
LogServer thread stackSize needs to be configurable and have a better default value
SDSCM00026675
Codec Engine must support generic algorithm interface
SDSCM00027121
Codec Engine's OSAL's Memory module for Linux must limit growth of the cached "contigBuf" list
2.10
New features
Updated C6x libraries to CG Tools 6.0.16
Added support for DM6467
Added support for IVIDDEC2 interface.
Added "experimental" asynchronous API support. Some customers have
requested support for asynchronous VISA APIs. This release provides
that support - with "experimental" quality. That is, the APIs are
supported, but compatibility in future releases may be broken or
removed/replaced completely. Customers should feel free to use these
APIs in products, but look for further guidance and roadmap advice
from TI as the product lifecycle continues.
Updated Dependencies
XDAIS 6.10
Framework Components 2.10
For codecs that acquire EDMA3 channels via IRES, FC
release notes state the appropriate, dependent EDMA3 LLD product
version.
CMEM 2.10
DSP/BIOS 5.32.01
DSP Link 1.50
XDC Tools 3.00.06
The following defects were resolved:
ID
Headline
SDSCM00022558
Codec Engine build files and instructions should explain better
how to build for particular platforms only, specificallyDM355
SDSCM00022858
extern declaration of function table symbol is wrong in examples'
<codec>_ti.h files
SDSCM00023298
VIDDEC1 doesn't provide enough buffers for CIF decode
(17 needed)
The following enhancements were resolved:
ID
Headline
2.00
New features
In Linux-based applications, Codec Engine is now callable from
multiple processes. For environments that require DSP/BIOS Link
(e.g. DM644x), users must use Link 1.40.05 P3. For single
processor environments (e.g. DM355), no special instructions are
required. Note that, as always, codecs that
share resources must be configured into the same scratch group. These
scratch groups span processes - so if two different apps use codecs
that share resources, the system integrator must ensure they are placed
into the same system-wide scratch group.
Support for the new IVIDTRANSCODE XDM API has been added. This
provides a standard API for invoking video transcoding algorithms.
See the Reference Guide for details.
Added cache management configuration to XDM 0.9-based remote
image and video algorithms. Using this feature, it is possible to
configure these interfaces to not writeback the output data
buffers if, for example, these are being moved between internal and
external (shared) memory using DMA. This can significantly improve
performance of remote process() calls, as writing back large video or
image buffers is time consuming. See the Configuration Reference Guide,
specifically the
ti.sdo.ce.video.VIDDECConfig/.VIDENCConfig
(and similar modules in the ti.sdo.ce.image package) for
details.
Applications can create remote instances of the same algorithm
to run at different priorities. This enables applications to have,
for example, background transcoding or encoding tasks running alongside
real-time encode or decode operations that use the same codec.
This is handled by adding the priority to the codec name during
creation (e.g. "mpeg3dec:4"). See the Application Developer's Guide
and API Reference Guide for details.
Improved trace usability with new CE_DEBUG environment
variable. See the Application Developer's Guide for details.
Updated Dependencies
Updated to XDAIS 6.00
Updated to Framework Components 2.00
Updated to CMEM 2.00
Updated to XDC 3.00.01
The following defects were resolved:
ID
Headline
SDSCM00017691
viddec1_skel.c has wrong array index
SDSCM00019236
SPHDEC1 and SPHENC1 stubs/skels don't support inArgs->data and
outBuf->bufSize fields
SDSCM00019266
VISA _create() calls with params.size "too big" cause assert for
remote algs
SDSCM00019432
XDM 1.00 stubs fail to initialize internal status->data.buf to
NULL
SDSCM00019767
Need to provide workaround for ISPHENC1/ISPHDEC1 creation params
The following enhancements were resolved:
ID
Headline
SDSCM00010976
Provide per-codec instance priority configuration/modification
SDSCM00015261
Codec Engine must be callable from multiple Linux Processes
SDSCM00017409
Provide an example app demonstrating dynamically loading a CE .so
SDSCM00018299
Add support for 'registering/unregistering' non-CMEM managed buffers
in the Memory_ lookup tables
1.20
General
Updated to XDAIS 5.21, which includes XDM 1.00 interfaces
Updated to DSP/BIOS Link 1.40.05 - this resulted in some
necessary configuration-related changes
Updated to Framework Components 1.20.02
Updated to new XDC Tools 2.93.01
Updated to CMEM 1.04
Added examples for single-processor, environments (e.g. DM643x) -
this includes placing executables into platform-specific directories,
as well as demonstrating necessary caching techniques for cache-enabled
environments.
Added Link Arbiter Daemon (LAD)
Added CERuntime_exit() for applications which want to erase any
CE Runtime from their environment without exiting their application.
This is useful if, for example, an application wants to switch between
a Codec Engine based environment, and a custom DSP Link-based framework.
Moved examples into "Codec Engine-specific" namespaces (e.g., the
previous codecs.viddec1_copy codec package is now the
ti.sdo.ce.examples.codecs.viddec1_copy package).
Added configuration option to XDM 0.9-based video encoders
to not manage the cache for the reconstruction buffers.
Added 'checked' builds to the distribution. This enables
some parameter and usage validation to occur within the CE
framework, helping to identify common coding errors in both
applications and algorithms. Enabling this optional feature
introduces some performance overhead, but is encouraged for
those early in development. This can be enabled in the
application configuration, as well as the Server (for systems
with remote algorithms). See the documentation on the
ti.sdo.ce.Settings Module's "checked" parameter in the
Configuration Reference Guide.
BIOS-based environments
Added LOG_events for profiling performance
The following defects were resolved:
ID
Headline
SDSCM00014413
xdcpaths.mak requires FC installation in ".lite" release
SDSCM00014540
CE OSAL requires presence of dsplink.dsp package even if it's used
in a DSP/BIOS-only setting
SDSCM00015336
Scale example's SCALE_Params struct does not have the required
IALG_Params struct as its first element
The following enhancements were resolved:
ID
Headline
SDSCM00013759
CMEM should support multiple processes
SDSCM00014703
Add Memory_cacheWb() to OSAL
1.10
General
Updated to C6x Codegen 6.0.7
Updated to DSP/BIOS 5.31.01
Updated to Framework Components 1.10.01
Updated to XDAIS 5.10, which includes XDM 1.00 beta
interfaces
CE Runtime
Added new methods to ti.sdo.ce.ICodec interface
(getCreationStackSize(),
getDaramScratchSize(), and
getSaramScratchSize()) to make Server configuration
easier. When codecs implement these methods, the XDC Tools
are able to either:
Auto-generate the DSKT2 scratch configuration, or
Validate the scratch config (if the server integrator
wants to continue explicitly configuring those values).
VISA
Added support for XDM 1.00 Beta interfaces. (Previous XDM
0.9 interfaces continue to be supported)
SPI (System Programming Interfaces)
Added VISA_setContext() and
VISA_getContext() services for stub/skeleton/API authors.
Documentation
Added "Adapter" application note describing how to integrate
non-XDM codecs, as well as a technique for adding pre- and post-
processing steps to existing codecs without modifying them.
Examples
Added new, Linux-only example demonstrating how users can
create a shared library from a single configuration, which can
then be used by multiple applications.
Added a new example, explicitly describing the steps taking
during configuration to better demonstrate the necessary
configuration steps for users who want to integrate this into
their own, custom build flows.
Modified example codecs, when possible, to utilize copy
codecs now distributed in XDAIS 5.10. In this way, it's more
clearly described what little XDC packaging is required to
integrate an already XDC packaged Codec (independant of CE) into
the CE framework.
Defects
SDSCM00010422 - CE and CMEM should set the close-on-exec
flag on any open file handles
SDSCM00005810 - Additional C++ testing required
SDSCM00004993 - GT no longer supports wildcards as second
character
SDSCM00004805 - GT computes (a lot) during GT_?trace()
Enhancements
SDSCM00010364 - GT needs productized
SDSCM00008121 - not possible to properly size RMS thread's
stack
SDSCM00007887 - Support VISA_getContext/setContext SPIs
SDSCM00006616 - CE should ensure unique UUIDs
SDSCM00003992 - Add pre- and/or post- process example to
codecs
SDSCM00002920 - ICodec should have a getScratchSize method
Minor updates to the Codec Engine Application Developer's
Guide (SPRUE67A)
1.01
General
Many trace strings were modified/added.
C64P libraries built with 6.0.3 compiler.
VISA Classes
Audio Encoding support has been added
Better compliance checking of "size" field. This field
must be set correctly in the various VISA APIs, as it is
now used to determine how much data to provide to the
codecs.
Related to previous bullet, added extended XDM support to
VIDDEC, VIDENC, AUDDEC, IMGDEC, and SPHDEC classes. There are
limits to the size of the extended structures, and they must not
contain pointers in the extended structures.
outArgs fixed to be provided in the case of a failed
process() call (enabling inspection of extendedError).
Removed cache alignment validation of input buffers. When the
application can ensure cache coherence, these buffers need not be
aligned.
Documentation
Minor updates to the Codec Engine Application Developer's
Guide (SPRUE67A)
This Codec Engine release is not suitable for BIOS 5-based DVSDKs.
DVSDK users should continue to use the BIOS 5-based Codec Engine 2.x
releases.
The Codec Engine packages are available in the "packages/"
subdirectory of the product. If you have a previous release of the
Codec Engine product, you can install this release next to it, and
modify your application and/or server builds to use this newer release.
If you're using the EZSDK, this can be done by setting the
CE_INSTALL_DIR variable in the Rules.make file at the
top of the EZSDK distribution directory.
Compatibility Breaks!
CE 3.24.00.08 requires system integrators to update to XDC Tools
3.25.00.48 (or newer).
CE 3.24.00.08 requires system integrators update to SysLink
undefined (or compatible).
CE 3.24.00.08 requires system integrators update to Framework
Components 3.24.00.09 (or compatible).
CE 3.24.00.08 requires system integrators update to OSAL
1.24.00.09 (or compatible).
CE 3.24.00.08 requires system integrators update to XDAIS
7.24.00.04 (or compatible).
CE 3.24.00.08 requires system integrators update to Linux Utils
undefined (or compatible).
CE 3.24.00.08 requires system integrators update to BIOS
6.35.01.29 (or compatible).
CE 3.24.00.08 requires system integrators update to IPC
1.25.02.12 (or compatible).
Note, if you're upgrading from a release earlier than Codec Engine undefined, be
sure to review the Upgrade section for each of the releases between
your current Codec Engine release and this one. Previous release notes are
available in the relnotes_archive directory.
The table below describes each package's compatibility with the
previous release (codec_engine_3_23_00_07). Compatibility keys highlighted in red
are incompatible with the previous release.
Note that CE 3.x has undergone internal changes from
CE 2.x releases, and as such, configuration scripts - especially on
BIOS-based environments may require significant rework. Please consult
the CE example applications, which include config scripts, for reference.
If migrating from a release prior to codec_engine_3_23_00_07, consult previous
releases available in the relnotes_archive directory.
Compatibility Key Definitions
Compatibility keys are intentionally independent of Marketing product
numbers and are intended to:
Enable tooling to identify incompatibilities between components,
and
Convey a level of compatibility between different releases to
set end user expectations.
Compatibility keys are composed of 3 comma-delimited numbers - M,S,R
- where:
M = Major. A difference in M indicates a break in
compatibility.
S = Source. A difference in S indicates source
compability. That is, the user's source doesn't require change, but
does require rebuilding.
R = Radix. A difference in R indicates an introduction
of new features, but compatibility with previous interfaces has not
broken. If libraries are provided by the package, an application
must re-link with the new libraries, but not rebuild from source.
This release was built and validated against using the following software
components. Please use the versions below, or compatible:
Framework Components 3.24.00.09
XDAIS 7.24.00.04
Linux Utils undefined
IPC 1.25.02.12
OSAL 1.24.00.09
XDCtools 3.25.00.48
SysLink undefined
SYS/BIOS 6.35.01.29
EDMA3 Resource Manager 02.11.05.02
TI816X PSP undefined
TI814X PSP undefined
TI811X PSP undefined
OMAP3 PSP undefined
Pre-built binaries were built with the following toolchains:
ti.targets.C64P - 7.2.0
ti.targets.C674 - 7.2.0
ti.targets.arm.elf.A8F - 5.0.1
ti.targets.arm.elf.M3 - 5.0.1
ti.targets.arm.elf.M4 - 5.0.1
ti.targets.elf.C64P - 7.2.0
ti.targets.elf.C64T - 7.2.0
ti.targets.elf.C66 - 7.2.0
ti.targets.elf.C674 - 7.2.0
This release was validated using the following hardware platforms. Note
that more devices may be supported, but validation was only performed on
a subset:
OMAP3530 EVM
multiprocessor configuration, running Linux (A8)
and SYS/BIOS (DSP)
single processor A8 configuration, running Linux
single processor DSP configuration, running SYS/BIOS
C6472
single processor DSP configuration, running SYS/BIOS
This product's version follows a version format, M.mm.pp.bb,
where M is a single digit Major number, mm is 2 digit
minor number, pp is a 2 digit patch number, and b is an
unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the
product version is encoded in the top level directory,
ex. codec_engine_3_24_00_08.
Subsequent releases of patch upgrades will be identified by the patch
number, ex. CE 3.24.01.XX with directory codec_engine_3_24_01_XX.
Typically, these patches only include critical bug fixes.