![]() |
![]() |
This header defines all types, constants, and functions shared by all implementations of the image encoder algorithms.
#include <ti/xdais/ialg.h>
#include <ti/xdais/xdas.h>
#include "xdm.h"
Go to the source code of this file.
Data Structures | |
struct | IIMGENC1_Obj |
This must be the first field of all IIMGENC1 instance objects. More... | |
struct | IIMGENC1_Params |
Defines the creation time parameters for all IIMGENC1 instance objects. More... | |
struct | IIMGENC1_DynamicParams |
This structure defines the algorithm parameters that can be modified after creation via control() calls. More... | |
struct | IIMGENC1_InArgs |
Defines the input arguments for all IIMGENC1 instance process() function. More... | |
struct | IIMGENC1_Status |
Defines instance status parameters. More... | |
struct | IIMGENC1_OutArgs |
Defines the run time output arguments for all IIMGENC1 instance objects. More... | |
struct | IIMGENC1_Fxns |
Defines all of the operations on IIMGENC1 objects. More... | |
Defines | |
#define | IIMGENC1_EOK XDM_EOK |
#define | IIMGENC1_EFAIL XDM_EFAIL |
#define | IIMGENC1_EUNSUPPORTED XDM_EUNSUPPORTED |
Typedefs | |
typedef struct IIMGENC1_Obj | IIMGENC1_Obj |
This must be the first field of all IIMGENC1 instance objects. | |
typedef struct IIMGENC1_Obj * | IIMGENC1_Handle |
Opaque handle to an IIMGENC1 objects. | |
typedef struct IIMGENC1_Params | IIMGENC1_Params |
Defines the creation time parameters for all IIMGENC1 instance objects. | |
typedef struct IIMGENC1_DynamicParams | IIMGENC1_DynamicParams |
This structure defines the algorithm parameters that can be modified after creation via control() calls. | |
typedef struct IIMGENC1_InArgs | IIMGENC1_InArgs |
Defines the input arguments for all IIMGENC1 instance process() function. | |
typedef struct IIMGENC1_Status | IIMGENC1_Status |
Defines instance status parameters. | |
typedef struct IIMGENC1_OutArgs | IIMGENC1_OutArgs |
Defines the run time output arguments for all IIMGENC1 instance objects. | |
typedef IALG_Cmd | IIMGENC1_Cmd |
Defines the control commands for the IIMGENC1 module. | |
typedef struct IIMGENC1_Fxns | IIMGENC1_Fxns |
Defines all of the operations on IIMGENC1 objects. |