Data Structures | Defines | Typedefs | Functions | Variables

Engine.h File Reference


Detailed Description

The Codec Engine Runtime. Provides the user an inteface to open and manipulate an Engine which can instantiate and communicate with XDAIS algorithms that run either on the local CPU or on a "remote" Server.

#include <ti/sdo/ce/Server.h>
#include <ti/sdo/ce/ipc/Comm.h>
#include <ti/xdais/ialg.h>
#include <ti/sdo/ce/node/node.h>
#include <stddef.h>
#include <stdio.h>
Include dependency graph for Engine.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  Engine_Attrs
 Attributes of an Engine. More...
struct  Engine_AlgInfo
 Properties of an Engine algorithm. More...
struct  Engine_DllAlgDesc
 Discriptor for a dynamically loaded codec. A dynamic library for a codec must export a function that fills in a structure of this type. More...
struct  Engine_DllAlgParams
 This structure is passed to Engine_addAlg(), and contains parameters to create a dynamic codec with. More...

Defines

#define Engine_MODNAME   "ti.sdo.ce.Engine"
 Name to pass to Diags_setMask() to enable logging for Engine functions. For example, Diags_setMask(Engine_MODNAME"+EX1234567"); turns on all Log statements in this module. Diags_setMask() must be called after initialization to take effect.
#define Engine_EOK   0
#define Engine_EEXIST   1
#define Engine_ENOMEM   2
#define Engine_EDSPLOAD   3
#define Engine_ENOCOMM   4
#define Engine_ENOSERVER   5
#define Engine_ECOMALLOC   6
#define Engine_ERUNTIME   7
#define Engine_ECODECCREATE   8
#define Engine_ECODECSTART   9
#define Engine_EINVAL   10
#define Engine_EBADSERVER   11
#define Engine_ENOTAVAIL   12
#define Engine_EWRONGSTATE   13
#define Engine_EINUSE   14
#define Engine_ENOTFOUND   15
#define Engine_ETIMEOUT   16
#define Engine_GETALGDESCFXN   "GetEngineAlgDesc"
 Name of function that a dynamically loaded codec must supply.

Typedefs

typedef struct Engine_Obj * Engine_Handle
 Opaque handle to an engine.
typedef Int Engine_Error
 Engine error code.
typedef struct Engine_Attrs Engine_Attrs
 Attributes of an Engine.
typedef struct Engine_AlgInfo Engine_AlgInfo
 Properties of an Engine algorithm.
typedef struct Engine_DllAlgDesc Engine_DllAlgDesc
 Discriptor for a dynamically loaded codec. A dynamic library for a codec must export a function that fills in a structure of this type.
typedef Int(* Engine_GetAlgDescFxn )(Engine_DllAlgDesc *dllAlgDesc)
 Prototype of function that must be supplied by a dynamic codec library to fill in a Engine_DllAlgDesc structure.
typedef struct Engine_DllAlgParams Engine_DllAlgParams
 This structure is passed to Engine_addAlg(), and contains parameters to create a dynamic codec with.

Functions

Engine_Error Engine_add (String engineName, String remoteName)
 Add an Engine to the database of engines that can be opened with Engine_open()
Engine_Error Engine_addAlg (Engine_Handle engine, String location, Engine_DllAlgParams *pAlgParams)
 Dynamically add an algorithm to an Engine instance.
Engine_Error Engine_removeAlg (Engine_Handle engine, String name)
 Dynamically remove an algorithm from an Engine instance.
Void Engine_close (Engine_Handle engine)
 Close an Engine.
Engine_Handle Engine_open (String name, Engine_Attrs *attrs, Engine_Error *ec)
 Open an Engine.
Int Engine_fwriteTrace (Engine_Handle engine, String prefix, FILE *out)
 Write Server's trace buffer to specifed file stream.
Engine_Error Engine_getAlgInfo (String name, Engine_AlgInfo *algInfo, Int index)
 Get details of an algorithm configured into an engine.
Int Engine_getCpuLoad (Engine_Handle engine)
 Get Server's cpu usage in percent.
Engine_Error Engine_getLastError (Engine_Handle engine)
 Get error code of the last failed operation.
String Engine_getName (Engine_Handle engine)
 Get the name of an opened engine.
Engine_Error Engine_getNumAlgs (String name, Int *numAlgs)
 Get the number of algorithms configured into an Engine.
Server_Handle Engine_getServer (Engine_Handle engine)
 Get handle to an Engine's Server.
UInt32 Engine_getUsedMem (Engine_Handle engine)
 Get Server's total memory usage.
Engine_Error Engine_remove (String engineName)
 Remove an engine from the list of engines that can be opened.
Int Engine_setTrace (Engine_Handle engine, String mask)
 Set Server's trace mask.

Variables

Engine_Attrs Engine_ATTRS
 Default engine attributes.
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated