![]() |
![]() |
The Codec Engine Runtime. Provides the user an inteface to open and manipulate an engine which can instantiate and communicate with xDAIS algorithms that run either on the local CPU or on a "remote" DSP Server.
#include <ti/sdo/ce/Server.h>#include <ti/sdo/ce/ipc/Comm.h>#include <ti/xdais/ialg.h>#include <ti/sdo/ce/node/node.h>#include <stddef.h>#include <stdio.h>

Go to the source code of this file.
Data Structures | |
| struct | Engine_Attrs |
| Attributes of an Engine. More... | |
| struct | Engine_AlgInfo |
| Properties of an Engine algorithm. More... | |
Defines | |
| #define | Engine_GTNAME "CE" |
| Trace name for the Engine module. | |
| #define | Engine_EOK 0 |
| #define | Engine_EEXIST 1 |
| #define | Engine_ENOMEM 2 |
| #define | Engine_EDSPLOAD 3 |
| #define | Engine_ENOCOMM 4 |
| #define | Engine_ENOSERVER 5 |
| #define | Engine_ECOMALLOC 6 |
| #define | Engine_ERUNTIME 7 |
| #define | Engine_ECODECCREATE 8 |
| #define | Engine_ECODECSTART 9 |
| #define | Engine_EINVAL 10 |
| #define | Engine_EBADSERVER 11 |
| #define | Engine_ENOTAVAIL 12 |
| #define | Engine_EWRONGSTATE 13 |
| #define | Engine_EINUSE 14 |
| #define | Engine_ENOTFOUND 15 |
| #define | Engine_ETIMEOUT 16 |
Typedefs | |
| typedef struct Engine_Obj * | Engine_Handle |
| Opaque handle to an engine. | |
| typedef Int | Engine_Error |
| Engine error code. | |
Functions | |
| Void | Engine_close (Engine_Handle engine) |
| Close an Engine. | |
| Engine_Handle | Engine_open (String name, Engine_Attrs *attrs, Engine_Error *ec) |
| Open an Engine. | |
| Int | Engine_fwriteTrace (Engine_Handle engine, String prefix, FILE *out) |
| Write Server's trace buffer to specifed file stream. | |
| Engine_Error | Engine_getAlgInfo (String name, Engine_AlgInfo *algInfo, Int index) |
| Get details of an algorithm configured into an engine. | |
| Int | Engine_getCpuLoad (Engine_Handle engine) |
| Get Server's cpu usage in percent. | |
| Engine_Error | Engine_getLastError (Engine_Handle engine) |
| Get error code of the last failed operation. | |
| String | Engine_getName (Engine_Handle engine) |
| Get the name of an opened engine. | |
| Engine_Error | Engine_getNumAlgs (String name, Int *numAlgs) |
| Get the number of algorithms configured into an engine. | |
| Server_Handle | Engine_getServer (Engine_Handle engine) |
| Get handle to an Engine's server. | |
| UInt32 | Engine_getUsedMem (Engine_Handle engine) |
| Get Server's total memory usage. | |
| Int | Engine_setTrace (Engine_Handle engine, String mask) |
| Set Server's trace mask. | |
Variables | |
| Engine_Attrs | Engine_ATTRS |
| Default engine attributes. | |