![]() |
![]() |
The "Generic Tracing" module. Provides producers of content the ability to, in a runtime-independant way, add tracing. Also provides consumers of trace-enabled content the mechanisms necessary to enable/disable the various trace statements.
Go to the source code of this file.
Data Structures | |
struct | GT_Mask |
Object representing a GT module instance. More... | |
Defines | |
#define | GT_ENTER ((UInt8)0x01) |
Mask for tracing entry and exit points within functions. | |
#define | GT_1CLASS ((UInt8)0x02) |
#define | GT_2CLASS ((UInt8)0x04) |
#define | GT_3CLASS ((UInt8)0x08) |
#define | GT_4CLASS ((UInt8)0x10) |
#define | GT_5CLASS ((UInt8)0x20) |
User mask 5. By convention, used for benchmarking related tracing. | |
#define | GT_6CLASS ((UInt8)0x40) |
User mask 6. By convention, used for internal warning related tracing. | |
#define | GT_7CLASS ((UInt8)0x80) |
User mask 7. By convention, used for internal error related tracing. | |
#define | GT_create(mask, modName) _GT_create((mask), (modName)) |
#define | GT_set(str) _GT_set(str) |
#define | GT_0trace(mask, classId, format) |
#define | GT_1trace(mask, classId, format, arg1) |
#define | GT_2trace(mask, classId, format, arg1, arg2) |
#define | GT_3trace(mask, classId, format, arg1, arg2, arg3) |
#define | GT_4trace(mask, classId, format, arg1, arg2, arg3, arg4) |
#define | GT_5trace(mask, classId, format, arg1, arg2, arg3, arg4, arg5) |
#define | GT_6trace(mask, classId, format, arg1, arg2, arg3, arg4, arg5, arg6) |
Functions | |
Void | _GT_create (GT_Mask *mask, String modName) |
Initialize a GT mask. | |
Void | GT_init (Void) |
Initialize the GT module. | |
Void | _GT_set (String str) |
Modify the current trace mask settings. | |
Int | _GT_trace (GT_Mask *mask, Int classId, String format,...) |
Conditionally emit a trace statement. |