TraceUtil.h File Reference


Detailed Description

The Codec Engine utility module for trace.

#include <ti/sdo/ce/Engine.h>
Include dependency graph for TraceUtil.h:

Go to the source code of this file.

Defines

#define TRACEUTIL_SUCCESS   0
#define TRACEUTIL_FAILURE   -1

Functions

Int TraceUtil_start (String engineName)
 Begin using the TraceUtil module; create thread that periodically collects DSP trace.
Int TraceUtil_stop (Void)
 Finish using the TraceUtil module, stop the collecting thread.
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2009, Texas Instruments Incorporated