1 /*
2 * Copyright (c) 2016 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * */
13 /*
14 * ======== Rta.xdc ========
15 */
16
17 package xdc.runtime;
18
19 /*!
20 * ======== Rta ========
21 * The Rta module contains target and configuration code for providing RTA
22 * support.
23 *
24 * The 'Command' enum defines the available control commands, and the
25 * 'CommandPacket' structure defines the format of commands received from
26 * the host.
27 *
28 * All commands should send back a response, even if only to acknowledge
29 * receipt and completion of the command. The format of the response
30 * is defined by the 'ResponsePacket' structure.
31 *
32 * The Rta_processCommand can be used to process commands received from a
33 * host to call the appropriate API. Alternatively, the individual APIs can
34 * be called if not all of the defined commands are used.
35 */
36 @DirectCall
37 module Rta {
38
39 /*! Logged when the Agent receives a command */
40 config Log.Event LD_cmdRcvd = {
41 mask: Diags.USER2,
42 msg: "LD_cmdRcvd: Received command: %d, arg0: 0x%x, arg1: 0x%x"
43 };
44
45 /*! Logged when a diags mask is changed */
46 config Log.Event LD_writeMask = {
47 mask: Diags.USER2,
48 msg: "LD_writeMask: Mask addres: 0x%x, New mask value: 0x%x"
49 };
50
51 /*! Assert if logger id in control command is invalid. */
52 config Assert.Id A_invalidLogger = {
53 msg: "A_invalidLogger: The logger id %d is invalid."
54 };
55
56 /*! Error raised if Agent receives an invalid command. */
57 config Error.Id E_badCommand = {
58 msg: "E_badCommand: Received invalid command, id: %d."
59 };
60
61 /*! Command ids */
62 enum Command : Int {
63 Command_READ_MASK = 0,
64 Command_WRITE_MASK = 1,
65 Command_LOGGER_OFF = 2,
66 Command_LOGGER_ON = 3,
67 Command_GET_CPU_SPEED = 4,
68 Command_RESET_LOGGER = 5,
69 Command_CHANGE_PERIOD = 6,
70 Command_START_TX = 7,
71 Command_STOP_TX = 8
72 };
73
74 /*!
75 * Structure of command received from host
76 * TODO - Either the types should be changed to 32-bits, or the packet
77 * size information should be added to the RTA XML file.
78 */
79 struct CommandPacket {
80 Command cmdId;
81 UArg arg0;
82 UArg arg1;
83 }
84
85 /*! Structure of response packet sent back to host */
86 struct ResponsePacket {
87 Command cmdId;
88 UArg resp0;
89 UArg resp1;
90 }
91
92 /*!
93 * ======== dataTransportClassName =========
94 * The name of the xdc.rta.IDataTransport class to use.
95 *
96 * The class specified here can be used on the host for reading RTA data
97 * from this target application.
98 */
99 config String dataTransportClassName = "";
100
101 /*!
102 * ======== controlTransportClassName ========
103 * The name of the xdc.rta.IControlTransport class to use.
104 *
105 * The class specified here can be used on the host for communicating with
106 * this target application to send control commands and receive responses.
107 */
108 config String controlTransportClassName = "";
109
110 /*!
111 * ======== processCommand ========
112 * Executes a command packet and prepares the response packet.
113 *
114 * This API will execute the command specified by the command packet
115 * argument, and will store the response information in the response
116 * packet argument.
117 *
118 * @param(cmd) The CommandPacket to execute.
119 * @param(resp) The ResponsePacket to populate with the response.
120 */
121 Void processCommand(CommandPacket *cmd, ResponsePacket *resp);
122
123 /*!
124 * ======== acknowledgeCmd ========
125 */
126 Void acknowledgeCmd(ResponsePacket *resp);
127
128 /*!
129 * ======== readMask ========
130 */
131 Void readMask(ResponsePacket *resp, UArg addr);
132
133 /*!
134 * ======== writeMask ========
135 */
136 Void writeMask(ResponsePacket *resp, UArg addr, UArg val);
137
138 /*!
139 * ======== enableLog ========
140 */
141 Void enableLog(ResponsePacket *resp, UArg log);
142
143 /*!
144 * ======== disableLog ========
145 */
146 Void disableLog(ResponsePacket *resp, UArg log);
147
148 /*!
149 * ======== getCpuSpeed ========
150 */
151 Void getCpuSpeed(ResponsePacket *resp);
152
153 /*!
154 * ======== resetLog ========
155 */
156 Void resetLog(ResponsePacket *resp, UArg log);
157
158 /*!
159 * ======== changePeriod ========
160 */
161 Void changePeriod(ResponsePacket *resp, UArg period);
162
163 /*!
164 * @_nodoc 165 * ======== genRta ========
166 * Generates the Rta XML file.
167 */
168 function genRta(outputFileName);
169
170 }
171 /*
172 * @(#) xdc.runtime; 2, 1, 0,0; 5-8-2019 15:48:09; /db/ztree/library/trees/xdc/xdc-G16/src/packages/
173 */
174