1 /*
2 * Copyright (c) 2008-2017 Texas Instruments Incorporated
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * */
13 /*
14 * ======== Error.xdc ========
15 */
16
17 /*!
18 * ======== Error ========
19 * Runtime error manager
20 *
21 * The `Error` module provides mechanisms for raising, checking, and
22 * handling errors in a program. At the configuration time, you can use the
23 * parameters `{@link Error#policy Error.policy}`,
24 * `{@link Error#policyFxn Error.policyFxn}` and
25 * `{@link Error#raiseHook Error.raiseHook}` to specify what happens when an
26 * error takes place. You can control how much debugging information is
27 * available in that case, while also controlling the memory footprint that the
28 * `Error' module adds to the program.
29 *
30 * Module producers use this module to define specific error types and
31 * reference these when raising an error. Each error type has a custom error
32 * message and can be parameterized with up to `{@link #NUMARGS}` arguments. A
33 * generic error type is provided for raising errors when not in a module.
34 *
35 * Use the `{@link #check Error_check()}` function in your application or
36 * module to determine if an error has been raised in a function that takes an
37 * `{@link #Block Error_Block}` as an argument. It is important to understand
38 * that it is the caller's responsibility to check the error block after
39 * calling such a function. Otherwise, a raised error may go undetected, which
40 * could compromise the integrity of the system. For example:
41 *
42 * @p(code) 43 * Task_create(..., &eb);
44 *
45 * if (Error_check(&eb)) {
46 * ...an error has been raised...
47 * }
48 * @p 49 *
50 * The function assigned to the parameter
51 * `{@link Error#policyFxn Error.policyFxn}` is the central part of the
52 * error handling mechanism in this module. Most of the users will either leave
53 * this parameter at its default value, or select one of the alternative
54 * implementations that are included with the `Error` module. However, this
55 * configuration parameter also allows users to completely take over the error
56 * handling by setting this parameter to their own implementation. In that
57 * case, we recommend that users first review the included implementations,
58 * and base their implementation on one of these function. The included
59 * implementations are `{@link #policyDefault}`, `{@link #policyMin}`, and
60 * `{@link #policySpin}`.
61 *
62 * The `{@link #raiseHook Error.raiseHook}` configuration parameter allows
63 * a configured function to be invoked when an error is raised.
64 * This function is invoked from the default implementation of
65 * `{@link Error#policyFxn Error.policyFxn}`. Therefore, if a different
66 * implementation of `Error.policyFxn` is used, the function specified by
67 * `Error.raiseHook` may or may not be called.
68 * This function is passed a pointer to the error's error block and makes it
69 * easy to manage all errors from a common point. For example, you can
70 * trap any error (fatal or not) by simply setting a breakpoint in this
71 * function. You can use the following functions to extract information
72 * from an error block.
73 *
74 * @p(blist) 75 * - `{@link #getData Error_getData()}`
76 * - `{@link #getCode Error_getCode()}`
77 * - `{@link #getId Error_getId()}`
78 * - `{@link #getMsg Error_getMsg()}`
79 * - `{@link #getSite Error_getSite()}`
80 * @p 81 *
82 * The Error module provides facilities for handling errors, but the Log
83 * module also provides features for logging error events. These are separate
84 * concepts; however, to ensure that users do not have to both raise and log
85 * an error, the Error module will automatically log an error event when one
86 * is raised. The Error module logs the standard {@link Log#L_error} event,
87 * passing it the error message and arguments.
88 *
89 * The error event is logged to the Error module's logger using the Error
90 * module's diags mask. Logging of errors is enabled by default in the diags
91 * mask, but the event will not be logged unless a logger is configured for
92 * the Error module as well.
93 *
94 * To make the error event appear as though it is coming from the module which
95 * called Error_raise, the event is logged with the caller's module id and
96 * with the caller's call site information.
97 *
98 * @a(Examples) 99 * Example 1: The following example shows how a module, named ModA,
100 * defines a custom error type and shows how this error is raised by
101 * the module. The module defines an `Id` of `E_notEven` in its module
102 * specification file (in this case, `ModA.xdc`). The error's message
103 * string takes only one argument. The module also defines a `mayFail()`
104 * function that takes an error block. In the module's C source file,
105 * the function checks for the error condition and raises the error if
106 * needed.
107 *
108 * This is part of ModA's XDC specification file for the module:
109 *
110 * @p(code) 111 * config xdc.runtime.Error.Id E_notEven = {
112 * msg: "expected an even number (%d)"
113 * };
114 *
115 * Void mayFail(Int x, xdc.runtime.Error.Block *eb);
116 * @p 117 *
118 * This is part of the C code for the module:
119 *
120 * @p(code) 121 * Void ModA_mayFail(Int x, Error_Block *eb)
122 * {
123 * if ((x % 2) != 0) {
124 * Error_raise(eb, ModA_E_notEven, x, 0);
125 * ...add error handling code here...
126 * return;
127 * }
128 * ...
129 * }
130 * @p 131 *
132 * @p(html) 133 * <hr />
134 * @p 135 *
136 * Example 2: The following C code supplies an error block to a function
137 * that requires one and tests the error block to see if the function
138 * raised an error. Note that an error block must be initialized before
139 * it can be used and same error block may be passed to several functions.
140 *
141 * @p(code) 142 * #include <xdc/runtime/Error.h>
143 * #include <ti/sysbios/knl/Task.h>
144 * Error_Block eb;
145 * Task_Handle tsk;
146 *
147 * Error_init(&eb);
148 * tsk = Task_create(..., &eb);
149 *
150 * if (Error_check(&eb)) {
151 * ...an error has been raised...
152 * }
153 * @p 154 *
155 * @p(html) 156 * <hr />
157 * @p 158 *
159 * Example 3: The following C code shows that you may pass a special constant
160 * `Error_ABORT` in place of an error block to a function requiring an error
161 * block. In this case, if the function raises an error, the program is aborted
162 * (via `{@link System#abort xdc_runtime_System_abort()}`), thus execution
163 * control will never return to the caller.
164 *
165 * @p(code) 166 * #include <xdc/runtime/Error.h>
167 * #include <ti/sysbios/knl/Task.h>
168 *
169 * tsk = Task_create(..., Error_ABORT);
170 * ...will never get here if an error was raised in Task_create...
171 * @p 172 *
173 * @p(html) 174 * <hr />
175 * @p 176 *
177 * Example 4: The following C code shows that you may pass a special constant
178 * `Error_IGNORE` in place of an error block to a function requiring an error
179 * block. The purpose of this constant is to avoid allocating an error block on
180 * stack in the use case where the caller is not checking the error block after
181 * the call returns.
182 * In this example, the caller only checks the returned value but not the error
183 * block. If the function raises an error, the program will return to the
184 * caller, assuming `Error_policy` is set to `{@link #Policy UNWIND}`.
185 *
186 * @p(code) 187 * #include <xdc/runtime/Error.h>
188 * #include <ti/sysbios/knl/Task.h>
189 *
190 * tsk = Task_create(..., Error_IGNORE);
191 * if (tsk != NULL) {
192 * ...
193 * }
194 * @p 195 *
196 * @p(html) 197 * <hr />
198 * @p 199 *
200 * Example 5: The following C code shows how to write a function that
201 * is not part of a module and that takes an error block and raises
202 * the generic error type provided by the Error module. Note, if the
203 * caller passes `Error_ABORT` for the error block or if the error policy is
204 * `{@link #Policy TERMINATE}`, then the call to
205 * `{@link #raise Error_raise()}` will call
206 * `{@link System#abort xdc_runtime_System_abort()}` and never return.
207 *
208 * @p(code) 209 * #include <xdc/runtime/Error.h>
210 *
211 * Void myFunc(..., Error_Block *eb)
212 * {
213 * ...
214 *
215 * if (...error condition detected...) {
216 * String myErrorMsg = "my custom error message";
217 * Error_raise(eb, Error_E_generic, myErrorMsg, 0);
218 * ...add error handling code here...
219 * return;
220 * }
221 * }
222 * @p 223 */
224 @DirectCall
225 @Template("./Error.xdt")
226
227 module Error {
228
229 /*!
230 * ======== Policy ========
231 * Error handling policies
232 *
233 * These constants are assigned to `{@link Error#policy Error.policy}` to
234 * control the flow of the program when an error is raised.
235 *
236 * @field(TERMINATE) All raised errors are fatal. A call to
237 * `{@link #raise Error_raise}` will never return to the caller. The
238 * program calls `System_abort` instead.
239 *
240 * @field(UNWIND) Errors are returned to the caller. A call to
241 * `{@link #raise Error_raise}` will return back to the caller.
242 */
243 enum Policy {
244 TERMINATE,
245 UNWIND
246 };
247
248 /*!
249 * ======== Desc ========
250 * Error descriptor
251 *
252 * Each type of error is defined with an error descriptor. This
253 * structure groups common information about the errors of this type.
254 *
255 * @field(msg) The error message using a `printf` style format string,
256 * but limited to `{@link #NUMARGS}` arguments.
257 * This format string together with the two arguments passed
258 * to `Error_raise`` are used to create a human readable
259 * error message.
260 *
261 * @field(code) A user assignable code, 0 by default. The user may
262 * optionally set this field during config to give the
263 * error a well-known numeric code.
264 */
265 metaonlystruct Desc {
266 String msg;
267 UInt16 code;
268 };
269
270 /*!
271 * ======== Id ========
272 * Error identifier
273 *
274 * Each type of error raised is defined with a metaonly
275 * `{@link Error#Desc}`. An `Error_Id` is a 32-bit target value that
276 * encodes the information in the `Desc`. Target programs use
277 * `Error_Id` values to "raise" and check for specific errors.
278 *
279 * @a(Warning) `{@link #Id}` values may vary among different
280 * configurations of an application. For example, the addition of a
281 * new module to a program may result in a different absolute value for
282 * `{@link #E_generic}`. If you need error numbers that remain
283 * invariant, use the user definable `{@link #Desc Desc.code}` field.
284 */
285 @Encoded typedef Desc Id;
286
287 /*!
288 * ======== HookFxn ========
289 * Function called whenever an error is raised
290 *
291 * The first parameter and only parameter passed to this function is a
292 * pointer to an `Error_Block`. Even if the client passes a `NULL` error
293 * block pointer to `{@link #raise Error_raise}`, this parameter passed
294 * to this "hook" function is always `non-NULL`.
295 */
296 typedef Void (*HookFxn)(Block *);
297
298 /*!
299 * ======== NUMARGS ========
300 * Maximum number of arguments supported by an error
301 */
302 const Int NUMARGS = 2;
303
304 /*!
305 * ======== Data ========
306 * Error args
307 *
308 * The two arguments (arg1, arg2) passed to `{@link #raise}` are
309 * stored in one of these arrays within the associated Error_Block.
310 * To access these arguments use `{@link #getData}` to obtain a
311 * pointer to the Error_Block's Data array.
312 *
313 * @see #getData
314 */
315 struct Data {
316 IArg arg[NUMARGS];
317 }
318
319 /*!
320 * ======== Block ========
321 * Error block
322 *
323 * An opaque structure used to store information about errors once raised.
324 * This structure must be initialized via `{@link #init Error_init()}`
325 * before being used for the first time.
326 */
327 @Opaque struct Block {
328 UInt16 unused; /* for backward compatibility (was code) */
329 Data data; /* arguments passed to raise() */
330 Id id; /* id passed to raise() */
331 CString msg; /* msg associated with id */
332 Types.Site site; /* info about Error_raise call site */
333 };
334
335 /*!
336 * ======== IGNORE ========
337 * A pointer to a special Error_Block used when the caller does not want to
338 * check Error_Block
339 *
340 * This constant should be used when the caller does not plan to check
341 * `Error_Block` after the call returns, but wants the call to return even
342 * in the case when an error is raised. `{@link #policy Error_policy}` is
343 * still in effect and the application will still terminate when an error
344 * is raised if `Error_policy` is not set to
345 * `{@link #Policy Error_UNWIND}`.
346 */
347 const Block IGNORE;
348
349 /*!
350 * ======== ABORT ========
351 * A special Error_Block pointer that terminates the application in case of
352 * an error
353 *
354 * This constant has the same effect as passing `NULL` in place of an
355 * `Error_Block`. If an error is raised when `Error_ABORT` is passed, the
356 * application terminates regardless of `{@link #policy Error_policy}`.
357 */
358 const Block ABORT;
359
360 /*!
361 * ======== PolicyFxn ========
362 * Error policy function signature
363 *
364 * @a(Parameters) 365 * A policy function is passed the following parameters:
366 * @p(dlist) 367 * - `eb`
368 * A pointer to an `{@link #Block Error_Block}` structure to be
369 * initialized using the subsequent arguments. This pointer may
370 * be `NULL`.
371 * - `modId`
372 * The module ID of the module calling
373 * `{@link #raise Error_raise()}`
374 * - `fileName`
375 * A string naming the source file which made the call to
376 * `{@link #raise Error_raise()}`
377 * - `lineNumber`
378 * An integer line number within the file named above where
379 * the call `{@link #raise Error_raise()}` occured
380 * - `errId`
381 * The `{@link #Id Error_Id}` of the error being raised
382 * - `arg1` and `arg2`
383 * Two `IArg` arguments associated with the error being raised
384 * @p 385 */
386 typedef Void (*PolicyFxn)(Block *, Types.ModuleId, CString, Int, Id,
387 IArg, IArg);
388
389 /*!
390 * ======== policyFxn ========
391 * Error handler function
392 *
393 * This function is called to handle all raised errors but, unlike
394 * `{@link raiseHook}`, this function is responsible for completely
395 * handling the error (including calling `{@link #raiseHook raiseHook}`
396 * with an appropriately initialized `{@link #Block Error_Block}`, if
397 * `raiseHook` functionality is required).
398 *
399 * The default value is a function which, in addition to calling
400 * `raiseHook` with an initialized `Error_Block` structure, logs the
401 * error using this module's logger.
402 *
403 * Alternately, `{@link #policySpin}`, which simply loops
404 * indefinitely, can be used to minimize target footprint. Note, this
405 * function does NOT call `raiseHook`, and also ignores
406 * `{@link Error#policy Error.policy}`.
407 *
408 * The third implementation, `{@link #policyMin}` finds a middle ground
409 * between the two implementations above in terms of memory footprint and
410 * the available error information. Only the `{@link #Id Error_Id}` of the
411 * error being raised is available in the resulting `Error_Block`,
412 * `raiseHook` is not invoked, but `{@link Error#policy Error.policy}` is
413 * observed.
414 */
415 config PolicyFxn policyFxn = Error.policyDefault;
416
417 /*!
418 * ======== E_generic ========
419 * Generic error
420 *
421 * This error takes advantage of the $S specifier to allow for recursive
422 * formatting of the error message passed to error raise.
423 *
424 * For example, the following is possible:
425 * @p(code) 426 * Error_raise(eb, Error_E_generic, "Error occurred, code: %d", code);
427 * @p 428 *
429 * @see System#extendedFormats
430 * @see System#printf
431 */
432 config Id E_generic = {msg: "%$S"};
433
434 /*!
435 * ======== E_memory ========
436 * Out of memory error
437 *
438 * The first parameter must be the heap instance handle. The second
439 * parameter is the size of the object for which the allocation failed.
440 */
441 config Id E_memory = {msg: "out of memory: heap=0x%x, size=%u"};
442
443 /*!
444 * ======== E_msgCode ========
445 * Generic error that displays a string and a numeric value
446 */
447 config Id E_msgCode = {msg: "%s 0x%x"};
448
449 /*!
450 * ======== policy ========
451 * System-wide error handling policy
452 *
453 * You can use this parameter to decide at the configuration time what
454 * happens when an error is raised. The program can either call
455 * `System_abort()` or return back to the caller. The implementations of
456 * `{@link Error#policyFxn Error.policyFxn}` should consider this
457 * parameter, but some implementations may not do so to save the memory
458 * footprint (`Error_policySpin`, for example).
459 *
460 */
461 config Policy policy = UNWIND;
462
463 /*!
464 * ======== raiseHook ========
465 * The function to call whenever an error is raised
466 *
467 * If set to a non-`null` value, the referenced function is always
468 * called when an error is raised, even if the `Error` policy is
469 * `{@link #Policy TERMINATE}`. In rare cases, it is possible that a
470 * raised error does not trigger a call to `raiseHook`; see
471 * `{@link #maxDepth}`.
472 *
473 * Regardless of the current policy in use, raising an error by
474 * calling `{@link #raise Error_raise}` will always invoke the
475 * error raise hook function assigned to the
476 * `{@link #raiseHook Error.raiseHook}` configuration parameter, if the
477 * default `{@link Error#policyFxn Error.policyFxn}` implementation is
478 * used.
479 *
480 *
481 * By default, this function is set to `{@link #print Error_print}`
482 * which causes the error to be formatted and output via
483 * `{@link xdc.runtime.System#aprintf System_printf}`. Setting this
484 * configuration parameter to `null` indicates that no function hook
485 * should be called.
486 *
487 * @see #maxDepth
488 * @see #HookFxn
489 * @see #print
490 */
491 config HookFxn raiseHook = Error.print;
492
493 /*!
494 * ======== maxDepth ========
495 * Maximum number of concurrent calls to `{@link #raiseHook}`
496 *
497 * To prevent errors that occur in the raiseHook function from
498 * causing an infinite recursion, the maximum number of concurrent
499 * calls to `{@link #raiseHook}` is limited by `Error_maxDepth`. If
500 * the number of concurrent calls exceeds `Error_maxDepth`, the
501 * `raiseHook` function is not called.
502 *
503 * In multi-threaded systems, errors raised by separate threads may
504 * be detected as recursive calls to `raiseHook`. So, setting
505 * `Error.maxDepth` to a small value may - in rare instances - result in
506 * `errorHook` not being called for some raised errors.
507 *
508 * If it is important that all raised errors trigger a call to the
509 * `raiseHook` function, set `Error.maxDepth` to an impossibly large
510 * number (0xffff) and either ensure that the raise hook never calls a
511 * function that can raise an error or add checks in `raiseHook` to
512 * protect against "double faults".
513 */
514 config UInt16 maxDepth = 16;
515
516 /*!
517 * ======== check ========
518 * Return TRUE if an error was raised
519 *
520 * @param(eb) pointer to an `Error_Block`, `Error_ABORT` or `Error_IGNORE`
521 *
522 * @a(returns) 523 * If `eb` is non-`NULL` and `{@link #policy Error.policy} == UNWIND` and
524 * an error was raised on `eb`, this function returns `TRUE`. Otherwise,
525 * it returns `FALSE`.
526 */
527 Bool check(Block *eb);
528
529 /*!
530 * ======== getData ========
531 * Get an error's argument list
532 *
533 * @param(eb) non-`NULL` pointer to an `Error_Block`
534 *
535 * @a(returns) 536 * `getData` returns an array of type `{@link #Data}` with
537 * `{@link #NUMARGS}` elements containing the arguments provided
538 * at the time the error was raised.
539 *
540 * @see #raise
541 */
542 Data *getData(Block *eb);
543
544 /*!
545 * ======== getCode ========
546 * Get an error's code
547 *
548 * @param(eb) non-`NULL` pointer to an `Error_Block`
549 *
550 * @a(returns) 551 * `getCode` returns the error code associated with this error block.
552 *
553 * @see #raise
554 * @see #Desc
555 */
556 UInt16 getCode(Block *eb);
557
558 /*!
559 * ======== getId ========
560 * Get an error's id
561 *
562 * @param(eb) non-`NULL` pointer to an `Error_Block`
563 *
564 * @a(Warning) 565 * `Error_Id` values may vary among different configurations
566 * of an application. For example, the addition of a new module to a
567 * program may result in a different absolute value for
568 * `{@link #E_generic}`. If you need error numbers that remain
569 * invariant, use the user definable `{@link #Desc Desc.code}` field.
570 *
571 * @see #raise
572 * @see #Desc
573 */
574 Id getId(Block *eb);
575
576 /*!
577 * ======== getMsg ========
578 * Get an error's "printf" format string
579 *
580 * @param(eb) non-`NULL` pointer to an `Error_Block`
581 *
582 * @see #raise
583 * @see #Desc
584 */
585 CString getMsg(Block *eb);
586
587 /*!
588 * ======== getSite ========
589 * Get an error's call site info
590 *
591 * @param(eb) non-`NULL` pointer to an `Error_Block`
592 *
593 * @a(returns) 594 * `getSite` returns a pointer to an initialized
595 * `{@link Types#Site Types.Site}` structure. However, in the
596 * event that the call site was compiled with `xdc_FILE` defined to
597 * be `NULL` (to minimize string space overhead) the `file`
598 * field may be set to `NULL`.
599 *
600 * @see #raise
601 * @see #Desc
602 */
603 Types.Site *getSite(Block *eb);
604
605 /*!
606 * ======== idToCode ========
607 * Extract the user's error code associated with an `Error_Id`
608 *
609 * @param(id) `Error_Id` from which to extract the user defined
610 * code
611 * @_nodoc 612 */
613 @Macro UInt16 idToCode(Id id);
614
615 /*!
616 * ======== idToUid ========
617 * Extract the unique error id associated with an `Error_Id`
618 *
619 * @param(id) `Error_Id` from which to extract the system unique
620 * id associated with the specified `Error_Id`
621 * @_nodoc 622 */
623 @Macro UInt16 idToUid(Id id);
624
625 /*!
626 * ======== init ========
627 * Put an error block into its initial state
628 *
629 * To ensure reliable error detection, clients must call `init` for
630 * an `Error_Block` prior to any use.
631 *
632 * If the same Error Block is used multiple times, only the last error
633 * raised is retained.
634 *
635 * @param(eb) pointer to an `Error_Block`, `Error_ABORT` or `Error_IGNORE`
636 *
637 * If `eb` is `NULL` this function simply returns.
638 */
639 Void init(Block *eb);
640
641 /*!
642 * ======== print ========
643 * Print error using System.printf()
644 *
645 * This function prints the error using `System_printf()`. The output
646 * is on a single line terminated with a new line character and has the
647 * following form:
648 * @p(code) 649 * <site>: <file>, line <line_num>: <err_msg>
650 * @p 651 * where `<site>` is the module that raised the error, `<file>` and
652 * `<line_num>` are the file and line number of the containing the call
653 * site of the `Error_raise()`, and `<err_msg>` is the error message
654 * rendered with the arguments associated with the error.
655 *
656 * @param(eb) pointer to an `Error_Block`, `Error_ABORT` or `Error_IGNORE`
657 *
658 * If `eb` is `Error_ABORT` or `Error_IGNORE`, this function simply
659 * returns with no output.
660 *
661 * @a(Warning) 662 * This function is not protected by a gate and, as a result,
663 * if two threads call this method concurrently, the output of the two
664 * calls will be intermingled. To prevent intermingled error output,
665 * you can either wrap all calls to this method with an appropriate
666 * `Gate_enter`/`Gate_leave` pair or simply ensure that only one
667 * thread in the system ever calls this method.
668 */
669 Void print(Block *eb);
670
671 /*!
672 * ======== policyDefault ========
673 * Default implementation of the policyFxn
674 *
675 * This function is the implementation which is plugged in by default to
676 * the `{@link #policyFxn}`. It processes the error and logs it before
677 * returning to the caller or aborting - depending on the error policy
678 * `{@link #policy}`.
679 */
680 Void policyDefault(Block *eb, Types.ModuleId mod, CString file, Int line,
681 Id id, IArg arg1, IArg arg2);
682
683 /*!
684 * ======== policyMin ========
685 * Implementation of the policyFxn with a smaller footprint
686 *
687 * This function is a compromise between a debug-friendly
688 * `{@link #policyDefault}`, which offers more details about any raised
689 * errors, but requires a larger footprint, and `{@link #policySpin}`,
690 * which is small but does not display any debug information.
691 *
692 * This function returns to the caller, unless `{@link #policy}` is set to
693 * `TERMINATE`, or the `Error_Block` passed to it is `NULL`. If it returns,
694 * the only information available in the returned `Error_Block` is the
695 * error ID.
696 */
697 Void policyMin(Block *eb, Types.ModuleId mod, CString file, Int line,
698 Id id, IArg arg1, IArg arg2);
699
700 /*!
701 * ======== policySpin ========
702 * Lightweight implementation of the policyFxn
703 *
704 * This function is a lightweight alternative which can be plugged in to
705 * the `{@link #policyFxn}`. It just loops infinitely.
706 *
707 * @a(Warning) 708 * This function does not call `{@link #raiseHook}` and never returns to
709 * the caller. As a result, ANY error raised by the application will cause
710 * it to indefinitly hang.
711 */
712 Void policySpin(Block *eb, Types.ModuleId mod, CString file, Int line,
713 Id id, IArg arg1, IArg arg2);
714
715 /*!
716 * ======== raise ========
717 * Raise an error
718 *
719 * This function is used to raise an `Error` by writing call site,
720 * error ID, and error argument information into the `Error_Block`
721 * pointed to by `eb`.
722 *
723 * If `Error_raise` is called more than once on an `Error_Block` object,
724 * the previous error information is overwritten; only the last error
725 * is retained in the `Error_Block` object.
726 *
727 * In all cases, any configured `{@link #raiseHook Error.raiseHook}`
728 * function is called with a non-`NULL` pointer to a fully
729 * initialized `Error_Block` object.
730 *
731 * @param(eb) pointer to an `Error_Block`, `Error_ABORT` or `Error_IGNORE`
732 *
733 * If `eb` is `Error_ABORT` or
734 * `{@link #policy Error.policy} == TERMINATE`,
735 * this function does not return to the caller; after calling any
736 * configured `{@link #raiseHook}`, `System_abort` is called with the
737 * string `"xdc.runtime.Error.raise: terminating execution\n"`.
738 *
739 * @param(id) the error to raise
740 *
741 * This pointer identifies the class of error being raised; the error
742 * class indicates how to interpret any subsequent arguments passed to
743 * `{@link #raise}`.
744 *
745 * @param(arg1) error's first argument
746 *
747 * The argument interpreted by the first control character
748 * in the error message format string. It is ignored if not needed.
749 *
750 * @param(arg2) error's second argument
751 *
752 * The argument interpreted by the second control character
753 * in the error message format string. It is ignored if not needed.
754 */
755 @Macro Void raise(Block *eb, Id id, IArg arg1, IArg arg2);
756
757 /*! @_nodoc */
758 Void raiseX(Block *eb, Types.ModuleId mod, CString file, Int line,
759 Id id, IArg arg1, IArg arg2);
760
761 /*! @_nodoc EXPERIMENTAL */
762 Void setX(Block *eb, Types.ModuleId mod, CString file, Int line,
763 Id id, IArg arg1, IArg arg2);
764
765 internal:
766
767 struct Module_State {
768 UInt16 count;
769 };
770
771 }
772 /*
773 * @(#) xdc.runtime; 2, 1, 0,0; 5-8-2019 15:48:08; /db/ztree/library/trees/xdc/xdc-G16/src/packages/
774 */
775