SYS/BIOS 6.37.01.24 GA Release Notes

This release note is divided into the following sections:

Introduction, Documentation, What's New, Upgrading And Compatibility Information, Host Support, Dependencies, Device Support, Validation Information, Known Issues, Benchmarks, Versioning, Technical Support And Product Updates,


Introduction

SYS/BIOS 6.37.01.24 is a GA release of SYS/BIOS 6.37.00.

SYS/BIOS is a real-time operating system that provides pre-emptive deterministic multithreading. The SYS/BIOS releases introduce a completely new SYS/BIOS kernel and toolset. The SYS/BIOS releases include numerous major enhancements, including completely new kernel APIs. They also include compatibility layers and tooling to facilitate easy porting of applications developed on DSP/BIOS 5.x releases.

A number of tools and libraries that were provided as an integrated part of DSP/BIOS 5.x releases must now be downloaded separately to obtain a functional solution. It is essential for even experienced DSP/BIOS users to refer to the Getting Started Guide and to the Upgrading and Compatibility Information section for further details.

Please read the Getting Started Guide for help installing and setting up your environment to use SYS/BIOS 6.37.01.24.

back to top

Documentation

The following documentation is provided with this release. These documents are also available via the CCS Eclipse help table of contents.

License and manifest.
Additional online sources of documentation.

Release notes from previous releases are also available in the release notes archive directory.

back to top

What's New

SYS/BIOS 6.37.01.24 GA Release (this release).

Defects Fixed in SYS/BIOS 6.37.01.24 GA (Fixes since SYS/BIOS 6.37.00):
ID                               Headline
SDOCM00105612    The upper PIE (INTx.9-16) support is missing on SYSBIOS support for F2837x devices
SDOCM00105479    GNU target apps do not build if rts.gnu.ReentSupport module is disabled
SDOCM00105239    Incorrect cpu irq check in IntXbar config code
SDOCM00105237    Add F2837x Delfino support to SYS/BIOS
SDOCM00105235    Add support for Delfino C28x devices to the boot module
back to top

Upgrading and Compatibility Information

SYS/BIOS releases have many significant changes from DSP/BIOS 5.x.  It is important to understand the information below in order to successfully use SYS/BIOS and to migrate applications from DSP/BIOS 5.x.

SYS/BIOS software downloads

SYS/BIOS 6.35

SYS/BIOS 6.34

SYS/BIOS 6.33

SYS/BIOS 6.32

SYS/BIOS 6.31

DA830 ROM

The 'ti.sdo.io' and 'ti.sdo.utils' packages are no longer provided with SYS/BIOS

The ti.sysbios.ipc package and its modules have been deprecated

   
The ti.sysbios.family.arm.m3.Exception module has been deprecated


Placing of sections using MEM configs is no longer supported (ie MEM.TEXTSEG is unsupported)


The ti.sysbios.family.c64p.Cache.initSize configuration item is no longer supported

SYS/BIOS no longer contains all the tools and objects you will need

Migrating DSP/BIOS 5.x applications to SYS/BIOS back to top

Host Support

back to top

Dependencies

back to top

Device Support

Click here  for the list of supported devices.
 
back to top

Validation Information

Click here for the list of compilers used to build and validate this release (scroll down to Supported Targets section).

back to top

Known Issues

The following issues are known to affect this release:

back to top

Benchmarks

    For a full description of Benchmarks please see the appendices in the SYS/BIOS 6 User's Guide. back to top

Versioning

All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, alpha/EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 6.30.00.00-eng or 6.30.00.10-beta).


This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

To support multiple side-by-side installations of the product, the product version is encoded in the top level directory (e.g. bios_6_30_00_00).

Subsequent releases of patch upgrades will be identified by the patch number, ex. SYS/BIOS 6.30.01.15 with directory bios_6_30_01_15. Typically, these patches only include critical bug fixes.

Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.

back to top

Technical Support and Product Updates

back to top

Last updated: December 20, 2013 Build Ver: 6.37.01.24 Rev: m24