1    /* 
     2     *  Copyright (c) 2016 Texas Instruments. All rights reserved.
     3     *  This program and the accompanying materials are made available under the
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ======== Reset.xdc ========
    15     */
    16    
    17    package xdc.runtime;
    18    
    19    /*!
    20     *  ======== Reset ========
    21     *  Startup reset function manager
    22     *
    23     *  This module defines an initial reset function and can be used without
    24     *  requiring any other `xdc.runtime` module.  The reset function is called
    25     *  as early as possible in the application startup and is intended for
    26     *  platform-specific hardware initialization.
    27     *
    28     *  The reset function sequentially calls each of the functions added to the
    29     *  `{@link #fxns}` array starting from index 0.  If
    30     *  `{@link Startup#resetFxn Startup.resetFxn}` is defined, it is called
    31     *  before any of the functions defined by the `fxns` array.
    32     *
    33     *  By providing an array of startup functions, rather than a single function
    34     *  as `{@link Startup}` does, modules that need very early initialization
    35     *  can simply add their initialization to the list of functions to be called
    36     *  without having to implement a "chaining" mechanism or requiring the user
    37     *  to implement and maintain an application reset function.
    38     *
    39     *  @a(Warning)
    40     *  The reset function is _not_ supported on all platforms and, as a result,
    41     *  you should never place any "portable" code that is required for your
    42     *  application in this function.  Use the `{@link Startup}` module to
    43     *  define required application startup functions.
    44     *
    45     *  @see Startup
    46     */
    47    @Template("xdc/runtime/Reset.xdt")
    48    metaonly module Reset
    49    {
    50        /*!
    51         *  ======== fxns ========
    52         *  List of functions to call at reset
    53         *
    54         *  This array defines the functions that will be executed by the reset
    55         *  initialization function (`xdc_runtime_Startup_reset__I`) _in addition
    56         *  to_ the function specified by `{@link Startup#resetFxn}`.
    57         *
    58         *  The following code fragment shows how to add the externally defined
    59         *  function `myReset()` to this array.
    60         *  @p(code)
    61         *      var Reset = xdc.useModule("xdc.runtime.Reset");
    62         *      Reset.fxns[Reset.fxns.length++] = "&myReset";
    63         *  @p
    64         *
    65         *  @a(Warning)
    66         *  Although the functions specified in `fxns[]` are ordinary C functions,
    67         *  they are often called _before_ the C runtime is fully initialized;
    68         *  e.g., they may be called _before_ static variables are initialized.
    69         *  Reset functions should only assume that a minimal execution stack has
    70         *  initialized.
    71         *
    72         *  @see Startup#resetFxn
    73         */
    74        metaonly config xdc.runtime.Startup.InitFxn fxns[] = [];
    75    }
    76    /*
    77     *  @(#) xdc.runtime; 2, 1, 0,0; 5-8-2019 15:48:09; /db/ztree/library/trees/xdc/xdc-G16/src/packages/
    78     */
    79