Modules like
ti.sdo.io.Stream use an ISync.Handle for
selecting the synchronization mechanism. This allows Stream to be
independent of the synchronization mechanism.
An instance of SyncSem requires a Semaphore.Handle. When given a null
Semaphore.Handle, SynSem will create a Semaphore for its use. Note that
the underlying Semaphore has to be binary in nature and initialized as
being unavailable.
| const SyncSem_NO_WAIT |
 |
Used to specify no waiting
#define SyncSem_NO_WAIT (UInt)0
| const SyncSem_Q_BLOCKING |
 |
Blocking quality
#define SyncSem_Q_BLOCKING (Int)1
DETAILS
Implementations with this "quality" may cause the calling thread to
block;
| const SyncSem_WAIT_FOREVER |
 |
Used to wait forever
#define SyncSem_WAIT_FOREVER (UInt)~(0)
| enum SyncSem_WaitStatus |
 |
Error codes returned by ISync_wait
typedef enum SyncSem_WaitStatus {
SyncSem_WaitStatus_ERROR,
SyncSem_WaitStatus_TIMEOUT,
SyncSem_WaitStatus_SUCCESS
} SyncSem_WaitStatus;
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool SyncSem_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool SyncSem_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 SyncSem_Module_getMask();
// Returns the diagnostics mask for this module
Void SyncSem_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
| Instance Object Types |
 |
typedef struct SyncSem_Object SyncSem_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct SyncSem_Struct SyncSem_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
| Instance Config Parameters |
 |
typedef struct SyncSem_Params {
// Instance config-params structure
// Common per-instance configs
// Semaphore handle to be used. When Semaphore.Handle is null SyncSem
will create a Semaphore instance
} SyncSem_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
| config SyncSem_Params.sem // instance |
 |
Semaphore handle to be used. When Semaphore.Handle is null SyncSem
will create a Semaphore instance
| Runtime Instance Creation |
 |
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
| Instance Deletion |
 |
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
| SyncSem_query() // instance |
 |
Query for a particular quality
ARGUMENTS
handle
handle of a previously-created SyncSem instance object
qual
quality
RETURNS
TRUE or FALSE.
DETAILS
FALSE is returned if quality not supported.
| SyncSem_signal() // instance |
 |
Called at completion of an activity
ARGUMENTS
handle
handle of a previously-created SyncSem instance object
DETAILS
This function is non-blocking. It is also required that the underlying
sync be binary in nature.
This function does not take an Error.Block intentionally because
it can be called from ISR context.
| SyncSem_wait() // instance |
 |
Called to wait/poll for completion of an activity
ARGUMENTS
handle
handle of a previously-created SyncSem instance object
timeout
Timeout in microseconds
eb
Hist Pointer to Error.Block
RETURNS
Refer to description above
DETAILS
This function can block. Non-blocking implementations should return
WaitStatus_TIMEOUT to indicate a timeout.
| Instance Convertors |
 |
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
| Instance Built-Ins |
 |
Int SyncSem_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object