| module ti.sysbios.rts.iar.MultithreadSupport |
 |
Provide the kernel support needed for IAR re-entrant C run-time
This multi-thread support module uses hook functions, hook context,
and an overloaded implementation of the C library's lock and thread
local storage access functions to make C run-time library calls
re-entrant.
[
more ... ]
#include <ti/sysbios/rts/iar/MultithreadSupport.h>
Functions common to all target modules |
|
|
Constants |
extern const Bool | |
DETAILS
This multi-thread support module uses hook functions, hook context,
and an overloaded implementation of the C library's lock and thread
local storage access functions to make C run-time library calls
re-entrant.
This module is used only with the IAR compiler.
To enable multi-thread support, load this module in your application
configuration script.
xdc.useModule('ti.sysbios.rts.iar.MultithreadSupport');
If your application is using a module which requires multi-thread
support, then that module is responsible for loading this module.
For example, the ti.posix.tirtos.Settings module will load this
module. In this case, it is not necessary to load it explicitly.
When this module is used, it will contribute the IAR linker option
--threaded_lib to the linker command.
When using the IAR Embedded Workbench IDE, if you enable thread support
in your project settings, you must also include this module in your
configuration (unless it is already used as described above). There is
no mechanism for the IAR IDE to communicate the project selections to
this module.
On memory limited devices, it is possible to disable the re-entrant
support in order to minimize the memory footprint. See
enableMultithreadSupport for
details.
NOTE
Calling C run-time functions from SWI or HWI threads is not supported
and will generate an exception if multi-thread support is enabled.
| config MultithreadSupport_enableMultithreadSupport // module-wide |
 |
Disable the multi-thread support feature
extern const Bool MultithreadSupport_enableMultithreadSupport;
DETAILS
When necessary, it is possible to disable the re-entrant support in
order to minimize the memory footprint. For example, if using POSIX
support on a memory limited device, you may disable re-entrant support
by adding the following to your application configuration script.
var MultithreadSupport = xdc.useModule('ti.sysbios.rts.iar.MultithreadSupport');
MultithreadSupport.enableMultithreadSupport = false;
NOTE
When multi-thread support is disabled, errno will be a global
symbol. If multiple threads are referencing errno, it will not
be thread-safe.
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool MultithreadSupport_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool MultithreadSupport_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 MultithreadSupport_Module_getMask();
// Returns the diagnostics mask for this module
Void MultithreadSupport_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var MultithreadSupport = xdc.useModule('ti.sysbios.rts.iar.MultithreadSupport');
module-wide config parameters
generated on Thu, 23 May 2019 00:23:09 GMT