module ti.sysbios.rts.gnu.ReentSupport |
|
|
Newlib RTS library re-entrancy support module
The Reentrancy Support module implements locking APIs for the
Newlib libraries and provides an overloaded implementation of
the library's __getreent() function to make the C runtime library
calls re-entrant and thread safe.
[
more ... ]
#include <ti/sysbios/rts/gnu/ReentSupport.h>
Functions common to all target modules |
|
|
Constants |
| |
extern const Bool | |
DETAILS
The Reentrancy Support module implements locking APIs for the
Newlib libraries and provides an overloaded implementation of
the library's __getreent() function to make the C runtime library
calls re-entrant and thread safe.
The C runtime library (newlib libc/libm) functions internally
call __getreent() to get the address of the currently executing
thread's reentrancy structure.
The __getreent() function allocates storage for the reentrancy
structure when it is called for the very first time within a
thread context. Any subsequent calls to __getreent() within the
same thread context read the current thread's stored context to
determine the previously allocated reentrancy structure's address
and return it.
When a thread is deleted, the DeleteHook is called and will free
any memory that was allocated to store the reentrancy structure
associated with the thread.
The C runtime library calls locking APIs to ensure thread
safety. The locking APIs are defined in the sys/lock.h header
that is distributed with XDC tools. This module provides an
implementation for these locking APIs.
Reentrancy support is enabled by default if tasking is enabled
and can be disabled by adding the following code to the application's
config script.
var ReentSupport = xdc.useModule('ti.sysbios.rts.gnu.ReentSupport');
// 'true' to enable Task level reentrancy support (default)
// 'false' to disable Task level reentrancy support
ReentSupport.enableReentSupport = false;
Note: Calling C runtime functions from SWI and HWI threads
is not supported and will generate an exception if
reentrancy support is enabled.
config ReentSupport_A_badThreadType // module-wide |
|
Asserted in ReentSupport_getReent()
extern const Assert_Id ReentSupport_A_badThreadType;
config ReentSupport_enableReentSupport // module-wide |
|
Enable re-entrancy support
extern const Bool ReentSupport_enableReentSupport;
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool ReentSupport_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool ReentSupport_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 ReentSupport_Module_getMask();
// Returns the diagnostics mask for this module
Void ReentSupport_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var ReentSupport = xdc.useModule('ti.sysbios.rts.gnu.ReentSupport');
module-wide config parameters
msg: "A_badThreadType: Cannot call a C runtime library API from a Hwi or Swi thread."
};
generated on Thu, 23 May 2019 00:23:09 GMT