1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31
32 33 34
35
36 package ti.sysbios.rts.gnu;
37
38 import xdc.rov.ViewInfo;
39
40 import xdc.runtime.Error;
41 import xdc.runtime.Assert;
42
43 import ti.sysbios.knl.Task;
44 import ti.sysbios.knl.Semaphore;
45
46 /*!
47 * ======== ReentSupport ========
48 * Newlib RTS library re-entrancy support module
49 *
50 * The Reentrancy Support module implements locking APIs for the
51 * Newlib libraries and provides an overloaded implementation of
52 * the library's __getreent() function to make the C runtime library
53 * calls re-entrant and thread safe.
54 *
55 * The C runtime library (newlib libc/libm) functions internally
56 * call __getreent() to get the address of the currently executing
57 * thread's reentrancy structure.
58 *
59 * The __getreent() function allocates storage for the reentrancy
60 * structure when it is called for the very first time within a
61 * thread context. Any subsequent calls to __getreent() within the
62 * same thread context read the current thread's stored context to
63 * determine the previously allocated reentrancy structure's address
64 * and return it.
65 *
66 * When a thread is deleted, the DeleteHook is called and will free
67 * any memory that was allocated to store the reentrancy structure
68 * associated with the thread.
69 *
70 * The C runtime library calls locking APIs to ensure thread
71 * safety. The locking APIs are defined in the sys/lock.h header
72 * that is distributed with XDC tools. This module provides an
73 * implementation for these locking APIs.
74 *
75 * Reentrancy support is enabled by default if tasking is enabled
76 * and can be disabled by adding the following code to the application's
77 * config script.
78 *
79 * @p(code)
80 * var ReentSupport = xdc.useModule('ti.sysbios.rts.gnu.ReentSupport');
81 *
82 * // 'true' to enable Task level reentrancy support (default)
83 * // 'false' to disable Task level reentrancy support
84 * ReentSupport.enableReentSupport = false;
85 * @p
86 *
87 * Note: Calling C runtime functions from SWI and HWI threads
88 * is not supported and will generate an exception if
89 * reentrancy support is enabled.
90 *
91 */
92
93 @Template ("./ReentSupport.xdt")
94 @ModuleStartup
95
96 module ReentSupport
97 {
98 /*!
99 * ======== ModuleView ========
100 * @_nodoc
101 */
102 metaonly struct ModuleView {
103 Bool enableReentSupport;
104 }
105
106 /*!
107 * ======== rovViewInfo ========
108 * @_nodoc
109 */
110 @Facet
111 metaonly config ViewInfo.Instance rovViewInfo =
112 ViewInfo.create({
113 viewMap: [
114 [
115 'Module',
116 {
117 type: ViewInfo.MODULE,
118 viewInitFxn: 'viewInitModule',
119 structName: 'ModuleView'
120 }
121 ],
122 ]
123 });
124
125 /*!
126 * ======== enableReentSupport ========
127 * Enable re-entrancy support
128 */
129 config Bool enableReentSupport = true;
130
131
132
133 /*! Asserted in ReentSupport_getReent() */
134 config Assert.Id A_badThreadType = {
135 msg: "A_badThreadType: Cannot call a C runtime library API from a Hwi or Swi thread."
136 };
137
138 internal:
139
140
141
142 143 144 145 146 147 148
149 Ptr getReent();
150
151 152 153 154
155 Void initGlobalReent();
156
157 158 159 160 161 162 163 164 165
166 Void taskCreateHook(Task.Handle task, Error.Block *eb);
167
168 169 170 171 172 173 174
175 Void taskDeleteHook(Task.Handle task);
176
177 178 179 180 181 182 183
184 Void taskRegHook(Int id);
185
186
187
188 struct Module_State {
189 Int taskHId;
190 Semaphore.Handle lock;
191 };
192 }