The Tesla and Ducati UniCaches do not support separate program and
data caches. Therefore none of the unique Cache_Type L1P/L1D/L2P/L2D
operations can be precisely supported. The APIs in this module ignore
the P/D and observe only the L1/L2 designations (ie Cache_Type_L1P
is functionally equivalent to Cache_Type_L1D and Cache_Type_L1).
enum Cache_Type |
|
Lists of bitmask cache types
typedef enum Cache_Type {
Cache_Type_L1P,
// Level 1 Program cache
Cache_Type_L1D,
// Level 1 Data cache
Cache_Type_L1,
// Level 1 caches
Cache_Type_L2P,
// Level 2 Program cache
Cache_Type_L2D,
// Level 2 Data cache
Cache_Type_L2,
// Level 2 caches
Cache_Type_ALLP,
// All Program caches
Cache_Type_ALLD,
// All Data caches
Cache_Type_ALL
// All caches
} Cache_Type;
struct Cache_CACHE |
|
Runtime representation of the Cache registers
typedef struct Cache_CACHE {
UInt32 L1_INFO;
UInt32 L1_CONFIG;
UInt32 L1_INT;
UInt32 L1_OCP;
UInt32 L1_MAINT;
Ptr L1_MTSTART;
Ptr L1_MTEND;
Ptr L1_CTADDR;
UInt32 L1_CTDATA;
UInt32 Reserved[0x77];
UInt32 L2_INFO;
UInt32 L2_CONFIG;
UInt32 L2_INT;
UInt32 L2_OCP;
UInt32 L2_MAINT;
Ptr L2_MTSTART;
Ptr L2_MTEND;
Ptr L2_CTADDR;
UInt32 L2_CTDATA;
} Cache_CACHE;
struct Cache_OCPConfig |
|
OCP Interface Configuration Register Settings
typedef struct Cache_OCPConfig {
UInt8 wrap;
UInt8 wrbuffer;
UInt8 prefetch;
UInt8 cleanbuf;
} Cache_OCPConfig;
struct Cache_SecurityConfig |
|
CONFIG Configuration Register Settings
typedef struct Cache_SecurityConfig {
UInt8 secure;
UInt8 nbypass;
UInt8 secint;
UInt8 secport;
UInt8 secmain;
} Cache_SecurityConfig;
config Cache_E_exception // module-wide |
|
Error raised when a Cache interrupt occurs
Reason bits are contents of Cache Interrupt Register
extern const Error_Id Cache_E_exception;
config Cache_configureCache // module-wide |
|
Configure cache at startup?
extern const Bool Cache_configureCache;
DETAILS
It is possible to configure the Cache at startup and not
enable it.
However, it is not possible to enable the Cache at startup
without configuring it.
Enabling the Cache will automatically enable configuring
the Cache.
config Cache_enableCache // module-wide |
|
Enable cache at startup?
extern const Bool Cache_enableCache;
DETAILS
Not implemented by all architectures. Refer to specific
architecture Cache module for details.
Enabling the Cache at startup will force
configuring the Cache at startup.
config Cache_maxLineModeBufSize // module-wide |
|
Maximum buffer size to use discrete cache line operations with
extern const SizeT Cache_maxLineModeBufSize;
DETAILS
For buffers below a certain size, cache maintenance operations are
more efficient if performed on single cache lines at a time
rather than on an entire region.
For buffer sizes equal to or less than this setting, the
inv,
wb, and
wbInv APIs will use a series of individual
cache line operations. For buffer sizes large than this setting, a
a single block mode operation will be performed.
For M3 cores, the default setting is 1024 bytes.
For 64T cores, the default setting is 4096 bytes.
extern Cache_cache |
|
This device's unicache register set address.
Initialized internally according to build target/device
Cache_CACHE Cache_cache; // linked as extern ti_sysbios_hal_unicache_Cache_cache
Cache_disable() // module-wide |
|
Disables the 'type' cache(s)
Void Cache_disable(Bits16 type);
ARGUMENTS
type
bit mask of Cache type
Cache_enable() // module-wide |
|
Enables all cache(s)
Void Cache_enable(Bits16 type);
ARGUMENTS
type
bit mask of Cache type
Cache_inv() // module-wide |
|
Invalidate the range of memory within the specified starting
address and byte count. The range of addresses operated on
gets quantized to whole cache lines in each cache. All lines
in range are invalidated for all the 'type' caches
Void Cache_inv(Ptr blockPtr, SizeT byteCnt, Bits16 type, Bool wait);
ARGUMENTS
blockPtr
start address of range to be invalidated
byteCnt
number of bytes to be invalidated
type
bit mask of Cache type
wait
wait until the operation is completed
Cache_invAll() // module-wide |
|
Invalidate all caches
DETAILS
Perform a global invalidate. All cache lines are
invalidated in L1 and L2 caches.
Waits for completion.
Cache_lock() // module-wide |
|
Locks a memory block into the cache
Void Cache_lock(Ptr blockPtr, SizeT byteCnt, Bits16 type, Bool wait);
ARGUMENTS
blockPtr
start address of range to be locked
byteCnt
number of bytes to be locked
type
bit mask of Cache type
wait
wait until the operation is completed
Cache_preload() // module-wide |
|
Loads a memory block into the cache
Void Cache_preload(Ptr blockPtr, SizeT byteCnt, Bits16 type, Bool wait);
ARGUMENTS
blockPtr
start address of range to be loaded
byteCnt
number of bytes to be loaded
type
bit mask of Cache type
wait
wait until the operation is completed
Cache_preloadLock() // module-wide |
|
Loads and locks a memory block into the cache
Void Cache_preloadLock(Ptr blockPtr, SizeT byteCnt, Bits16 type, Bool wait);
ARGUMENTS
blockPtr
start address of range to be loaded
byteCnt
number of bytes to be loaded
type
bit mask of Cache type
wait
wait until the operation is completed
Cache_read() // module-wide |
|
Read a block of memory from the cache.
Only whole numbers of 32 bit words are transferred.
byteCnt is divided by 4 to convert to number of words
Void Cache_read(Ptr blockPtr, SizeT byteCnt, Bits16 type, Ptr destBuf);
ARGUMENTS
blockPtr
start address of range to be loaded
byteCnt
number of bytes to be loaded
type
bit mask of Cache type
destBuf
address of destination buffer
Cache_unlock() // module-wide |
|
Unlocks a cached memory block
Void Cache_unlock(Ptr blockPtr, SizeT byteCnt, Bits16 type, Bool wait);
ARGUMENTS
blockPtr
start address of range to be locked
byteCnt
number of bytes to be locked
type
bit mask of Cache type
wait
wait until the operation is completed
Cache_wait() // module-wide |
|
Wait for a previous cache operation to complete
DETAILS
Wait for the cache wb/wbInv/inv operation to complete. A cache
operation is not truly complete until it has worked its way
through all buffering and all memory writes have landed in the
source memory.
Cache_wb() // module-wide |
|
Writes back a range of memory from all cache(s)
Void Cache_wb(Ptr blockPtr, SizeT byteCnt, Bits16 type, Bool wait);
ARGUMENTS
blockPtr
start address of range to be invalidated
byteCnt
number of bytes to be invalidated
type
bit mask of Cache type
wait
wait until the operation is completed
DETAILS
Writes back the range of memory within the specified starting
address and byte count. The range of addresses operated on
gets quantized to whole cache lines in each cache. All lines
within the range are left valid in the 'type' caches and the data
within the range will be written back to the source memory.
Cache_wbAll() // module-wide |
|
Write back all caches
DETAILS
Perform a global write back. There is no effect on program cache.
All data cache lines are left valid.
Perform a global write back.
All cache lines are left valid in L1 and L2 caches and the data in L1
cache is written back to L2 or external. All cache lines are left
valid in L2 cache and the data in L2 cache is written back to
external.
Waits for completion.
Cache_wbInv() // module-wide |
|
Writes back and invalidates the range of memory within the
specified starting address and byte count. The range of
addresses operated on gets quantized to whole cache lines in
each cache. All lines within the range are written back to the
source memory and then invalidated for all 'type' caches
Void Cache_wbInv(Ptr blockPtr, SizeT byteCnt, Bits16 type, Bool wait);
ARGUMENTS
blockPtr
start address of range to be invalidated
byteCnt
number of bytes to be invalidated
type
bit mask of Cache type
wait
wait until the operation is completed
Cache_wbInvAll() // module-wide |
|
Write back invalidate all caches
DETAILS
Performs a global write back and invalidate. All cache lines
are written out to physical memory and then invalidated.
Perform a global write back.
Then perform a global invalidate.
All cache lines are invalidated in L1 and L2 caches.
Waits for completion.
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool Cache_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool Cache_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 Cache_Module_getMask();
// Returns the diagnostics mask for this module
Void Cache_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
enum Cache.Type |
|
Lists of bitmask cache types
values of type Cache.Type
const Cache.Type_L1P;
// Level 1 Program cache
const Cache.Type_L1D;
// Level 1 Data cache
const Cache.Type_L1;
// Level 1 caches
const Cache.Type_L2P;
// Level 2 Program cache
const Cache.Type_L2D;
// Level 2 Data cache
const Cache.Type_L2;
// Level 2 caches
const Cache.Type_ALLP;
// All Program caches
const Cache.Type_ALLD;
// All Data caches
const Cache.Type_ALL;
// All caches
C SYNOPSIS
struct Cache.CACHE |
|
Runtime representation of the Cache registers
var obj = new Cache.CACHE;
obj.L1_INFO = UInt32 ...
obj.L1_CONFIG = UInt32 ...
obj.L1_INT = UInt32 ...
obj.L1_OCP = UInt32 ...
obj.L1_MAINT = UInt32 ...
obj.L1_MTSTART = Ptr ...
obj.L1_MTEND = Ptr ...
obj.L1_CTADDR = Ptr ...
obj.L1_CTDATA = UInt32 ...
obj.Reserved = UInt32[0x77] ...
obj.L2_INFO = UInt32 ...
obj.L2_CONFIG = UInt32 ...
obj.L2_INT = UInt32 ...
obj.L2_OCP = UInt32 ...
obj.L2_MAINT = UInt32 ...
obj.L2_MTSTART = Ptr ...
obj.L2_MTEND = Ptr ...
obj.L2_CTADDR = Ptr ...
obj.L2_CTDATA = UInt32 ...
C SYNOPSIS
struct Cache.OCPConfig |
|
OCP Interface Configuration Register Settings
var obj = new Cache.OCPConfig;
obj.wrap = UInt8 ...
obj.wrbuffer = UInt8 ...
obj.prefetch = UInt8 ...
obj.cleanbuf = UInt8 ...
C SYNOPSIS
struct Cache.SecurityConfig |
|
CONFIG Configuration Register Settings
var obj = new Cache.SecurityConfig;
obj.secure = UInt8 ...
obj.nbypass = UInt8 ...
obj.secint = UInt8 ...
obj.secport = UInt8 ...
obj.secmain = UInt8 ...
C SYNOPSIS
config Cache.E_exception // module-wide |
|
Error raised when a Cache interrupt occurs
Reason bits are contents of Cache Interrupt Register
msg: "E_exception: L%d reason: 0x%x"
};
C SYNOPSIS
config Cache.configureCache // module-wide |
|
Configure cache at startup?
Cache.configureCache = Bool false;
DETAILS
It is possible to configure the Cache at startup and not
enable it.
However, it is not possible to enable the Cache at startup
without configuring it.
Enabling the Cache will automatically enable configuring
the Cache.
C SYNOPSIS
config Cache.enableCache // module-wide |
|
Enable cache at startup?
Cache.enableCache = Bool false;
DETAILS
Not implemented by all architectures. Refer to specific
architecture Cache module for details.
Enabling the Cache at startup will force
configuring the Cache at startup.
C SYNOPSIS
config Cache.maxLineModeBufSize // module-wide |
|
Maximum buffer size to use discrete cache line operations with
Cache.maxLineModeBufSize = SizeT undefined;
DETAILS
For buffers below a certain size, cache maintenance operations are
more efficient if performed on single cache lines at a time
rather than on an entire region.
For buffer sizes equal to or less than this setting, the
inv,
wb, and
wbInv APIs will use a series of individual
cache line operations. For buffer sizes large than this setting, a
a single block mode operation will be performed.
For M3 cores, the default setting is 1024 bytes.
For 64T cores, the default setting is 4096 bytes.
C SYNOPSIS
metaonly config Cache.common$ // module-wide |
|
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly config Cache.configL1 // module-wide |
|
L1_CONFIG register settings
secure: 0,
nbypass: 0,
secint: 1,
secport: 1,
secmain: 1
};
metaonly config Cache.configL2 // module-wide |
|
L2_CONFIG register settings
secure: 0,
nbypass: 0,
secint: 1,
secport: 1,
secmain: 1
};
metaonly config Cache.l1InterruptHandler // module-wide |
|
L1 Interrupt Handler.
Default is set to an internal L1 interrupt handler
Cache.l1InterruptHandler = Void(*)(UArg) undefined;
metaonly config Cache.l1InterruptNumber // module-wide |
|
L1 Interrupt number.
Default is device unique but can be set in the user config file
Cache.l1InterruptNumber = UInt undefined;
metaonly config Cache.l1InterruptPriority // module-wide |
|
L1 Interrupt priority.
Default is device unique but can be set in the user config file
Cache.l1InterruptPriority = UInt undefined;
metaonly config Cache.l2InterruptHandler // module-wide |
|
L2 Interrupt Handler.
Default is set to an internal L2 interrupt handler
Cache.l2InterruptHandler = Void(*)(UArg) undefined;
metaonly config Cache.l2InterruptNumber // module-wide |
|
L2 Interrupt number.
Default is device unique but can be set in the user config file
Cache.l2InterruptNumber = UInt undefined;
metaonly config Cache.l2InterruptPriority // module-wide |
|
L2 Interrupt priority.
Default is device unique but can be set in the user config file
Cache.l2InterruptPriority = UInt undefined;
metaonly config Cache.ocpL1 // module-wide |
|
L1_OCP register settings
wrap: 0,
wrbuffer: 0,
prefetch: 0
};
metaonly config Cache.ocpL2 // module-wide |
|
L2_OCP register settings
wrap: 0,
wrbuffer: 0,
prefetch: 0,
cleanbuf: 0
};